:TRIGger:SEQuence:TRANsition:RSTart

Command Syntax

:TRIGger:SEQuence{A|B}:TRANsition:RSTart <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:TRANsition:RSTart?

Description

In the Edge Transition trigger mode (see :TRIGger:SEQuence:MODE), when triggering when the pulse width is inside or outside a range (see :TRIGger:SEQuence:PATTern:MODE), this command specifies the lower range of the width.