:TRIGger:SEQuence:TRANsition:REND
Command Syntax
:TRIGger:SEQuence{A|B}:TRANsition:REND <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:SEQuence{A|B}:TRANsition:REND?
Description
In the Edge Transition trigger mode (see :TRIGger:SEQuence:MODE), when triggering on a transition that is inside or outside a time range (see :TRIGger:SEQuence:TRANsition:MODE), this command specifies the range end time.