:TRIGger:SEQuence:TRANsition:TIME

Command Syntax

:TRIGger:SEQuence{A|B}:TRANsition:TIME <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:TRANsition:TIME?

Description

In the Edge Transition trigger mode (see :TRIGger:SEQuence:MODE), when triggering on a transition that is longer or shorter than specified time (see :TRIGger:SEQuence:TRANsition:MODE), this command specifies the amount of time.