:WAVeform:YFORmat:FLOat:YDATa?

Query Syntax

:WAVeform:YFORmat:FLOat:YDATa? [<starting_point_index>,[<number_of_points>]]
<starting_point_index>
Optional zero-based integer that is the starting point index.
<number_of_points>
Optional integer that is the number of point values to return. When using this parameter, the <starting_point_index> parameter is required. If this parameter is not used, it means the number of points to the end of the record.

Description

Returns the amplitude (Y-axis) data points values. The data is sent point-by-point starting from the graticule's left side and progressing to the right side. The returned amplitude values are in volts or Watts and do not require scaling. The data returned from this query has high resolution but can require long transfer times for long patterns. If fast transfer time is more important than measurement resolution, use the :WAVeform:YFORmat:WORD:YDATa? query instead. Use the :WAVeform:SOURce query to select data from a channel, differential channel, waveform memory, or a function.

Y-Format Commands
Query Description
:WAVeform:YFORmat:XINCrement? The time spacing between the data points and is returned with the :WAVeform:YFORmat:XINCrement? query.
:WAVeform:YFORmat:POINts? Returns the number of points in the data . The value Xindex in the following equation, is the data point count, starting at zero and ending at the number of points minus one.
:WAVeform:YFORmat:XORigin? The time value of the first data point.
The time at any data point:
Xtime = (Xdata)(Xincrement) + (Xorigin)

Pattern waveforms or waveforms captured when using a precision timebase have unequal time separations between the samples. In this situation, return the data in XY-format using the :WAVeform:XYFormat:FLOat:XDATa? and :WAVeform:XYFormat:FLOat:XDATa? queries.

See Definite-Length Block Response Data for more information.

Returned Data Type

The :WAVeform:YFORmat:FLOat:YDATa? query returns float (4 bytes) values as definite-length block data. You must specify this data type in your program language's command that you use to query the data. The specifier for this data type in your programming language will likely be "f" and it is identified in this example with red text. Confirm this with your programming language's documentation. The following is an example of the command used in Python using PyVISA.

endianness = Infiniium.query(':SYSTem:BORDer?')
Infiniium.write(':SYSTem:BORDer LENDian')
data = Infiniium.query_binary_values(':WAVeform:YFORmat:FLOat:YDATa?',
	datatype='f',
	container=list,
	is_big_endian=False,
	header_fmt='ieee')
Infiniium.write(':SYSTem:BORDer ' + endianness)

Endianness of Returned Block Data

To correctly interpret block data, you must know the endianness (byte order) of the returned data (integers or real), and you will most likely have to specify this same endianness in your program language's command that is used to query the data. Endianness can be set to "little endian" order in which the least significant byte is sent first and the most significant byte sent last. Or, the endianness can be set to "big endian" order in which the most significant byte is sent first and the least significant byte sent last.

To specify or query the endianness setting for binary block data, use the :SYSTem:BORDer command. The endianness setting applies to all binary queries except for :DISK:FILE:READ? query.

If you plan to change Infiniium's current endian setting, it is a good practice to query Infiniium's current endian setting and restore the setting when your program completes. This will avoid other programs having errors due to assuming a particular endianness setting.

After a factory default (:SYSTem:FACTory), little endian is set. A default setup (:SYSTem:DEFault) does not affect endianness.

Be aware that VXI plug-and-play drivers can change the endianness setting. As a result always explicitly set the endianness in your program before transferring any binary data.