:WAVeform:YFORmat:WORD:ENCoding:HOLE?

Query Syntax

:WAVeform:YFORmat:WORD:ENCoding:HOLE?

Description

Returns the data value 32,672 which is used to represent a waveform data point that has no sample data. To return the number of data points that contain holes, use the :WAVeform:HOLes? query. This condition applies to Y-format data (:WAVeform:YFORmat:WORD:YDATa?).