:WAVeform:YFORmat:WORD:ENCoding:CHIGh?

Query Syntax

:WAVeform:YFORmat:WORD:ENCoding:CHIGh?

Description

Returns the data value 32,736 which is used to represent a waveform data point that is clipped high. This indicates a data point's amplitude that is too high to be displayed on the screen. Use the :SYSTem:AUToscale command to properly scale the waveform to the display. To return whether any data points have been clipped, use the :WAVeform:CLIPped? query. This condition applies to Y-format data (:WAVeform:YFORmat:WORD:YDATa?).