:WAVeform:YFORmat:WORD:ENCoding:CLOW?
Query Syntax
:WAVeform:YFORmat:WORD:ENCoding:CLOW?
Description
Returns the data value 32,704 which is used to represent a waveform data point that is clipped low. This indicates a data point's amplitude that is too low to be displayed on the screen. Use the :SYSTem:AUToscale command to properly scale the waveform to the display. To return whether any data points have been clipped, use the :WAVeform:CLIPped? query. This condition applies to Y-format data (:WAVeform:YFORmat:WORD:YDATa?).