:WMEMory:FILE:LOAD
Command Syntax
:WMEMoryN:FILE:LOAD
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Description
Loads the selected waveform file (.h5, .csv, or .txt) into the indicated waveform memory location. Use the :WMEMory:FILE:NAME command to specify the name of the file to load. Use the :WMEMory:DISPlay command to display the waveform memory.
To load a waveform source into memory, for example connection 1 channel 1, use the :WMEMory:LOAD command.