:WMEMory:LOAD:SOURce

Command Syntax

:WMEMoryN:LOAD:SOURce <source_waveform>

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Where <source_waveform> can be one of the following:

  • CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply use CHANnel<ch1-8>.
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:64}

Query Syntax

:WMEMoryN:LOAD:SOURce?

Description

Selects the source waveform to load into waveform memory. Use the :CGMemory:LOAD command to actually load the selected source.

Example Command Sequence

:WMEMory2:LOAD:SOURce CHAN3
:WMEMory2:LOAD

Parent Command