:WMEMory:FILE:NAME
Command Syntax
:WMEMoryN:FILE:NAME "filename"
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:FILE:NAME?
Query Response
"string"
Description
Enters the name (including path) of a file to be imported into an waveform memory using the :WMEMory:FILE:LOAD command. If no path is given, the file expected to be in the default \Waveforms folder.