:WMEMory:LOAD
Command Syntax
:WMEMoryN:LOAD
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Description
Loads the selected waveform source into the indicated waveform-memory location. Use the :WMEMory:LOAD:SOURce command to select the source. Use the :WMEMory:DISPlay command to display the waveform-memory.
To load a waveform file into waveform memory, use the :WMEMory:LOAD and :WMEMory:LOAD:SOURce commands.
Example Command Sequence
:WMEMory2:LOAD:SOURce CHAN1_1 :WMEMory2:LOAD :WMEMory2:DISPlay ON
Child Commands
:WMEMory:LOAD:SOURcespecifies the source waveform on which to perform the measurement.