Simulation Operators

Simulation operators transform measured waveforms to compensate for the effects of various test-setup devices. For example, you can remove a cable's insertion loss from the measured waveform thus simulating a measurement at the input to the device under test.

De-embedding a Cable with Simulated Measurement Point

These are filtering operators that requires a single-valued waveform, as opposed to an eye diagram. Be sure that your trigger setup results in a single-valued waveform at the input to this operator.

Simulation Operators