Clock TIE

To measure Clock TIE (Time Interval Error), Clock Recovery must be performed to determine the clock locations.

Once the ideal clock frequency is determined, all of the cycles of your waveform are compared to the ideal clock frequency and the error statistics are computed. The following figure shows how the Clock TIE is measured on rising edges of the clock.

When measuring over the waveform, the Clock TIE measurement is made on all the cycles of the waveform including any cycles that are not in the waveform window. When measuring in a region, the Clock TIE measurement is made on all the cycles inside the region only.

Configurable Measurement Parameters

This measurement is affected by the following settings (choose Measure > Thresholds...):

To measure

  1. Click the toolbar's Clock tab.
  2. Click the Clock TIE button to open the Clock TIE dialog box.

  3. Select the signal on which to make the measurement.
  4. Select the Region in which to make the measurement:
    • Displayed Waveform — is what you see in the waveform window (which can be a zoomed-in view of the complete waveform).
    • Entire Waveform — specifies the complete waveform.
    • Region N — If regions are enabled for the selected signal, you can select one of those regions.
  5. Select the measurement units as either Second or Unit Interval.
  6. Specify the Edge Direction as Rising, Falling, or Both.
  7. If you want to apply a filter to the TIE measurement, select Filter TIE. Then, specify the filter parameters using these controls:

    • TIE Filter Type — Selects Low-pass, Band-pass, or High-pass.

    • Start Frequency — Frequencies below this value are filtered out of the TIE measurement.

    • Stop Frequency — Frequencies above this value are filtered out of the TIE measurement.

    • TIE Filter Shape — You can select from these TIE filter edge shapes:

      • Rectangular — The TIE filter is a brickwall filter.

      • 20dB/Decade — The TIE filter edge(s) roll off at 20 dB per decade.

      • 40dB/Decade — The TIE filter edge(s) roll off at 40 dB per decade.

      • 60dB/Decade — The TIE filter edge(s) roll off at 60 dB per decade.

      • First Order — Available with the High-pass and Low-pass filter types only, this is similar to the 20 dB per decade roll off, but the response is more curved. See:

      • Second Order — Available with the High-pass and Low-pass filter types only, this is similar to the 40 dB per decade roll off, but the response is more curved. See:

        When the Second Order TIE filter edge shape is selected, you can also specify the Damping Factor:

        < 1 underdamped
        > 1 overdamped
        = 1.0 critically damped
        = 0.707 Often considered ideal or optimal because of its fast settling time (optimally flat) and Butterworth type response.
  8. Click Apply.

SCPI Command

:MEASure:CLOCk:CTIerror