PAM Measurements

If the PAM-N Analysis software option is installed, you can make the following measurements on PAM waveforms.

The Linearity, Levels, and Levels RMS measurements can also be used on NRZ waveforms (0 and 1 levels for one eye, in other words, PAM-2).