Follow the steps below to confirm the results of the DUT’s segment phase noise measurement by using the E5052B’s segment PN window.
Other topics about Common Settings
Format options are not available for Segment Phase Noise measurement.
When the downconverter is turned on, the RF input is set to Downconverter, and the external mixer is set to Not Used, the function to search for the carrier signal in the specified carrier frequency band and reflect the result to the nominal frequency is available.
Press Setup
Press Carrier Search to execute the carrier signal search.
The detected signal frequency is reflected on the nominal frequency.
Press Marker to display marker 1 on the screen.
Move marker 1 to the point you want to confirm and read the measurement value displayed in the upper part of the graph. To confirm multiple values, press Marker > Marker x (x=1 to 10), which allows you to display up to marker 10.
Example of Measurement Screen (Phase Noise vs. Segment PN)

In this measurement, you cannot specify the sweep time. It will be determined automatically based on the selection of the offset frequency sweep range and the resolution bandwidth.
Specify the noise integration range by using the band marker. For more information, refer to Searching in Specified Range. You do not have to use the band marker to integrate the entire range.
Press Marker Fctn > Analysis Type.
Press Integral. In the upper right part of the screen, you will see the Integral Phase Noise value [dBc], the RMS Noise value [rad, deg], the RMS Jitter value [sec] and Residual FM value [Hzrms].
Calculate Integral Phase Noise, Jitter and Residual FM, using the specified data by Analysis range.
Integral Phase Noise returns the value of SSB Integral result. RMS Noise, Jitter and Residual FM returns the value after applying the DSB conversion.
|
Value |
Formula |
|
Integral Phase Noise |
10 * log(integ(10 ^ (L(f) / 10))) [dBc] |
|
RMS Noise |
sqrt(2 * 10 ^ (Integral Phase Noise / 10)) [rad] |
|
RMS Jitter |
RMS Noise / (2 x ƒÎ x Carrier frequency) [sec] |
|
Residual FM |
sqrt(2 x integ(f ^ 2 * 10 ^ (L(f) / 10))) [Hz] |
where, L(f): Phase Noise [dBc/Hz] and integ(x): Integral
When Power is selected in the Spurious measurement, it is calculated with adding the power of Spurious after integrating except Spurious.
It is available to calculate the Allan Variance and Jitter using the measured average time and the measured cut-off frequency.
This operation is available to execute with SCPI commands, and it is not supported with the key operation. For more information refer to the following SCPI commands
SCPI.CALCulate.PS(Ch).TRACe(Tr).FUNCtion.AVARiance.DATA
SCPI.CALCulate.PS(Ch).TRACe(Tr).FUNCtion.AVARiance.MEMory
The value obtained with E5052B as Sigma is standard deviation, and the Allan Variance as the general definition is the value that is squared this Sigma.