Screen Area: Names and Functions of Parts

 

 

Click on the name or area for details of the topic:

1. Data Entry Bar

2. Softkey Menu Bar

3. Instrument Status Bar

4. Measurement Windows

5. Windows Status Bar - Windows Status Bar may or may not appear, depending on the Windows license. Under the same condition, either Windows resize buttons or E5052B resize button will appear. For more information, refer to Windows License.