Show Taskbar: Show the Windows Taskbar
Move App to Back
Exit: Exit the VNA application
Control Panel... : Open Windows Control Panel
Manage Files... : Open Windows File Explore
Next/Prev Keys : Select Next/Previous window/channel/trace for the selected one
On The Web... : Connect to the Web on the keysight.com.
Tech Support
Verification
Diagnostics
Display Test
Front Panel: Check the front panel functionality.
SSA Cal Status... Opens the PathWave Calibration Advisor Status dialog: For information on how to set up the PahtWave Calibration Advisor, click on in the top-right part of the dialog to access the PathWave Calibration Advisor Help.