CALCulate:FSIMulator:DRAFt: | APPLy | CIRCuit: | ADD | CATalog? | DELete | DEVice | PORTs | ARRay | REVerse | EMBED | TYPE | FILE | MODify | NEXT? | PARameter | C | C2 | DELay | G | G2 | L | L2 | LOSS | VALue | R | R2 | RIN | ROUT | Z0 | RESet | STATe | VNA | PORTs | DISCard | EXTension:PORT: | DELay | DISTance | VALue | UNIT | END | LOSS | VALue | STATe | MEDium | WAVEguide | FCUToff | COUPle | VELocity | FACTor | COUPle | STATe | SAVE |SECTion | CIRCuit | ENABle | EXTension | ENABle | ZCONversion | ENABle | ZCONversion | DIFFerential | STATe |
BPORt | SCALar |
:LPORt | SCALar | COMMonmode | STATe |
BPORt | SCALar |
LPORt<pnum> | SCALar | SENDed:PORT | STATe | COMPLex | SCALar
|
See Also
Example Programs
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
CALC:PAR:CAT? alone can NOT be used to return a balanced measurement parameter. If a balanced measurement transform is being performed, then additional querying of the CALC:FSIM system is required to determine the balanced parameter type. See an example.
BPORt versus LPORt commands - For each command in this subsystem that includes a BPORt keyword, there is an LPORt equivalent. The commands are identical except for the way in which the balanced / logical port numbers are specified:
The BPORt commands refer to the Balanced port number. There can only be up to two balanced ports. This method is compatible with the ENA network analyzer.
The LPORt commands refer to the Logical port number. A balanced port can appear as either logical port 1, 2, or 3. These are the references as they appear in the front-panel user interface.
Applicable Models: E505xA with VNA ports (Write only) Copies the draft fixture to active fixture. Exact same functionality as CALC:FSIM:APPL |
|
Parameters |
Not applicable |
Example |
CALC:FSIM:DRAF:APPL calculate:fsimulator:draft:apply |
Return Type |
Not applicable |
Not applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:ADD <block type>, <fixt port count>
Applicable Models: E505xA with VNA ports (Write only) Create a block of the specified block type with the specified fixture port count. By default, this block will be created on the VNA Port 1 with "de-embed". It can be moved and changed to "embed" with commands below. |
|||||||||||||||||||||||||||||||||||||
Parameters |
|
||||||||||||||||||||||||||||||||||||
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
||||||||||||||||||||||||||||||||||||
<circN> |
Circuit Number |
||||||||||||||||||||||||||||||||||||
<block type> |
|
||||||||||||||||||||||||||||||||||||
<fixt port count> |
Number of block port |
||||||||||||||||||||||||||||||||||||
Examples |
CALC:FSIM:DRAF:CIRC:ADD SLPC,2 calculate2:fsimulator:draft:circuit:add SLPC,2 |
||||||||||||||||||||||||||||||||||||
Query Syntax |
Not Applicable |
||||||||||||||||||||||||||||||||||||
Return Type |
Not Applicable |
||||||||||||||||||||||||||||||||||||
Not Applicable |
|||||||||||||||||||||||||||||||||||||
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:CATalog?
Applicable Models: E505xA with VNA ports (Read only) Returns a comma-separated list of circuit numbers created in the draft circuit. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
Examples |
CALC:FSIM:DRAF:CIRC:CAT? calculate2:fsimulator:draft:circuit:catalog? |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:CATalog? |
Return Type |
comma-separated string |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DELete
Applicable Models: E505xA with VNA ports (Write only) Deletes the specified circuit. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:DEL calculate2:fsimulator:draft:circuit:delete |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs[:ARRay] <port list - in, out>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the Device ports for the specified circuit. The number of ports must be even and correspond to the number of ports of the fixture. This command can be used to reverse or change the order of ports in an SNP file. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:DEV:PORT 2,1 calculate2:fsimulator:draft:circuit:device:ports:array 2,1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs[:ARRay]? |
Return Type |
Numeric |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs:REVerse <bool>
Applicable Models: E505xA with VNA ports (Read-Write) Sets whether or not to reverse the ports on an existing S2P file. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
Choose from: ON or 1 - Reverse the ports. OFF or 0 - Do not reverse the ports. |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:DEV:PORT:REV ON calculate2:fsimulator:draft:circuit:device:ports:reverse 1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs:REVerse? |
Return Type |
Boolean |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:EMBED:TYPE <embed | deembed>
Applicable Models: E505xA with VNA ports (Read-Write) Sets whether the circuit should be embedded or de-embedded. Valid for all block Types. The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<char> |
Choose from : EMBed - Add Network circuit. DEEMbed - Remove Network circuit |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:EMBED:TYPE EMBED calculate2:fsimulator:draft:circuit:embed:type deembed |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:EMBED:TYPE? |
Return Type |
character |
EMBed |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE <filename>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the filename. Valid blocks: FILe, D4PFile, FGLoop The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<filename> |
File name and extension (.s2P) of the de-embedding circuit. Files are stored in the default folder "D:\". To recall from a different folder, specify the full path name. |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:FILE 'myFile.s2P' calculate2:fsimulator:draft:circuit:file "D:\myFile.s2P" |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE? |
Return Type |
string |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:EXTRapolate <bool>
Applicable Models: E505xA with VNA ports (Read-Write) Sets whether or not extrapolation is allowed. Valid blocks: FILe, D4PFile, FGLoop. The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
Choose from: ON or 1 - Turns Extrapolation ON OFF or 0 - Turns Extrapolation OFF |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:FILE:EXTR ON calculate2:fsimulator:draft:circuit:file:extrapolate 1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:EXTRapolate? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:MODify <enum>
Applicable Models: E505xA with VNA ports (Read-Write) Sets all reflection and crosstalk parameters on the DUT side to zero. Learn more. The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<enum> |
Choose from: NONE - Does not modify the block. NREFlect - Sets all reflection parameters on the DUT-side to zero. NXTalk - Sets all reflection and crosstalk parameters on the DUT-side to zero. |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:FILE:MOD NONE calculate2:fsimulator:draft:circuit:file:modify nreflect |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:MODify? |
Return Type |
Enumeration |
NONE |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:NEXT?
Applicable Models: E505xA with VNA ports (Read only) Returns the next free circuit number than be used to create a new circuit block |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:NEXT? calculate2:fsimulator:draft:circuit:next? |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:NEXT? |
Return Type |
Numeric |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the capacitance (C) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL. The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Capacitance value in farads. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:C 0.00002 calculate2:fsimulator:draft:circuit:parameter:C 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C2 <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the capacitance (C2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Capacitance value in farads. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:C2 0.00002 calculate2:fsimulator:draft:circuit:parameter:C2 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C2? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:DELay <num>
Applicable Models: E505xA with VNA ports (Read-Write) Sets port extension delay in time. Valid blocks: ILIN. The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<num> |
The port extension in seconds; may include suffix. Choose a number between: -1E18 and 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:DEL 2MS calculate2:fsimulator:draft:circuit:parameter:delay .00025 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:DEL? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the conductance (G) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL. The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Conductance value in siemens. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:G 0.00002 calculate2:fsimulator:draft:circuit:parameter:g 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G2 <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the conductance (G2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Conductance value in siemens. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:G2 0.00002 calculate2:fsimulator:draft:circuit:parameter:g2 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G2? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the inductance (L) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL. The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Inductance value in henries. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:L 0.00002 calculate2:fsimulator:draft:circuit:parameter:l 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L2 <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the inductance (L2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Inductance value in henries. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:L2 0.00002 calculate2:fsimulator:draft:circuit:parameter:l2 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L2? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:LOSS:VALue <num>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the loss at DC. Valid blocks: ILIN. The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<num> |
Loss in dB. Choose a value between -90 and 90. |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:LOSS:VAL 1.5 calculate2:fsimulator:draft:circuit:parameter:loss:value .1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:LOSS:VALue? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the resistance (R) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL. The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:R 0.00002 calculate2:fsimulator:draft:circuit:parameter:r 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R2 <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the resistance (R2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:R2 0.00002 calculate2:fsimulator:draft:circuit2:parameter:r2 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R2? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:RIN <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the resistance (R) value at input of transformer (real only). Valid blocks: TRANs The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:RIN 0.00002 calculate2:fsimulator:draft:circuit2:parameter:rin 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:RIN? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:ROUT <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the resistance (R) value at output of transformer (real only). Valid blocks: TRANs The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:ROUT 0.00002 calculate2:fsimulator:draft:circuit2:parameter:rout 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:ROUT? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:Z0 <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the impedance (Z0) for the ideal block (scalar value). Valid blocks: ILIN. The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
Impedance value in ohms. Choose a value between -1E18 to 1E18 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:PAR:Z0 0.00002 calculate2:fsimulator:draft:circuit:parameter:z0 0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:Z0? |
Return Type |
Numeric |
50 |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:RESet
Applicable Models: E505xA with VNA ports (Write only) Resets the circuit section to preset values Note: This command impacts the circuits and the port extensions. It does not change any impedance conversion values. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
Examples |
CALC:FSIM:DRAF:CIRC:RES calculate2:fsimulator:draft:circuit:reset |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:STATe <bool>
Applicable Models: E505xA with VNA ports (Read-Write) Turns the circuit ON and OFF. Valid for all block types The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
Choose from: ON or 1 - Turns the circuit ON OFF or 0 - Turns the circuit OFF |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:STAT ON calculate2:fsimulator:draft:circuit1:state off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:STATe? |
Return Type |
Boolean |
ON |
|
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:VNA:PORTs <port list>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the VNA ports for the specified circuit. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<circN> |
Circuit Number |
Examples |
CALC:FSIM:DRAF:CIRC:VNA:PORT 2 calculate2:fsimulator:draft:circuit2:vna:ports 2 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:VNA:PORTs? |
Return Type |
Numeric |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Write only) Copies the active fixture into scratch/draft fixture (discards changes on scratch/draft fixture) |
|
Parameters |
Not applicable |
Example |
CALC:FSIM:DRAF:DISC calculate:fsimulator:draft:discard |
Return Type |
Not applicable |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the delay value in time at the specified port. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
<pnum> |
Port Number that will receive the delay setting. If unspecified, value is set to 1. |
<value> |
The port extension in seconds; may include suffix. Choose a number between: -1E18 and 1E18e. |
Examples |
CALC:FSIM:DRAF:EXT:PORT1:DEL
0.02 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DELay? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the units for specifying port extension delay in physical length (distance). |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
<pnum> |
Port Number. This number is ignored and all ports have the same setting. |
<char> |
Units for delay in distance. Choose from:
|
Examples |
CALC:FSIM:DRAF:EXT:PORT2:DIST:UNIT
MET |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT:DISTance:UNIT? |
Return Type |
Character |
METer |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the port extension delay in physical length (distance). |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
<pnum> |
Port Number that will receive the delay setting. If unspecified, value is set to 1. |
<value> |
Physical length of fixture of added transmission line. First specify units with :CALC:FSIM:DRAF:EXT:PORT:DIST:UNIT |
Examples |
CALC:FSIM:DRAF:EXT:PORT1:DIST:VAL
12 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DISTance:VALue? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Write Only) Moves the port extension block to the left-most side of the circuit sections. This command allows the port extensions to be moved around in the circuit . This command should be executed after adding the other block. Because adding the block resets the port extension block position. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
<pnum> |
Port Number that will receive the delay setting. If unspecified, value is set to 1. |
Examples |
CALC:FSIM:DRAF:EXT:PORT1:END |
Query Syntax |
Not applicable |
Return Type |
Not applicable |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the frequency for the Freq and Loss pair number and for the specified port number. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number that will receive the freq/loss settings. If unspecified, value is set to 1. |
<n> |
Freq and Loss pair number. Choose from 1 or 2. If unspecified, value is set to 1. |
<value> |
Frequency value. Choose a frequency within the frequency span of the VNA. |
Examples |
CALC:FSIM:DRAF:EXT:PORT1:LOSS2:FREQ
10E9 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:FREQuency? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the Loss value for the specified port number. Learn about Loss Compensation values. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number that will receive the Freq/Loss settings. If unspecified, value is set to 1. |
<n> |
Loss "Use" number. Choose from 1 or 2. If unspecified, value is set to 1. |
<value> |
Loss in dB. Choose a value between -90 and 90 |
Examples |
CALC:FSIM:DRAF:EXT:PORT:LOSS1:VAL 1 calculate:fsimulator:draft:extension:port2:loss2:value .1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:VALue? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the ON/OFF state for the Freq and Loss pair number and for the specified port number. Learn about Loss Compensation values. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number that will receive the Freq/Loss settings. If unspecified, value is set to 1. |
<n> |
Freq and Loss pair. Choose from 1 or 2. If unspecified, value is set to 1. |
<value> |
State of Freq and Loss values for port extension. 0 or OFF Specified Freq and Loss values are OFF 1 or ON Specified Freq and Loss values are ON |
Examples |
CALC:FSIM:DRAF:EXT:PORT:LOSS:STAT
0 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:STATe? |
Return Type |
Boolean |
OFF |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the Port Loss at DC value for the specified port number. Learn about Loss Compensation values. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port number to receive Loss value. If unspecified, value is set to 1. |
<value> |
Loss in dB. Choose a value between -90 and 90 |
Examples |
CALC:FSIM:DRAF:EXT:PORT:DCL:VAL 1.5 calculate:fsimulator:draft:extension:port2:dcloss:value .1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DCLoss:VALue? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the media type of the added fixture or transmission line. See also SENS:CORR:EXT:PORT:SYSMedia Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number. This number is ignored and all ports have the same setting. |
<char> |
Medium type. Choose from:
|
Examples |
CALC:FSIM:DRAF:EXT:PORT:MED COAX calculate:fsimulator:draft:extension:port2:medium waveguide |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:MEDium? |
Return Type |
Character |
COAX |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the cuttoff (minimum) frequency of the added waveguide fixture or transmission line. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number for which media type is being set. If unspecified, value is set to 1. |
<value> |
Cutoff frequency in Hz. This value is ignored when CALC:FSIM:DRAF:EXT:PORT:MED is set to COAX for the same port. |
Examples |
CALC:FSIM:DRAF:EXT:PORT:WAVE:FCUT 1e8 calculate:fsimulator:draft:extension:port2:waveguide:cutoff 100Mhz |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:WAVEguide:FCUToff? |
Return Type |
Numeric |
System Media Cutoff Frequency |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the state of coupling with the system Velocity Factor value. Learn more. Note: This command potentially affects ALL measurements on the VNA. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number. This number is ignored and all ports have the same setting. |
<bool> |
Coupling state. Choose from:
|
Examples |
CALC:FSIM:DRAF:EXT:PORT:WAVE:COUP 1 calculate:fsimulator:draft:extension:port2:waveguide:couple off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:WAVEguide:COUPle? |
Return Type |
Boolean |
1 or ON (Coupled) |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the velocity factor of the fixture or added transmission line. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number for which velocity factor is being set. If unspecified, value is set to 1. |
<value> |
Velocity Factor. Set SENS:CORR:EXT:PORT:SYSV to use the system velocity factor. |
Examples |
CALC:FSIM:DRAF:EXT:PORT:VEL:FAC .6 calculate:fsimulator:draft:extension:port2:velocity:factor 1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:VELocity:FACtor? |
Return Type |
Numeric |
System Velocity Factor |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the state of coupling with the system Velocity Factor value. Learn more. Note: This command potentially affects ALL measurements on the VNA. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number. This number is ignored and all ports have the same setting. |
<bool> |
Coupling state. Choose from:
|
Examples |
CALC:FSIM:DRAF:EXT:PORT:VEL:COUP 1 calculate:fsimulator:draft:extension:port2:velocity:couple off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:VELocity:COUPle? |
Return Type |
Boolean |
1 or ON (Coupled) |
|
Applicable Models: E505xA with VNA ports (Read-Write) Sets and returns the state of port extension for the specified port. Note: This command potentially affects ALL measurements on the VNA. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<pnum> |
Port Number for which port extension is being set. If unspecified, value is set to 1. |
<bool> |
Port extension state. Choose from:
|
Examples |
CALC:FSIM:DRAF:EXT:PORT:STAT 1 calculate:fsimulator:draft:extension:port2:state off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>[:STATe]? |
Return Type |
Boolean |
0 |
|
Applicable Models: E505xA with VNA ports (Write only) Saves SNP file corresponding to the entire scratch/draft fixture. |
|
Parameters |
|
<snpName> |
String - snp file name. Appends ".sNp" depending on num ports |
Example |
CALC:FSIM:DRAF:SAVE "myFixure" calculate:fsimulator:draft:save "D:\myfixture" |
Return Type |
Not applicable |
Not applicable |
|
CALCulate<cnum>:FSIMulator:DRAFt:SECTion:CIRCuit:ENABle <ON | OFF>
Applicable Models: E505xA with VNA ports (Read-Write) Turns all circuits ON or OFF for all ports. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<ON | OFFl> |
ON (or 1) - turns all circuits ON. OFF (or 0) -turns all circuits OFF. |
Examples |
CALC:FSIM:DRAF:SECT:CIRC:ENAB ON calculate2:fsimulator:draft:section:circuit:enable off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:SECTionCIRCuit:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|
CALCulate<cnum>:FSIMulator:DRAFt:SECTion:EXTension:ENABle <ON | OFF>
Applicable Models: E505xA with VNA ports (Read-Write) Turns port extensions ON or OFF for all ports. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<ON | OFFl> |
ON (or 1) - turns port extensions ON. OFF (or 0) - turns port extensions OFF. |
Examples |
CALC:FSIM:DRAF:SECT:EXT:ENAB ON calculate2:fsimulator:draft:section:extension:enable off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:SECTion:EXTension:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
|
CALCulate<cnum>:FSIMulator:DRAFt:SECTion:ZCONversion:ENABle <ON | OFF>
Applicable Models: E505xA with VNA ports (Read-Write) Turns all ZConversions ON or OFF (both SE and BAL). Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<ON | OFFl> |
ON (or 1) - turns all ZConversions ON. OFF (or 0) - turns all ZConversions OFF. |
Examples |
CALC:FSIM:DRAF:SECT:ZCON:ENAB ON calculate2:fsimulator:draft:section:zconversion:enable off |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:SECTion:ZCONversion:ENABle? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:STATe <bool>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the differential port impedance conversion function ON/OFF. Must also set the fixture simulator function to ON using CALC:FSIM:STAT. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
State of the differential port impedance conversion function. Choose from OFF (or 0) Differential port impedance conversion OFF ON (or 1) Differential port impedance conversion ON |
Examples |
CALC:FSIM:DRAF:ZCON:DIFF:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:STATe? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:COMPLex <real>,<img>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the complex impedance value for the differential port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Balanced port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<real> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
<img> |
Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18. |
Examples |
CALC:FSIM:DRAF:ZCON:DIFF:BPOR2:COMPL
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:COMPlex? |
Return Type |
Comma-separated numeric |
0,0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:SCALar <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the real part of impedance value for the differential port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Balanced port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<value> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
Examples |
CALC:FSIM:DRAF:ZCON:DIFF:BPOR2:SCAL
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:SCALer? |
Return Type |
Numeric |
1 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:LPORt<pnum>:COMPLex <real>,<img>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the complex impedance value for the differential mode port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Logical port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<real> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
<img> |
Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18. |
Examples |
CALC:FSIM:DRAF:ZCON:DIFF:LPOR2:COMPL
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:LPORt<pnum>:COMPlex? |
Return Type |
Comma-separated numeric |
0,0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential::LPORt<pnum>:SCALar <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the real part of impedance value for the differential:mode port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
logical port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<value> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
Examples |
CALC:FSIM:DRAF:ZCON:COMM:LPOR2:DiFF
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential::LPORt<pnum>:SCALer? |
Return Type |
Numeric |
1 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:STATe <bool>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the common mode port impedance conversion function ON/OFF. Must also set the fixture simulator function to ON using CALC:FSIM:STAT. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
State of the differential port impedance conversion function. Choose from OFF (or 0) Differential port impedance conversion OFF ON (or 1) Differential port impedance conversion ON |
Examples |
CALC:FSIM:DRAF:ZCON:COMM:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:STATe? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:COMPLex <real>,<img>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the complex impedance value for the common mode port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Balanced port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<real> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
<img> |
Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18. |
Examples |
CALC:FSIM:DRAF:ZCON:COMM:BPOR2:COMPL
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:COMPlex? |
Return Type |
Comma-separated numeric |
0,0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:SCALar <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the real part of impedance value for the common mode port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Balanced port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<value> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
Examples |
CALC:FSIM:DRAF:ZCON:COMM:BPOR2:SCAL
200 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:SCALer? |
Return Type |
Numeric |
1 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:COMPLex <real>,<img>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the complex impedance value for the common mode port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Logical port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<real> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
<img> |
Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18. |
Examples |
CALC:FSIM:DRAF:ZCON:COMM:LPOR2:COMPL
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:COMPlex? |
Return Type |
Comma-separated numeric |
0,0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:SCALar <value>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the real part of impedance value for the common mode port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
logical port number. Choose from 1 to 999. Note: See Balanced port versus Logical port. |
<value> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
Examples |
CALC:FSIM:DRAF:ZCON:COMM:LPOR2:SCAL
200 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:SCALer? |
Return Type |
Numeric |
1 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:STATe <bool>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the single-ended impedance conversion function ON/OFF. Must also set the fixture simulator function to ON using CALC:FSIM:STAT. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Port number. Choose from 1 to 999. |
<bool> |
State of the single-ended port impedance conversion function. Choose from OFF (or 0) single-ended port impedance conversion OFF ON (or 1) single-ended port impedance conversion ON |
Examples |
CALC:FSIM:DRAF:ZCON:SEND:PORT3:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT:STATe? |
Return Type |
Boolean |
ON |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORTpnum>:COMPLex <real>,<img>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the complex impedance value for the single-ended port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Pport number. Choose from 1 to 999. |
<real> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
<img> |
Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18. |
Examples |
CALC:FSIM:DRAF:ZCON:SEND:POR2:COMPL
200,10 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:COMPlex? |
Return Type |
Comma-separated numeric |
0,0 |
|
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:SCALer <val>
Applicable Models: E505xA with VNA ports (Read-Write) Sets the real part of impedance value for the single-ended port impedance conversion function. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<pnum> |
Pport number. Choose from 1 to 999. |
<val> |
Real part of the Impedance value in Units. Choose a number between 0 and 1E18 |
Examples |
CALC:FSIM:DRAF:ZCON:SEND:PORT:SCAL
0 |
Query Syntax |
CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:SCALer? |
Return Type |
Numeric |
1 |
|