Sense:Class Command


SENSe:CLASs:

NAME?

Click on a keyword to view the command details.

See Also


SENSe<cnum>:CLASs:NAME?

Applicable Models: E505xA with VNA ports

(Read-only) Returns the measurement class name of the specified channel. Use CALCulate:MEASure:DEFine and CALCulate:MEASure:PARameter commands to create measurements.

Parameters

 

<cnum>

Any existing channel number; if unspecified, value is set to 1.

Examples

SENS:CLAS:NAME?
sense2:class:name?

For a standard S-Parameter channel, returns...
"Standard"

Default

Not applicable