Front Panel: Names and Functions of Parts

 

Ground Terminal

Ground terminal is provided with the E5061B and is connected to the chassis of the E5061B. You can connect a banana-type plug to this terminal for grounding.

Hardkeys

ACTIVE CH/TRACE Block

A group of keys for selecting active channels and traces. For more on the concepts of channels and traces, see Setting Channels and Traces.

Hardkey Name

Description

Channel Next

Selects the next channel as the active channel. (Each time the key is pressed, the active channel steps up from the current channel to the channel with one number larger than the current channel number). A channel must be active before you can define such parameters as the sweep range. To change the settings of a channel, use this key to first make the channel active.

Channel Prev

Selects the previous channel as the active channel. (Each time the key is pressed,the active channel steps down from the current channel to the channel with one number smaller than the current channel number).

Trace Next

Selects the next trace as the active trace. (Each time the key is pressed, the active trace steps up from the current trace to the trace with one number larger than the current trace number). A trace must be active before you can define measurement parameters and other settings. To change the settings of a trace, use this key to first make the trace active.

Trace Prev

Selects the previous trace as the active trace. (Each time the key is pressed, active trace steps down from the current trace to the trace with one number smaller than the current trace number).

ENTRY Block

A group of keys used for entering numeric data is provided on the front panel of the E5061B.

Hardkey Name

Description

0, 1,  2, 3 ..... 9 , .
Keys (numeric keys)

Type numeric characters or a decimal point at the position of the cursor in the data entry area.

+/-

 +/- alternately changes the sign (+, - ) of a numeric value in the data entry area.

G/n, M/u, k/m,  x1 
 

Adds a prefix to the numeric data typed by using the numeric key and +/- key. One of the two prefixes written on the surface of the key is automatically selected depending on the parameter to be entered. x1 is entered without a prefix.

Softkey On/Off , Entry Off

Turns off the data entry bar if it is displayed. If the dialog box is displayed, it cancels the entry and closes the dialog box. If the data entry bar and dialog box are not displayed, it turns the softkey menu display on/off.

Bk Sp

Backspace key.

Foc

Changes the selection (focus) among the objects to be manipulated by the NAVIGATION Block keys and ENTRY Block keys. The objects to be manipulated by the NAVIGATION Block keys and ENTRY Block keys include softkey menus, data entry areas, tables (e.g., segment tables, limit tables, and marker tables), and dialog boxes. When two or more of these objects are displayed on the screen and need selecting, use this key to change the selection (focus) among the objects to be manipulated. When a softkey menu is selected, the menu name area at the top of the menu is displayed in blue. When a data entry area is selected, the data entry bar is displayed in blue. When a table is selected, the frame of the table window is displayed in light gray. While a dialog box is displayed, the focus is fixed on the dialog box and cannot be changed.

Help

Displays help for E5061B.

INSTR STATE Block

A group of keys related to the macro function, store and call function, control/management function, and presetting of the E5061B (returning it to the preset state).

Hardkey Name

Description

Macro Setup

Displays the Macro Setup Menu in Softkey Menu Bar. Manipulating the Macro Setup Menu enables you to start up the VBA editor or to create, call, or store a VBA project.

Macro Run

Executes a VBA procedure called "main" that has a VBA module named Module1.

Macro Break

Stops the VBA procedure being executed.

Save/Recall

Displays the Save/Recall Menu in Softkey Menu Bar. Manipulating the Save/Recall Menu enables you to store the setup conditions to or read from the storage devices, calibration data, and trace data of the analyzer.

Capture/System

First, temporarily saves the data for the image displayed on the LCD screen the moment this key is pressed to the internal memory (clipboard). Immediately after that, displays the System Menu in Softkey Menu Bar. Manipulating the System Menu enables you to define the setup for the limit test and then execute it, or to define the setup for the control and management of the analyzer. Using the Dump Screen Image option enables you to store the image data in the clipboard to a file on the storage devices. Also, using the Print option in the System menu enables you to print the image data in the clipboard to a printer.

Preset

Displays the Preset Menu in Softkey Menu Bar. Clicking OK in the Preset Menu enables you to return the analyzer to the initial setup state, called the preset setup.

MKR/ANALYSIS Block

A group of keys used for analyzing the measurement results by using the markers and etc.

Hardkey Name

Description

Marker

Displays the Marker Menu in Softkey Menu Bar. Manipulating the Marker Menu enables you to turn the markers on/off and move them by entering stimulus values. You can place up to 10 markers on each trace.

Marker Search

Displays the Marker Search Menu in Softkey Menu Bar. Manipulating the Marker Search Menu enables you to move a marker to a specific point (maximum, minimum, peak, and a point with a target value) on a trace. You can also find the bandwidth parameters (up to six) and display them.

Marker Fctn

Displays the Marker Function Menu in Softkey Menu Bar. Manipulating the Marker Function Menu enables you to not only specify the marker sweep range and the coupling of markers on a channel but also to display statistics data on traces.

Analysis

Displays the Analysis Menu in Softkey Menu Bar. Manipulating the Analysis Menu enables you to use the analytical function of the fault location, the SRL, and each limit test.

NAVIGATION Block (No Label on Front Panel)

The keys and Rotary knob in the NAVIGATION Block are used to navigate between softkey menus, tables (limit table, segment table, etc.), or selected (highlighted) areas in a dialog box as well as to change a numeric value in the data entry area by stepping up or down. When selecting one of two or more objects (softkey menus, data entry areas, etc.) to manipulate with the NAVIGATION Block keys displayed on the screen, first press the Foc (Focus) key in the ENTRY Block to select the object to be manipulated (placing focus on the object) and then manipulate the NAVIGATION Block keys (knob) to move among selected (highlighted) objects or change numeric values.

The following descriptions show how the NAVIGATION Block keys work both when the focus is on a softkey menu and when the focus is on the data entry area. For more on tables and dialog boxes manipulation, refer to the manipulation procedure for each of these functions.

RESPONSE Block

A group of keys used mainly for setting up response measurements on the E5061B.

Hardkey Name

Description

Channel Max

Changes between normal and maximum display of the active channel window. In normal display, all of the defined channel windows (both active and non-active) are displayed in split views on the screen. In maximum display, only the active channel window is displayed over the entire area, with non-active windows not displayed. To maximize the active channel, double-click the channel window frame. Measurements are also carried out on the non-active channels that are not displayed.

Trace Max

Changes between normal and maximum display of the active trace window. In normal display, all of the defined trace windows (both active and non-active) are displayed in split views on the screen. In maximum display, only the active trace is displayed over the entire channel window, with non-active traces not displayed. To maximize the trace, double-click anywhere in the channel window. Measurements are also carried out on the non-active traces that are not displayed.

Meas

 

Displays the Measurement Menu in Softkey Menu Bar. Manipulating the Measurement Menu enables you to specify the measurement parameters (types of S-parameters) for each trace.

Format

Displays the Format Menu in Softkey Menu Bar. Manipulating the Format Menu enables you to specify the data format (data transformation and graph formats) for each trace.

Scale

Displays the Scale Menu in Softkey Menu Bar. Manipulating the Scale Menu enables you to specify the scale for displaying a trace (magnitude per division, value of the reference line, etc.) for each trace. You can also specify the electrical delay and phase offset for each trace.

Display

Displays the Display Menu in Softkey Menu Bar. Manipulating the Display Menu enables you to specify the number of channels and the channel window array, the number and arrangement of traces, the setup for data math, etc.

Avg

Displays the Average Menu in Softkey Menu Bar. Manipulating the Average Menu enables you to define the averaging, smoothing, and IF bandwidth.

Cal

Displays the Calibration Menu in Softkey Menu Bar. Manipulating the Calibration Menu enables you to turn the calibration and error correction on/off and change definitions for calibration kits.

STIMULUS Block

A group of keys for defining the stimulus values (signal sources and triggers).

Hardkey Name

Description

Start

Displays the data entry bar for specifying the start value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu for specifying the sweep range in Softkey Menu Bar.)

Stop

Displays the data entry bar for specifying the stop value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu in the same way as Start.)

Center

Displays the data entry bar for specifying the center value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu in the same way as Start.)

Span

Displays the data entry bar for specifying the span value of the sweep range in the upper part of the screen. (It also displays the Stimulus Menu in the same way as Start.)

Sweep Setup

Displays the Sweep Setup Menu in Softkey Menu Bar. Manipulating the Sweep Setup Menu enables you to specify the signal source power level, sweep time, number of points, sweep type, etc.

Trigger

Displays the Trigger Menu in Softkey Menu Bar. Manipulating the Trigger Menu enables you to specify the trigger mode and trigger source. You can specify the trigger mode for each channel.

LCD Screen

The E5061B is equipped with a 10.4-inch TFT color, touch-sensitive LCD screen for displaying traces, scales, settings, softkeys and other measurement related information. The touch screen LCD allows you to manipulate softkeys by touching the LCD screen directly with a finger. For more on the LCD screen, see Screen Area: Names and Functions of Parts.

Probe Power

The E5061B Option 3L5/3L4/3L3 comes with two ports that can be used to provide power to external probes. See the Data sheet for the voltage and maximum current.

Standby Switch

This switch can turn on/off the E5061B. The color on the button shows the status as shown below:

Indicator Color

Description

Green

Normal power on status.

Orange

Standby status.

Red

Illegal power on status.

To turn off the power of the E5061B, be sure to follow the steps described below:

  1. First, press this standby switch or send a shutdown command from the external controller to activate the shutdown process (the processing of software and hardware necessary to turn off the power supply). This will put the E5061B into the standby state.

  2. Next, if necessary, turn off power supply to the Power Cable Receptacle (to LINE) on the rear panel.

Test Ports

Port 1 and Port 2

Port 1 and Port 2 are for S-parameter measurement. Port 1 can apply DC Bias. While signals are being output from a test port, the yellow LED above the test port is lit.

LF Out, R and T Ports

LF Out, R and T Ports are for Gain-Phase measurement. LF Out is a source port and it can apply DC Bias on measurement signal. The R and T ports are receiver ports. The input impedance for R and T ports can be selected from 50 Ω or 1 MΩ.

LF Out can be used for DC voltage source during S parameter measurement.

The test ports comply with Installation Category I of IEC 61010-1.

USB Ports

Two USB (Universal Serial Bus) Ports are provided that can be used for connecting to ECal (Electronic Calibration) module, USB keyboard, USB mouse, USB memory or a printer. Connecting a designated ECal module to this port enables ECal measurements to be taken. Connecting a compatible printer to this port enables screen information on the E5061B to be printed. See Using USB for more detail.