:SENS<Ch>:CORR:COEF:SAVE

Type

Command

Syntax

:SENSe<Ch>:CORRection:COEFficient:SAVE

Description

This command enables the calibration coefficients depending on the selected calibration type from the writing calibration data.  

      • Enabling the calibration coefficients clears all the calibration data regardless of whether the data are used for the calculation and also clears the calibration type selections.

If you execute this command before all the calibration data needed for calculating the calibration coefficients are written, an error occurs and the command is ignored.

Examples

See Reading/Writing Error Coefficient.

Related Commands

:SENS:CORR:COEF

:SENS:CORR:COEF:METH:ERES

:SENS:CORR:COEF:METH:OPEN

:SENS:CORR:COEF:METH:SHOR

:SENS:CORR:COEF:METH:SOLT1

:SENS:CORR:COEF:METH:SOLT2

:SENS:CORR:COEF:METH:THRU

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.SENSE(ch).CORRECTION.COEFFICIENT.SAVE