This section describes the steps you should take when you believe the Keysight E5071C is operating improperly. The results of these simple investigative procedures may help you avoid the down-time and inconvenience of repair service. The troubleshooting instructions are divided into three categories.
When taking all solution but it does not work. Contact Keysight Technology's Customer Contact.
|
Symptom |
Solution |
|
Turning on (|) the standby switch does not start up the system. |
|
|
The system starts up, but it automatically shuts down immediately. |
Execute the system recovery. |
|
The system starts up, but it enters the service mode (The instrument status bar in the lower right part of the screen displays SVC in red). |
Execute the system recovery. |
|
The measurement screen appears after startup, but the date and time displayed on the instrument status bar in the lower right part of the screen differ greatly from the previous settings. |
Execute the system recovery. |
|
The measurement screen appears after startup, but the power-on test is failed, with Error Message 241 appearing against a red background in the instrument message/warning area in the lower left part of the screen. |
Execute the system recovery. |
|
It is not possible to lock the removable hard disk after replacing it with another one.
|
Confirm that the connector at the rear end of the HDD is the same as the original HDD. There are two types of connectors as shown in the following figure. If they are different, contact your Keysight service office.
|
|
Symptom |
Solution |
|
The Error Message "Port N receiver overload" (N denotes a port number) is Displayed. During the measurement of an amplifier, Error Messages 221 through 224 "Port N receiver overload" (N denotes a port number) are displayed. This error occurs when the input to a test port exceeds the maximum input level in the measurement of an amplifier. The measurement value obtained in such a case is not correct. In the worst case, a failure (damage to the receiver) may occur. |
|
|
A Clearly Abnormal Measurement Value The measurement value is not reproducible, or clearly abnormal. |
|
|
The System Cannot be Operated Manually (Front Panel Keys, Keyboard, Touch Screen and Mouse) The keyboard or mouse becomes inoperable. |
|
|
The front panel key or keyboard becomes inoperable. |
|
|
The touch screen becomes inoperable. |
|
|
The mouse becomes inoperable. |
|
|
All of the front panel keys, keyboard, and mouse become inoperable. |
|
|
The keyboard and mouse have been connected after power-on. |
|
|
The Screen Freezes and All Operations Become Impossible. The measurement in progress or screen update is stalled and all of the front panel keys, keyboard, mouse, and touch screen are inoperable. |
|
|
The System Freezes while in Operation.
|
|
|
The Rear Cooling Fan Does Not Operate.
|
|
|
The Sweep Action Stops during Measurement or Is Not Executed. An Error or Warning Message Appears. |
|
|
An error or warning message is displayed on the instrument message/warning area in the lower part of the screen |
|
|
All front panel keys except Trace Prev, Trace Next, Trace Max and ENTRY block are inoperable. |
|
|
Symptom |
Solution |
|
Cannot Output to a Printer Cannot output a measurement screen or data to a printer. Attempting to output to a printer causes Error Messages 120 and 121 to appear. |
|
|
Does Not Respond to an External Controller/Fails to Function Normally A GPIB device does not respond to the external controller, or fails to function normally. |
|
|
An ECal module can not be detected. |
When you install the firmware A.09.31 and below in the HDD revision CN960 and above, this symptom may occur. Follow the following steps.
|
|
The E5071C hung up when two (or more) ECals are connected/disconnected at the same time. |
When you install the firmware A.09.60 and above in the HDD revision CN954 and below, this symptom may occur. Follow the following steps.
|