Controls writing and reading VNA measurement data.
These commands are Superseded by the CALCulate:MEASure:DATA commands.
|
| CUSTom | CATalog? | MFData? | MSData? | SNP? | PORTs? | SAVE |
Click on a red keyword to view the command details.
Red is a superseded command.
See Also
To read receiver data, use CALC:RDATA?
To read error terms, use SENS:CORR:CSET:DATA
To read SnP measurement data, use CALC:DATA:SNP?
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Reads or writes Measurement data, Memory data, or Normalization Divisor data from the Data Access Map location.
Equation Editor Notes:
Note: The Calc:Data SCORR command to read / write error terms is Superseded with SENS:CORR:CSET:DATA. SCORR commands do NOT accommodate greater than 12 error terms. |
||
|
Parameters |
|
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
|
<char> |
FDATA |
Formatted measurement data to or from Data Access Map location Display (access point 2). Note: When querying FDATA, data is received in degrees. When setting phase using FDATA, the command expects the data in radians.
|
|
|
RDATA |
Complex measurement data. Writes data to Data Access Map location Raw Measurement (access point 0).
Reads data from Data Access Map location Raw Measurement (access point 0).
|
|
|
SDATA |
Complex measurement data. Writes data to Data Access Map location Raw Measurement (access point 0).
Reads data from Apply Error Terms (access point 1).
|
|
|
FMEM |
Formatted memory data to or from Data Access Map location Memory result (access point 4).
|
|
|
SMEM |
Complex measurement data to or from Data Access Map location Memory (access point 3).
|
|
|
SDIV |
Complex data from Data Access Map location Normalization (5).
|
The following Calc:Data SCORR command to read / write error terms is Superseded with SENS:CORR:CSET:DATA. These SCORR commands do NOT accommodate greater than 12 error terms.
|
For 2-Port SOLT and TRL calibrations |
Specify this <char> |
to get or put this Error Term... |
|
SCORR1 |
Forward Directivity |
|
|
SCORR2 |
Forward Source Match |
|
|
SCORR3 |
Forward Reflection Tracking |
|
|
SCORR4 |
Forward Isolation |
|
|
SCORR5 |
Forward Load Match |
|
|
SCORR6 |
Forward Transmission Tracking |
|
|
SCORR7 |
Reverse Directivity |
|
|
SCORR8 |
Reverse Source Match |
|
|
SCORR9 |
Reverse Reflection Tracking |
|
|
SCORR10 |
Reverse Isolation |
|
|
SCORR11 |
Reverse Load Match |
|
|
SCORR12 |
Reverse Transmission Tracking |
|
EXAMPLE CALC:DATA FDATA,Data(x) See another example using this command. |
|
Return Type: Block data |
|
Default - Not Applicable |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Note: This command has been replaced by CALC:DATA: which can now be used with all VNA applications. (Read-Write) Reads or writes data from a custom-named measurement buffer. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<name> |
Name of the buffer to be read or written |
|
<data> |
Data to be read or written to the custom buffer. Format as one number per data point. |
|
Examples |
CALC:DATA:CUST 'VectorResult0',0,1,2,3,4,5 'Write CALC:DATA:CUST? 'VectorResult0' 'Read |
|
Query Syntax |
CALCulate:DATA:CUSTom? <name> |
|
Return Type |
Depends on Form:Data |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Note: This command has been replaced by CALC:DATA:CAT which can now be used with all VNA applications. (Read-only) Reads the list of buffer names (comma separated list of string values) available from the selected parameter. Specify the measurement using CALCulate:PARameter:SELect. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:DATA:CUST:CAT? calculate:data:custom:catalog? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-only) Gets the formatted data array of multiple traces (traces-n, m, .... to l) of the selected channel. This command gets multiple trace data with one command, while CALC:MEAS:DATA:FDAT returns only one trace with one command. Note: If valid data is not calculated because of the invalid measurement, “1.#QNB” is read out. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<measList> |
Trace number. "n, m, l, ..." where n, m, l are 1 to the maximum trace number. Note: Use comma for separator of trace number. |
|
Examples |
CALC:DATA:MFD? "1,2" |
|
Return Type |
Data Block |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-only) Gets the corrected data array of multiple traces (traces-n, m, .... to l) of the selected channel. This command is allows to get several corrected data with one command, while CALC:MEAS:DATA:SDAT returns only one corrected data with one command. Note: If valid data is not calculated because of the invalid measurement, “1.#QNB” is read out. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<measList> |
Trace number. "n, m, l, ..." where n, m, l are 1 to the maximum trace number. Note: Use comma for separator of trace number. |
|
Examples |
CALC:DATA:MSD? "1,2" |
|
Return Type |
Data Block |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Note: This command has been replaced by CALC:DATA:SNP:PORTs? (Read-only) Reads SnP data from the selected measurement. Learn more about SnP data. This command is valid ONLY with standard S-parameter measurements.
|
||
|
Parameters |
|
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
|
<n> |
Amount of data to return. If unspecified, <n> is set to 2. The number you specify must be less than or equal to the number of available ports on the VNA. Choose from: 1 (S1P) returns 1-Port data for the active measurement if the active measurement is a reflection parameter such as S11 or S22. The behavior is UNDEFINED if the active measurement is a transmission parameter such as an S21. 2 (S2P) returns data for the four 2 port parameters associated with the current measurement. Default. Data that is not available is zero-filled. 3 (S3P) returns data for the nine 3 port parameters associated with the current measurement. Data that is not available is zero-filled. 4 (S4P) returns data for the sixteen 4 port parameters associated with the current measurement. Data that is not available is zero-filled. SnP data can be output using several data formatting options. See MMEM:STORe:TRACe:FORMat:SNP. See also MMEM:STOR <file>.<snp> |
|
|
Examples |
CALC:PAR:DEF MyMeasurement, S11 CALC:PAR:SEL MyMeasurement CALC:DATA:SNP? 1 |
|
|
Return Type |
Depends on FORMat:DATA. |
|
|
Not Applicable |
||
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Note: This command replaces CALC:DATA:SNP?. This command is more explicit regarding the data to be returned, and works for VNAs with multiport test sets. (Read-only) Reads SNP data from the selected measurement for the specified ports. Learn more about SNP data. This command is valid ONLY with standard S-parameter measurements.
|
||
|
Parameters |
|
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
|
<"x,y,z"> |
Comma or space delimited port numbers for which data is requested, enclosed in quotes. SNP data can be output using several data formatting options. See MMEM:STORe:TRACe:FORMat:SNP. |
|
|
Examples |
CALC:DATA:SNP:PORTs? "1,2,4,5,7" 'read data for these ports |
|
|
Return Type |
Depends on FORMat:DATA |
|
|
Not Applicable |
||
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Note: This command replaces MMEM:STOR sNp. This command is more explicit regarding the data to be saved, and works for VNAs with multiport test sets. (Write-only) Saves SNP data from the selected measurement for the specified ports. Learn more about SNP data.
|
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<"x,y,z"> |
String Comma or space delimited port numbers for which data is requested, enclosed in quotes. |
|
<filename> |
String Path, filename, and suffix of location to store the SNP data, enclosed in quotes. The suffix is not checked for accuracy. If saving 2 ports, specify "filename.s2p"; If saving 4 ports, specify "filename.s4p.", and so forth. SNP data can be output using several data formatting options. See MMEM:STORe:TRACe:FORMat:SNP. |
|
Examples |
CALC:DATA:SNP:PORTs:Save '1,2,4','D:\MyData.s3p';*OPC? |
|
Return Type |
Depends on FORMat:DATA |
|
Not Applicable |
|
|
(Read-only) Returns receiver data for the selected measurement. To query measurement data, see CALC:DATA? Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<char> |
Choose from any physical receiver in the VNA. For example: "A" Also, REF - returns data for either R1 or R2 data depending on the source port of the selected measurement. See the block diagram showing the receivers in VNA. Note: Logical receiver notation is NOT allowed with this command. Learn more. |
|
Example |
INITiate:CONTinuous OFF CALCulate:RDATA? REF |
|
Return Type |
Depends on FORM:DATA command - Two numbers per data point |
|
Not Applicable |
|
Notes:
Generally when you query the analyzer for data, you expect that the number of data values returned will be consistent with the number of points in the sweep.
However, if you query receiver data while the instrument is sweeping, the returned values may contain zeros. For example, if your request for receiver data is handled on the 45th point of a 201 point sweep, the first 45 values will be valid data, and the remainder will contain complex zero.
This can be avoided by synchronizing this request with the end of a sweep or putting the channel in hold mode.
Learn about Unratioed Measurements