Gain Compression Analysis Commands


Sets and reads Gain Compression Analysis controls.

These commands are Superseded by the CALCulate:MEASure:GCMeas commands.

CALCulate:GCMeas:ANALysis

CWFRequency

ENABle

ISDisfreq

XAXis

Click on a keyword to view the command details.

Other Gain Compression commands

The calibration commands listed in this topic are supplemental to the Guided Cal commands.

See Also


CALCulate<cnum>:GCMeas:ANALysis:ENABle <bool>

Applicable Models: N522xB, N524xB, M9485A, E5080A

(Read-Write)  Enables and disables a compression analysis trace.

Parameters

 

<cnum>

Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1.

<bool>

ON (or 1) - Enable compression analysis.

OFF (or 0) - Disable compression analysis.

Examples

CALC:GCM:ANAL:ENAB ON
calculate2:gcmeas:analysis:enable off

Query Syntax

CALCulate<cnum>:GCMeas:ANALysis:ENABle?

Return Type

Boolean (1 = ON, 0 = OFF)

Default

OFF


CALCulate<cnum>:GCMeas:ANALysis:CWFRequency <num>

Applicable Models: N522xB, N524xB, M9485A, E5080A

(Read-Write)  Set and return the CW frequency for a compression analysis trace.

Parameters

 

<cnum>

Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1.

<num>

CW frequency in Hz. Choose a frequency within the range of the gain compression channel.

Examples

CALC:GCM:ANAL:CWFR 1e9
calculate2:gcmeas:analysis:cwfrequency 1e10

Query Syntax

CALCulate<cnum>:GCMeas:ANALysis:CWFRequency?

Return Type

Numeric

Default

Not Applicable


CALCulate<cnum>:GCMeas:ANALysis:DISCrete | ISD[:STATe] <bool>

Applicable Models: N522xB, N524xB, M9485A, E5080A

(Read-Write)  Sets and returns whether the CW frequency for the compression analysis trace can be set to only the discrete frequencies or provides interpolation.

Parameters

 

<cnum>

Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1.

<bool>

ON (or 1) - Discrete data points only.

OFF (or 0) - Interpolated data points.

Examples

CALC:GCM:ANAL:ISD ON
calculate2:gcmeas:analysis:isdisfrequency off

Query Syntax

CALCulate<cnum>:GCMeas:ANALysis:ISDisfrequency?

Return Type

Boolean (1 = ON, 0 = OFF)

Default

OFF


CALCulate<cnum>:GCMeas:ANALysis:XAXis <char>

Applicable Models: N522xB, N524xB, M9485A, E5080A

(Read-Write)  Sets and returns the type of data to display on the x-axis of a compression analysis trace.

Parameters

 

<cnum>

Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1.

<bool>

Data to display on X-axis. Choose from:

  • PIN - Input power to the DUT.

  • PSOurce - power from the source.

Examples

CALC:GCM:ANAL:XAX PIN
calculate2:gcmeas:analysis:xaxis psource

Query Syntax

CALCulate<cnum>:GCMeas:ANALysis:XAXis?

Return Type

Character

Default

PIN