The following commands are sent as a string argument from:
CONTrol:CALPod:COMMand <string>
|
CALPod INITialize | ACTive | ALL RECorrect | ACTive | ALL |
Click on a blue keyword to view the command details.
In addition to the above Calpod commands, the following IEE 488 Common Commands can also be sent as a string argument:
*CLS - Clears all errors and event data from the error/event queue.
*IDN? - Returns the instrument identification information.
*OPC? - Operation complete query. This query immediately returns a value, independent of whether or not the operation is complete. A return value of 0 indicates the operation is not complete. A value of +1 indicates the operation is complete. Typically this command is used in a loop with a 0.25 second delay when waiting for an operation to complete.
*TST? - Performs a communication test on all the currently enabled Calpods. 0 = Test failed on one or more enabled Calpods. 1 = All enabled Calpods working.
SYSTem:ERRor? - Queries the Event/Error queue and returns the most recent error element.
Important Notes
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, E5080A, P937xA (Write-only) Unassign Calpod serial number from the specified VNA port. |
|
|
Parameters |
|
|
<port> |
VNA port number to un-assign. |
|
Examples |
CONT:CALP:COMM 'CALP:DIS 2' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-read) Assign or return the Calpod serial number for the specified VNA port. If a Calpod module is already assigned to the specified VNA port, this assignment will replace the existing assignment. |
|
|
Parameters |
|
|
<port> |
VNA port number to be assigned the Calpod serial number. |
|
<sn> |
Calpod serial number. |
|
Examples |
CONT:CALP:COMM 'CALP:ENAB 2, 0001234' 'WRITE CONT:CALP:COMM? 'CALP:ENAB? 2' 'READ |
|
Query Syntax |
CONTrol:CALPod:COMMand? 'CALPod:ENABle? <port>' |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Hides the Calpod setup dialog. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:HIDE' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Performs the initialize process for the active (selected) channel. Select a channel using CALCulate:MEASure:PARameter. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:INIT:ACT' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Performs the initialize ALL channels process. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:INIT:ALL' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Starts the Calpod software. The Calpod software can be started using this (Launch) command or by activating the Calpod user interface. Once the Calpod software is started it remains active until the VNA application is terminated. Send this command first in your program, then wait a couple seconds while the software starts before sending the next command. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:LAUN' wait 3 |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Performs the recorrect process for the active (selected) channel. Select a channel using CALCulate:MEASure:PARameter. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:REC:ACT' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Performs the recorrect process for ALL channels. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:REC:ALL' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Shows the Calpod setup dialog. |
|
|
Parameters |
None |
|
Examples |
CONT:CALP:COMM 'CALP:SHOW' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Write-only) Sets the specified Calpod module to specified impedance state. |
|
|
Parameters |
|
|
<sn> |
Serial number of the Calpod module. When set to 1, all modules are set to the specified state. |
|
<state> |
Impedance state. Not case sensitive. Choose from: Short, Open, Load, or Thru |
|
Examples |
CONT:CALP:COMM 'CALPod:STATe 0001234,thru' |
|
Query Syntax |
Not Applicable |
|
Thru |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA E5080A, P937xA (Read-only) Returns the temperature of the specified Calpod module in degrees Celsius. |
|
|
Parameters |
|
|
<sn> |
Serial number of the Calpod module. |
|
Examples |
CONT:CALP:COMM? 'CALPod:TEMP? 0001234' |
|
Query Syntax |
Not Applicable |
|
Return Type |
String |
|
Not Applicable |
|