Specifies the settings to remotely control the rear panel connectors, an external test set, Calpod modules, and ECal Module state.
|
CONTrol CHANnel:INTerface:CONTrol: | [STATe] ECAL:MODule: | PATH: | COUNt? | STATe | STATe EXTernal:TESTset - More Commands | TRIGger | ATBA | |
Click on a keyword to view the command details.
Blue command is superseded.
See Also
External Test Set IO connector
Material Handler IO connector
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, E5080A, P937xA (Write-Read) Sends commands that control a Calpod module. Reads query versions Calpod commands. See ALL Calpod commands. |
|
|
Parameters |
|
|
<string> |
Calpod command. See ALL Calpod commands that can be used in this string. |
|
Write Example |
CONT:CALP:COMM 'CALP:INIT:ACT' 'Enclose all strings in SINGLE quotes (NOT double quotes) |
|
Query Syntax |
CONTrol:CALPod:COMMand? <string> Relevant only for query strings. |
|
Read Example |
CONT:CALP:COMM? '*OPC?' 'returns 0 if the calpod software is currently processing an operation 'returns 1 if operations are complete |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A (Write-only) Recalls an Interface Control configuration file. Learn more about Interface Control. |
|
|
Parameters |
|
|
<string> |
File name and extension (.xml) of the configuration file to recall. Files are typically stored in the default folder "D:\". To recall from a different folder, specify the full path name. |
|
Examples |
CONT:CHAN:INT:CONT:CONF:REC 'MyConfigFile.xml' control:channel:interface:control:config:recall:state 'D:\MyFile.xml' |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A (Read-Write) Enables and disables ALL Interface Control settings. To send data, the individual interfaces must also be enabled. Learn more about Interface Control. |
|
|
Parameters |
|
|
<bool> |
Boolean OFF (0) - Interface Control is disabled;NO control data is sent. ON (1) - Interface Control is enabled. |
|
Examples |
CONT:CHAN:INT:CONT 1 control:channel:interface:control:state 0 |
|
Query Syntax |
CONTrol:CHANnel:INTerface:CONTrol[:STATe]? |
|
Return Type |
Boolean |
|
OFF (0) |
|
|
Applicable Models: All (Read-only) Returns the number of unique states that exist for the specified path name on the selected ECal module. This command performs exactly the same function as SENS:CORR:CKIT:ECAL:PATH:COUNt? Use the CONT:ECAL:MOD:PATH:STAT command to set the module into one of those states. Use SENS:CORR:CKIT:ECAL:PATH:DATA? to read the data for a state. |
|
|
Parameters |
|
|
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
|
<name> |
Name of the path for which to read number of states. Choose from: Reflection paths
Transmission paths
Note: For each transmission path, the first of the available states is the through state, the second is the confidence (attenuator) state. |
|
Examples |
CONT:ECAL:MOD:PATH:COUNt? A control:ecal:module2:path:count? cd |
|
Return Type |
Integer |
|
Not Applicable |
|
|
Applicable Models: All (Write-only) Sets the internal state of the selected ECAL module. This command supersedes CONT:ECAL:MOD:STAT.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Parameters |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<path> |
Path name for which to set a state. Note: The impedance paths are not independent. For example, changing the impedance presented on path A will cause a change to the impedance on path B. Choose from: Reflection paths
Transmission paths
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<stateNum> |
Number of the state to set. Refer to the following table to associate the <stateNum> with a state in your ECal module. In addition, CONT:ECAL:MOD:PATH:COUNt? returns the number of states in the specified ECal module.
** The following modules have only FOUR Impedance states (1, 2, 3, 4): N4690B ,N4691B ,N4692A ,N4696B, N7550A - N7556A. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Examples |
CONT:ECAL:MOD:PATH:STATe A,5 control:ecal:module2:state BC,1 |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Query Syntax |
Not Applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Not Applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA This command is replaced with CONT:ECAL:MOD:PATH:STATe. (Write-only) Sets the internal state of the selected ECAL module. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Parameters |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:COLL:CKIT:INF? to verify their identity. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<value> |
Integer code for switching the module. The following are codes for Keysight ECal modules.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Examples |
CONT:ECAL:MOD:STAT 36 |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Query Syntax |
Not Applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Not Applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Applicable Models: E5080A
|
(Read-Write) Sets or returns the output port data for specified group with id of the E5092A multiport test set. Notes: This command is available only for E5092A multiport test set. |
|||||||||||||||||||
|
Parameters |
|
||||||||||||||||||
|
<id> |
Id of the multiport test set either 1 or 2. If unspecified, Id is assumed to be 1. |
||||||||||||||||||
|
<grp> |
A | B | C | D |
||||||||||||||||||
|
<num> |
An integer specifying the decimal value of the control line. Values are obtained by adding weights from the following table that correspond to individual lines. The output port data range is between 0 to 255 (0=All line are turns OFF and 255 all lines are turn ON).
|
||||||||||||||||||
|
Examples |
CONT:MULT1:OUTP:B 8 |
||||||||||||||||||
|
Query Syntax |
CONTrol:MULTiplexer<id>:OUTPut:<grp>[:DATa]? |
||||||||||||||||||
|
Return Type |
Numeric |
||||||||||||||||||
|
0 |
|||||||||||||||||||
Applicable Models: E5080A
|
(Read-Write) Sets or returns the output voltage for specified group with id of the E5092A multiport test set. Notes: This command is available only for E5092A multiport test set. |
|
|
Parameters |
|
|
<id> |
Id of the multiport test set either 1 or 2. If unspecified, Id is assumed to be 1. |
|
<grp> |
A | B | C | D |
|
<volt> |
Output voltage range for <grp> is between 0 to 5.2V and resolution is 10mV. |
|
Examples |
CONT:MULT1:OUTP:B:VOLT 4.2 |
|
Query Syntax |
CONTrol:MULTiplexer<id>:OUTPut:<grp>:VOLtage[:DATa]? |
|
Return Type |
Numeric |
|
0 V |
|
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Set and read the noise source (28V) ON and OFF. |
|
|
Parameters |
|
|
<bool> |
Boolean OFF (0) - Noise Source OFF ON (1) - Noise Source ON |
|
Examples |
CONT:NOIS:SOUR 1 control:noise:source:state 0 |
|
Query Syntax |
CONTrol:NOISe:SOURce[:STATe]? |
|
Return Type |
Boolean |
|
For VNA models with a Noise Figure option (028/029/H29), the 28V line is ON at application start and after a preset. The ON/OFF state is also available from a VNA softkey menu. For VNA models WITHOUT a Noise Figure option (028/029/H29), the 28V line is OFF at application start and its state is not affected by a preset. The ON/OFF state is NOT available from a VNA softkey menu. |
|
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Configures external triggering in the VNA. Note: To configure external triggering in the current VNA models, use the Trigger commands.
|
|
|
Parameters |
|
|
<conn> |
Rear Panel connector to send or receive trigger signals. Choose from: BNC1 Trigger IN from rear-panel Trigger IN BNC connector Note: Only one of the input connectors is active at a time. When a command is sent to one, the VNA automatically makes the other INACTIVE. BNC2 Trigger OUT to rear-panel Trigger OUT BNC connector. MATHtrigger - Trigger IN from rear-panel Material Handler connector Pin 18 RDY - Ready for trigger OUT.
|
|
<char> |
INACTIVE - Disables the specified connector <conn>. Choose from ONLY the following when <conn> is set to BNC1 or AUXT or MATHtrigger:
Choose from ONLY the following when <conn> is set to BNC2: Use CONTrol:SIGNal:TRIGger:OUTP to enable the BNC2 output. The following selections send a positive or negative pulse before or after each trigger acquisition. This normally occurs each sweep unless a channel is in point trigger mode.
Choose from ONLY the following when <conn> is set to RDY:
|
|
Examples |
CONT:SIGN BNC1,TIENEGATIVE CONT:SIGN RDY,LOW |
|
Query Syntax |
CONTrol:SIGNal? <conn> In addition to the arguments listed above, the following is also a possible returned value: NAVAILABLE - This feature is not available on this VNA |
|
Return Type |
Character |
|
At Preset: BNC1 = INACTIVE When Output is enabled: BNC1 = INACTIVE |
|
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Accept Trigger Before Armed Determines what happens to an EDGE trigger signal if it occurs before the VNA is ready to be triggered. (LEVEL trigger signals are always ignored.) For more information, see External triggering. |
|
|
Parameters |
|
|
<bool> |
Boolean OFF (0) - A trigger signal is ignored if it occurs before the VNA is ready to be triggered. ON (1) - A trigger signal is remembered and then used when the VNA becomes armed (ready to be triggered). The VNA remembers only one trigger signal. |
|
Examples |
CONT:SIGN:TRIG:ATBA 0 |
|
Query Syntax |
CONTrol:SIGNal:TRIGger:ATBA? |
|
Return Type |
Boolean |
|
OFF |
|
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Output Enabled The VNA can be enabled to send trigger signals out the rear-panel TRIGGER OUT BNC connector. Use CONTrol:SIGNal to configure for output triggers. Note: To configure external triggering in the current VNA models, use the Trigger commands. For more information, see External triggering. |
|
|
Parameters |
|
|
<bool> |
Boolean OFF (0) - VNA does NOT output trigger signals. ON (1) - VNA DOES output trigger signals. |
|
Examples |
CONT:SIGN:TRIG:OUTP 1 control:signal:trigger:outp OFF |
|
Query Syntax |
CONTrol:SIGNal:TRIGger:OUTP? |
|
Return Type |
Boolean |
|
OFF |
|