These commands, along with the standard Guided commands, performs a SMC calibration on a frequency converting device.
Note: These commands replace the SENSe:CORRectionCOLLect:Session:SMC commands. These commands allow the entire SMC cal to be performed from the Guided cal interface.
These commands are also used to perform a GCx Calibration. See an example.
|
SENSe:CORRectionCOLLect:GUIDed:SMC FSIMulator | NETWork | FILename | MODE PHASe | DELay | METHod | MIXer PWRCal | CANCel | RECeiver | SEParate |
Click on a red keyword to view the command details.
Red keywords are obsolete.
See Also
NOTE: To configure a power meter and sensor see SOURce:POWer: commands.
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-Write) Specifies the S2P filename to embed or de-embed on the input or output of your mixer measurement. Learn more. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<p> |
Apply network to input or output of mixer. Choose from: 1 - Input of mixer 2 - Output of mixer |
|
<string> |
Filename of the S2P used for embedding or de-embedding. Use the full path name, file name, and .S2P suffix, enclosed in quotes. |
|
Examples |
SENS:CORR:COLL:GUID:SMC:FSIM:NETW1:FIL "D:\WaveguideAdapt.S2P" |
|
Query Syntax |
SENS<ch>:CORRection:COLLect:GUIDed:SMC:FSIMulator:NETWork<x>:FILename? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-Write) Allows you to embed (add) or de-embed (remove) circuit network effects on the input and output of your mixer measurement. Learn more. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<p> |
Apply network to input or output of mixer. Choose from: 1 - Input of mixer 2 - Output of mixer |
|
<char> |
Choose from: NONE - Do nothing with effects of S2P file. EMBed - Add effects of S2P file from the measurement results. DEEMbed - Remove effects of S2P file from the measurement results. |
|
Examples |
SENS:CORR:COLL:GUID:SMC:FSIM:NETW1:MODE EMB |
|
Query Syntax |
SENS<ch>:CORRection:COLLect:GUIDed:SMC:FSIMulator:NETWork<x>:MODE? |
|
Return Type |
Character |
|
NONE |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Write-only) Imports Guided Power Cal or Phase Reference Cal into the current SMC calibrations. For the Guided Power Cal: The port of the mixer input must have the same source attenuator setting between the SMC channel and the Guided Power Cal Set. The frequencies of the Guided Power Cal must include all the mixer frequencies. Interpolation will be applied to the Guided Power Cal frequencies if they do not exactly match. For the Phase Reference Cal: The port of the mixer input must have the same source attenuator setting as used in the phase reference cal. The phase reference cal must include all the mixer frequencies. Interpolation will be applied to the phase reference cal frequencies if they do not exactly match. Learn more about Phase Reference Cal. The following error message may appear (it is not written to the VNA Error Log):
|
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<calName> |
(String) Name of existing Cal Set from which to import power data. |
|
<dataset> |
(String) Name of the data set. Choose from:
|
|
Examples |
SENS2:CORR:COLL:GUID:SMC:IMP "MyPowerCal","POWER_STEP" See example program SENS:CORR:COLL:GUID:SMC:IMP "MyPhaseRefCal","POWER_AND_PHASE" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-Write) Sets and returns whether or not the LO power cal step is included in the cal steps when an SMC or GCx cal is performed. Learn more. Set LO Power level for the calibration using SENS:CORR:COLL:GUID:PSEN1:POW:LEV. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<n> |
LO Stage. Choose 1. |
|
<bool> |
LO Power Cal state. Choose from: O or OFF - Skips over the LO Power Cal when calibrating. 1 or ON - Includes a step for LO Power Cal when calibrating |
|
Examples |
SENS:CORR:COLL:GUID:SMC:LO1:PCAL 0 |
|
Query Syntax |
SENSe<ch>:CORRection:COLLect:GUIDed:SMC:LO<n>:PCAL[:STATe] |
|
Return Type |
Boolean |
|
Default |
OFF or 0 |
|
Applicable Models: N522xB, N523xB, N524xB, P937xA (Read-Write) Set and return the known delay through the calibration mixer. Learn more. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Known delay through the calibration mixer in seconds. |
|
Examples |
SENS:CORR:COLL:GUID:SMC:PHAS:DEL 12e-9 sense2:correction:collect:guided:smc:phase:delay 12e-10 |
|
Query Syntax |
SENSe<ch>:CORRection:COLLect:GUIDed:SMC:PHASe:DELay? |
|
Return Type |
Numeric |
|
0 seconds |
|
|
Applicable Models: N522xB, N523xB, N524xB, P937xA (Read-Write) Set and return the method of setting the delay through the calibration mixer. Learn more. To select Phase Reference Cal method for correcting an SMC+Phase measurement, use SENS:CORR:COLL:GUID:SMC:IMPort |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Choose from: FIXed - use a known delay value set with SENS:CORR:COLL:GUID:SMC:PHAS:DEL MIXer - use the S2P file set with SENS:CORR:COLL:GUID:SMC:PHAS:MIX |
|
Examples |
SENS:CORR:COLL:GUID:SMC:PHAS:METH FIX sense2:correction:collect:guided:smc:phase:method mixer |
|
Query Syntax |
SENSe<ch>:CORRection:COLLect:GUIDed:SMC:PHASe:METHod? |
|
Return Type |
Character |
|
FIXed |
|
|
Applicable Models: N522xB, N523xB, N524xB, P937xA (Write-only) Set the filename of the S2P file used to characterize the calibration mixer. Learn more. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<string> |
Calibration mixer filename. Use the following rules to specify path names:
|
|
Examples |
SENS:CORR:COLL:GUID:SMC:PHAS:MIX "MyCalMixer.s2p" sense2:correction:collect:guided:smc:phase:mixer "MyCalMixer.s2p" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Write-only) Aborts a power cal. This command should be sent when a power cal is running. |
|
|
Parameters |
|
|
<ch> |
Channel number of the SMC cal being performed. If unspecified, value is set to 1 |
|
Examples |
SENS:CORR:COLL:GUID:SMC:PWRC:CANC |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-Write) Set whether to use the reference receiver for faster iteration during power cal or use a power meter. This command should be set during calibration setup. Learn more. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
OFF or 0 - Use a power meter only. ON or 1 - Use a power meter for the first reading and the reference receiver for all subsequent readings. |
|
Examples |
SENS:CORR:COLL:GUID:SMC:PWRC:REC 1 |
|
Query Syntax |
SENSe<ch>:CORRection:COLLect:GUIDed:SMC:PWRCal:RECeiver? |
|
Return Type |
Boolean |
|
ON or 1 |
|
|
Applicable Models: N522xB, N523xB, N524xB, E5080A, M948xA, P937xA (Read-Write) Specifies whether to use a Thru standard or to use two power sensor connections during the power cal of an SMC calibration. Note: This command must be sent BEFORE ALL other calibration commands. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<bool> |
OFF or 0 - Perform Cal with Thru standard. ON or 1 - Do NOT use a Thru, but instead perform separate power cals on Input and Output reference planes. |
|
Examples |
'The following is an example sequence of commands: SENS:CORR:COLL:GUID:SMC:PWRC:SEP 1 SENS:CORR:COLL:GUID:CONN:PORT1 "APC 3.5 female" SENS:CORR:COLL:GUID:CONN:PORT2 "APC 3.5 female" SENS:CORR:COLL:GUID:CONN:PORT3 "Not used" SENS:CORR:COLL:GUID:CONN:PORT4 "Not used" SENS:CORR:COLL:GUID:CKIT:PORT1 "N4691-60006 ECal 02638" SENS:CORR:COLL:GUID:CKIT:PORT2 "N4691-60006 ECal 02638" SENS:CORR:COLL:GUID:INIT |
|
Query Syntax |
SENSe<ch>:CORRection:COLLect:GUIDed:SMC:PWRCal:SEParate? |
|
Return Type |
Boolean |
|
OFF or 0 |
|