Performs and applies calibration and other error correction features.
To perform a Guided Calibration, use ONLY the Sens:Corr Coll:GUIDed commands.
To perform an Unguided Calibration, do NOT use the Sens:Corr:Coll:Guided commands.
See the "Unguided" example programs for clarification.
|
SENSe:CORRection CCHeck | DONE COLLect | APPLy | DISPlay:WINDow | AOFF | [STATe] | ISOLation: | METHod | PORT:SUBS: | FULL:VAL | RESet | STAT | SAVE | SESSion - More Commands | SWEep:CHANnel | AOFF | [STATe] GCSetup | POWer | SENSor: | CKIT IMPedance:INPut PREFerence | CALibration | CSET | SAVE | ECAL | PMAP RPOWer:OFFSet RVELocity | COAX SFOWard | [STATe] TSTandards | [STATe] TYPE | CATalog? |
Click on a Red keyword to view the command details.
Red commands are superseded.
See Also
Applicable Models: E5080A, M9485A
|
(Write-only) Reads the 'confidence data' associated with the specified ECal module and puts it into memory. The measurement is selected using SENS:CORR:CCH:PAR. This command is compatible with *OPC. Note: A confidence check can NOT be performed remotely from User Characterizations that are stored on the VNA disk. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
|
<mod> |
ECAL Module that contains the confidence data. Choose from: ECAL1 ..through.. ECAL50 |
|
[char] |
Optional argument. Specifies which characterization within the ECal module that the confidence data will be read from. CHAR0 Factory characterization (data that was stored in the ECal module by Keysight). Default if not specified. CHAR1 User characterization #1 CHAR2 User characterization #2 ...and so forth up to: CHAR12 User characterization #12 |
|
Examples |
SENS:CORR:CCHeck ECAL2 sense2:correction:ccheck:acquire ecal1,char1 |
|
Query Syntax |
Not applicable |
|
Not applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Concludes the Confidence Check and sets the ECal module back into the idle state. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:CORR:CCH:DONE |
|
Query Syntax |
Not applicable |
|
Not applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies an existing measurement to be used for the Confidence Check. Note: A confidence check can NOT be performed remotely from User Characterizations that are stored on the VNA disk. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<Mname> |
Name of the measurement you are selecting for the confidence check. The measurement must already exist. |
|
Examples |
SENS:CORR:CCH:PAR 'TEST' sense2:correction:ccheck:parameter 'test' |
|
Query Syntax |
SENSe<cnum>:CORRection:CCHeck:PARameter? Returns the name of the selected measurement on channel <cnum>. |
|
Return Type |
String |
|
Not applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) For UNGUIDED calibration, measures the specified standards from the selected calibration kit. The calibration kit is selected using the Sense:Correction:Collect:CKIT command. For using two sets of standards, see SENS:CORR:TST. Note: Before using this command you must select two items: |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<class> |
Measures the standards associated with these class labels. Choose from: |
|
|
Label |
Forward |
Reverse |
|
|
STAN1 |
S11A |
S22A |
|
|
STAN2 |
S11B |
S22B |
|
|
STAN3 |
S11C |
S22C |
|
|
STAN4 |
S21T |
S12T |
|
|
STAN5 |
Generic Isolation; not associated with calibration kit definition. |
|
|
|
ECAL1 through ECAL50 |
ECAL modules |
|
|
|
RESPonse |
Same as Normalize selection in Unguided Cal. (subclass is ignored) |
|
|
|
POWer |
Take a receiver power cal sweep and turn correction ON |
|
|
|
SLSET |
Sets 'sliding load type', and increments the "number of slides" count. The total number of slides is critical to the correct calculation of the sliding load algorithm. See a sliding load cal example. |
|
|
|
SLDONE |
Computes the sliding load using a circle fit algorithm. |
|
|
[subclass] |
Optional argument. For mechanical calibration kits, choose from the following to specify the standard to be acquired from the SENS:CORR:COLL:CKIT:ORDer list. If not specified, subclass is set to SST1. |
||
|
|
SST1 |
First standard in the order list |
|
|
SST2 |
Second standard in the order list |
|
|
SST3 |
Third standard in the order list |
|
|
SST4 |
Fourth standard in the order list |
|
|
SST5 |
Fifth standard in the order list |
|
|
SST6 |
Sixth standard in the order list |
|
|
SST7 |
Seventh standard in the order list |
|
|
If an ECAL module (1 through 8) is specified for <class>, choose one of the following for specifying which characterization within the ECal module will be used for the acquire. If not specified, the default is CHAR0. |
|
|
|
CHAR0 |
Factory characterization (data that was stored in the ECal module by Keysight) |
|
|
CHAR1 |
User characterization #1 |
|
|
CHAR2 |
User characterization #2 |
|
|
...and so forth up to: |
|
|
|
CHAR12 |
User characterization #12 |
|
[sync] |
Optional argument. Choose from: SYNChronous - blocks SCPI commands during standard measurement (default behavior) ASYNchronous - does NOT block SCPI commands during standard measurement. |
|
|
Examples |
SENS:CORR:COLL STAN1 'If SENS:CORR:COLL:CKIT:ORDer2 5,3,7 SENS:CORR:COLL ECAL4,ASYN; *OPC? sense2:correction:collect:acquire ecal2,char1 |
|
Query Syntax |
Not applicable |
|
Not applicable |
Applicable Models: E5080A, M9485A
|
(Write-only) Applies error terms to the measurement that is selected using Calc:Par:Select. Note: Before using this command you must select a measurement using CALC:PAR:SEL. You can select one measurement for each channel. Note: This command is only necessary if you need to modify error terms. If you do not need to modify error terms, SENSe<cnum>:CORRection:COLLect:SAVE calculates and then automatically applies error terms after you use SENS:CORR:COLL:ACQuire to measure cal standards. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Example |
|
|
Query Syntax |
Not applicable |
|
Not applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Clears the flags for windows to be shown during calibrations. To flag a window to be shown see SENS:CORR:COLL:DISP:WIND. |
|
|
Examples |
SENS:CORR:COLL:DISP:WIND:AOFF sense:correction:collect:display:window:aoff See an example using this command. |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Set the 'show' state of the window to be displayed during a calibration. Learn more. When this command is sent, the specified window is 'flagged' to be shown during calibration. The flag is cleared when the window is closed. A Preset or Instrument State Recall also closes the window. If the same window number is reopened, this command must be sent again to show the window during a calibration. The flag is NOT saved with an instrument state. Send this command for each additional window to show during a calibration. |
|
|
Parameters |
|
|
<wNum> |
Window number to show during a calibration. The calibration window will also be shown with this window. The window must already be created. Use DISPlay:CATalog? to read all existing window numbers. |
|
<bool> |
Window state. Choose from: ON (or 1) - Show the specified window during calibration. OFF (or 0) - Do NOT show the specified window during calibration. |
|
Examples |
SENS:CORR:COLL:DISP:WIND1 1 sense:correction:collect:display:window2:state off See an example using this command. |
|
Query Syntax |
Not Applicable |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies amount to increment (increase) the channel averaging factor during isolation measurement of the ECal module during an unguided ECal calibration. Note: if the channel currently has averaging turned OFF and <num> is greater than 1, averaging will be turned ON only during the isolation measurements and with the averaging factor equal to <num>. |
|
|
Parameters |
|
|
<num> |
Incremental Averaging factor. The maximum averaging factor is 65536 (2^16). |
|
Examples |
SENS:CORR:COLL:ISOL:AVER:INCR 16 sense:correction:collect:isolation:average:increment 0 |
|
Query Syntax |
SENSe:CORRection:COLLect:ISOLation:AVERage:INCRement? |
|
Return Type |
Numeric |
|
8 - If this command is NOT sent, but ECal isolation is measured, then averaging will be turned ON with factor set to 8 during the isolation measurement. |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies whether or not the isolation state of the ECal module will be measured as part of an unguided ECal calibration. An unguided calibration is performed using the SENS:CORR:COLL:METH and SENS:CORR:COLL:ACQ commands. Note: The inherent isolation of the VNA is better than that attained with this command. ONLY use this command when using an external test set, and ONLY using a 8509x ECal module. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
ON (or 1) - isolation is measured during the unguided ECal calibration. OFF (or 0) isolation is NOT measured during the unguided ECal calibration. |
|
Examples |
SENS1:CORR:COLL:ISOL:ECAL ON sense2:correction:collect:isolation:ecal:state 0 |
|
Query Syntax |
SENSe:CORRection:COLLect:ISOLation:ECAL:STATe? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) For UNGUIDED calibration, sets the calibration method (also known as 'Calibration Type' on calibration dialog box.) To select a Cal Type from a Cal Set, use CALC:CORR:TYPE. Note: Before using this command you must select a measurement using CALC:PAR:SEL. You can select one measurement for each channel. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Choose from: |
|
|
Method |
Description |
|
|
NONE |
No Cal method |
|
|
REFL1OPEN |
Response Open |
|
|
REFL1SHORT |
Response Short |
|
|
RESPonse |
Same as Normalize selection in Unguided Cal. |
|
Examples |
SENS:CORR:COLL:METH REFL1SHORT |
|
Query Syntax |
SENSe<cnum>:CORRection:COLLect:METHod? |
|
Return Type |
Character |
|
Not Applicable |
Applicable Models: M9485A
|
(Read-Write) : Specify the ports allowed to participate in a multiport calibration. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<port numbers> |
comma separated list of ports |
|
Examples |
SENS:CORR:COLL:METH:PORT:SUBS:FULL:VAL 1,2,3
Calset is 16 port VNA with a 16 port calibration. Full 3Port (1,2,3) error correction on ports 1,2,3 All other port parameters are uncorrected. |
|
Query Syntax |
SENSe<cnum>:CORRection:COLLect:METHod:PORT:SUBS:FULL:VAL? |
|
Return Type |
Character |
|
Not Applicable |
Applicable Models: M9485A
|
(Write Only) : Reset the the full and response list of the port subset correction. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:CORR:COLL:METH:PORT:SUBS:RES |
|
Query Syntax |
Not Applicable |
|
Return Type |
Not Applicable |
|
Not Applicable |
Applicable Models: M9485A
|
(Read-Write) : Specify the ports that can be corrected using lesser corrections (enhanced response). This list is not allowed to overlap with the full multiport calibration list specified by :SENS:CORR:COLL:METH:PORT:FULL:VAL. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<port numbers> |
comma separated list of ports |
|
Examples |
Calset: 16 port VNA with a 16 port calibration Example 1 SENS:CORR:METH:PORT:SUBS:FULL:VAL 1,2,3,4,5,6 SENS:CORR:METH:PORT:SUBS:RESP:VAL 7,8, Full 6 Port on ports 1 to 6 Enhanced Response for parameters involving ports 7 and 8 No correction for ports 9 to 16
Example 2 SENS:CORR:METH:PORT:SUBS:FULL:VAL 0 SENS:CORR:METH:PORT:SUBS:RESP:VAL 1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16 All parameters are enhance response corrected |
|
Query Syntax |
SENSe<cnum>:CORRection:COLLect:METHod:PORT:SUBS:RESPonse:VAL? |
|
Return Type |
Character |
|
Not Applicable |
Applicable Models: M9485A
|
(Read-Write) Enabling the port subset correction |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
Devolve Calibration state. Choose from: OFF or 0 - Off . ON or 1 - On |
|
Examples |
SENS:CORR:COLL:METH:PORT:SUBS:STAT ON |
|
Query Syntax |
SENSe<cnum>:CORRection:COLLect:METHod:PORT:SUBS:STAT? |
|
Return Type |
Boolean |
|
Not Applicable |
Applicable Models: E5080A, M9485A
|
(Write-only) For UNGUIDED calibrations ONLY. This command does the following:
The Cal Register or User Cal Set is determined by the setting of the SENS:CORR:PREFerence:CSET:SAVE command.
Do NOT use this command during an ECAL. When performing an ECAL calibration using SENS:CORR:COLL:ACQuire, this SAVE operation is performed automatically before the completion of a successful ACQuire. Before using this command you must select a measurement using CALC:PAR:SEL. You can select one measurement for each channel. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENS:CORR:COLL:SAVE |
|
Query Syntax |
Not applicable |
|
Not applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Clears ALL flags for channels to sweep during calibration. To flag a channel, see SENS:CORR:COLL:SWE:CHAN. |
|
|
Examples |
SENS:CORR:COLL:SWE:CHAN:AOFF sense:correction:collect:sweep:channel:aoff See an example using this command. |
|
Not applicable |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Specifies the channel to sweep during a Calibration. When this command is sent, the <cnum2> channel is 'flagged' to be swept during calibration. The flag is cleared when the channel is deleted, if the Measurement Class is changed, or if all measurements are deleted from the channel. If the same channel number is recreated, this command must be sent again to sweep the channel during a calibration. The flag is NOT saved with an instrument state. A Preset or Instrument State Recall deletes the channel. |
|
|
Parameters |
|
|
<cnum> |
The channel to be calibrated. If unspecified, value is set to 1. |
|
<cnum2> |
The channel to sweep when waiting to measure a standard. This channel must already exist with at least one measurement in the channel. If this channel is in continuous sweep mode, it must have the same attenuator settings and path configuration (VNA only). |
|
<bool> |
Channel sweep state. Choose from: ON (or 1) - Sweep the channel during calibration. OFF (or 0) - Do NOT sweep the channel during calibration. |
|
Examples |
SENS:CORR:COLL:SWE:CHAN2 1 sense2:correction:collect:sweep:channel3:state off See an example using this command. |
|
Query Syntax |
Not Applicable |
|
OFF |
|
Applicable Models: M9485A
|
(Read-Write) Set and read the power level at which to perform the Source Power Cal portion of a Gain Compression (Opt 086) Calibration. Learn more about this setting. |
|
|
Parameters |
|
|
<num> |
Power level in dB. Choose a value from +30 to (-30). |
|
Examples |
SENS:CORR:GCS:POW 0 |
|
Query Syntax |
SENSe:CORRection:GCSetup:POWer? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: M9485A
|
(Read-Write) Set and read the cal kit to be used for calibrating at the port 1 reference plane when the power sensor connector is different from the DUT port 1. Learn more. |
|
|
Parameters |
|
|
<string> |
Cal Kit. Use SENS:CORR:COLL:GUID:CKIT:PORT1:CAT? to return a list of valid cal kits. |
|
Examples |
SENS:CORR:GCS:SENS:CKIT "85052B" |
|
Query Syntax |
SENSe:CORRection:GCSetup:SENSor:CKIT? |
|
Return Type |
String |
|
Not Applicable |
|
Applicable Models: M9485A
|
(Read-Write) Set and read the power sensor connector type which is used to perform the Source Power Cal portion of a Gain Compression Calibration. Learn more. |
|
|
Parameters |
|
|
<string> |
Power sensor connector type. Use SENS:CORR:COLL:GUID:CONN:CAT? to return a list of valid connector types. Select "Ignored" to NOT compensate for the adapter. |
|
Examples |
SENS:CORR:GCS:SENS:CKIT "3.5 mm (50) male" |
|
Query Syntax |
SENSe:CORRection:GCSetup:SENSor:CKIT? |
|
Return Type |
String |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the system impedance value for the analyzer. |
|
|
Parameters |
|
|
<num> |
System Impedance value in ohms. Choose any number between 0 and 1000 ohms. |
|
Examples |
SENS:CORR:IMP:INP:MAGN 75 |
|
Query Syntax |
SENSe:CORRection:IMPedance:INPut:MAGNitude? |
|
Return Type |
Numeric |
|
50 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns correction interpolation ON or OFF. Note: Before using this command you must select a measurement using CALC:PAR:SEL. You can select one measurement for each channel. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<ON | OFF> |
ON (or 1) - turns interpolation ON. |
|
Examples |
SENS:CORR:INT ON |
|
Query Syntax |
SENSe<cnum>:CORRection:INTerpolate[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns match-correction ON or OFF. Use this command AFTER performing an Guided Power Cal. Learn more. |
|
|
Parameters |
|
|
<ch> |
Channel number on which Guided Power Cal was performed. If unspecified, value is set to 1 |
|
<bool> |
ON (or 1) - Turns match-correction ON OFF (or 0) - Turns match-correction OFF. |
|
Examples |
SENS:CORR:METH:MATC 0 |
|
Query Syntax |
SENSe<cnum>:CORRection:METHods:MATCh? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies the FOM frequency range to use when performing calibration. |
|
|
Parameters |
|
|
<char> |
Choose from: PRIMary - Used for calibrating at the mmWave frequencies when NOT using a test set. Learn more. AUTO - All other calibration situations. |
|
Examples |
SENS:CORR:PREF:CAL:RANG PRIM |
|
Query Syntax |
SENSe:CORRection:PREFerence:CALibration[:FOM]:RANGe? |
|
Return Type |
Character |
|
AUTO |
|
Applicable Models: E5080A, M9485A
|
Important Notes:
(Read-Write) Specifies the default manner in which calibrations that are performed using SCPI or COM are to be stored. Cal data is ALWAYS stored to the channel Cal Register regardless of this setting. This setting survives instrument preset and reboot. It remains until changed by another execution of this command. Note: Cal Set arguments used with commands such as SENS:CORR:COLL:GUID:INIT, SENS:CORR:COLL:GUID:SAVE and SENS:CORR:COLL:GUID:SAVE:CSET will override of any of these default preference settings. Learn about Cal Registers and User Cal Sets. |
|
|
Parameters |
|
|
<char> |
CALRegister - Each Cal is saved ONLY to the channel Cal Register. If the error terms from a new Cal can co-exist with those in the Cal Register, they are appended. USER - Each Cal is saved to its own new User Cal Set file. The Cal Set name is automatically generated. To change the name, send SENS:CORR:CSET:NAME after the cal is complete. This reverts to pre-6.0 behavior. REUSe - The cal is saved to the Cal Set that is currently selected on the specified channel, which could be the channel Cal Register. If the channel does not yet have a selected Cal Set, the cal will be saved to a new User Cal Set with an automatically-generated name. If the error terms from a new Cal can co-exist with those in the Cal Set, they are appended. |
|
Examples |
SENS:CORR:PREF:CSET:SAVE USER |
|
Query Syntax |
SENSe:CORRection:PREFerence:CSET:SAVE? |
|
Return Type |
Character |
|
CALRegister |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies whether or not the VNA should perform orientation of the ECal module during calibration. Orientation is a technique by which the VNA automatically determines which ports of the module are connected to which ports of the VNA. Orientation begins to fail at very low power levels or if there is much attenuation in the path between the VNA and the ECal module. If orientation is turned OFF, the SENS:CORR:PREF:ECAL:PMAP command must be used to specify the port connections before performing a cal. Note: For 3-port or 4-port measurements, when orientation is OFF, you are not allowed to specify how the ECAL module is connected. Instead, the VNA determines the orientation. Use SENS:CORR:COLL:GUID:DESC? to query the orientation. The VNA does not verify that you made the connection properly. This setting remains until the VNA is restarted or this command is sent again. |
|
|
Parameters |
|
|
<bool> |
ECAL orientation state. Choose from: ON or 1 - VNA performs orientation of the ECal module. OFF or 0 - VNA does NOT performs orientation of the ECal module. |
|
Examples |
SENS:CORR:PREF:ECAL:ORI OFF sense:correction:preference:ecal:orientation:state on |
|
Query Syntax |
SENSe:CORRection:PREFerence:ECAL:ORIentation[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON (1) |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) When ECal module orientation is turned OFF (SENS:CORR:PREF:ECAL:ORI), this command specifies the port mapping (which ports of the module are connected to which ports of the VNA) prior to performing ECal calibrations. This setting remains until the VNA is restarted or this command is sent again. |
|
|
Parameters |
|
|
<module> |
Specifies which ECal module this port map is being applied to. Choose from: ECAL1 .through. ECAL50 |
|
<string> |
Format this parameter in the following manner: Aw,Bx,Cy,Dz where
Ports of the module which are not used are omitted from the string. For example, on a 4-port ECal module with port A connected to VNA port 2 port B connected to VNA port 3 port C not connected port D connected to VNA port 1 the string would be: A2,B3,D1 If either the receive port or source port (or load port for 2-port cal) of the CALC:PAR:SELected measurement is not in this string and orientation is OFF, an attempt to perform an ECal calibration will fail. |
|
Examples |
SENS:CORR:PREF:ECAL:PMAP ECAL2, 'A1,B2' sense:correction:preference:ecal:pmap ecal3, 'a2,b1,c3' |
|
Query Syntax |
SENSe:CORRection:PREFerence:ECAL:PMAP? <module> |
|
Return Type |
String |
|
Null string () |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the preference for the trigger behavior during a calibration. This setting persists until it is changed. Note: If TRIGger:SOURce = Manual, during a calibration the VNA ALWAYS switches to Internal for one trigger, then back to Manual, regardless of this preference command. |
|
|
Parameters |
|
|
<char> |
Character - Calibration type. Choose from: GUIDed - preference setting pertains to a Guided calibration. UNGuided - preference setting pertains to an Unguided calibration. |
|
<bool> |
Boolean - Choose from: 0 - OFF - The trigger behavior during the specified calibration type DOES respect the setting of the TRIGger:SOURce command. For example,when Trigger source = External, the single trigger method will wait for the External trigger signal and then allow only one sweep. 1 - ON - (Pre-6.0 behavior) The trigger behavior during the specified calibration type does NOT respect the setting of the TRIGger:SOURce command. For example, when Trigger source = External, during calibration the VNA switches to Internal sweep, responds to one trigger signal to measure the standard, then switches back to External. |
|
Examples |
SENS:CORR:PREF:TRIG:FREE GUID,1 sense:correction:preference:trig:free unguided,0 |
|
Query Syntax |
SENSe:CORRection:PREFerence:TRIG:FREE? <char> |
|
Return Type |
Boolean |
|
OFF for both calibration types. |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Adjusts a receiver power cal to account for components or adapters that are added between the source port and receiver while performing this cal. For more information, see Receiver Cal. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Offset Value in dB. Specify loss as a negative number; and gain as a positive number. Choose a number between -200 and 200. |
|
Examples |
SENS:CORR:RPOW:OFFS .5 |
|
Query Syntax |
SENSe<cnum>:CORRection:RPOWer:OFFSet[:AMPLitude]? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the velocity factor to be used with Electrical Delay and Port Extensions. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Velocity factor. Choose a number between 0 and 10 (.66 polyethylene dielectric; .7 PTFE dielectric) |
|
Examples |
SENS:CORR:RVEL:COAX .66 |
|
Query Syntax |
SENSe<cnum>:CORRection:RVELocity:COAX? |
|
Return Type |
Numeric |
|
1 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the direction a calibration will be performed when only one set of standards is used. Use SENSe:CORRection:TSTandards[:STATe] OFF to specify that only one set of standards will be used. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<boolean> |
ON (1) - FORWARD direction of a 2-port calibration will be performed OFF (0) - REVERSE direction of a 2-port calibration will be performed |
|
Examples |
SENS:CORR:SFOR 1 See an example using this command |
|
Query Syntax |
SENSe<cnum>:CORRection:SFORward[:STATe]? |
|
Return Type |
Boolean |
|
ON |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns error correction ON and OFF for the specified channel. Note: Before using this command you must select a measurement using CALC:PAR:SEL. You can select one measurement for each channel. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<ON | OFF> |
ON (or 1) - correction is applied to the channel. OFF (or 0) - correction is NOT applied to the channel. |
|
Examples |
SENS:CORR ON |
|
Query Syntax |
SENSe<cnum>:CORRection[:STATe]? To query the error correction state for a measurement, use CALC:CORR:STATe? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the temperature of the noise source connector. Learn more about Noise Figure Calibration. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
|
<num> |
Noise source temperature in Kelvin. |
|
Examples |
SENS:CORR:TCOL:USER:VAL 295 sense2:correction:tcold:user:value 298 See an example using this command |
|
Query Syntax |
SENSe<cnum>:CORRection:TCOLd:USER:VALue? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies the acquisition of calibration data using ONE or TWO sets of standards. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
|
<boolean> |
ON (1) - TWO identical sets of standards will be used to simultaneously calibrate two ports (for both Forward and Reverse parameters). OFF (0)- ONE set of standards will be used to perform a full 2-port calibration, one port at a time. When specifying ON (use two sets), the SENS:CORR:COLL:ACQuire command uses the same standard index for each calibration class. To specify the calibration standard gender for each port, you must first ensure that the order of calibration class accurately reflects the configuration of your DUT. For example, for a DUT with a male connector on port 1 and a female connector on port 2, order the devices within the S11 classes (A, B, and C) such that the MALE standards are first in the list. Then order the S22 classes specifying the FEMALE standards as the first in the list. |
|
Examples |
SENS:CORR:TST 1 See an example using this command |
|
Query Syntax |
SENSe<cnum>:CORRection:TSTandards[:STATe]? |
|
Return Type |
Boolean |
|
ON |
|
Applicable Models: E5080A, M9485A
|
(Read only) Lists the Cal Types in the VNA by either GUID or registered name. Learn more about applying Cal Type using SCPI. Note: Before using this command you must select a measurement using CALC:PAR:SEL. You can select one measurement for each channel. |
|
|
Parameters |
|
|
<char> |
(Optional) Specifies the type of list. Choose from: GUID - the registered GUID of the Cal Type NAME - the registered name of the Cal Type (Default) |
|
Examples |
SENS:CORR:TYPE:CAT? GUID |
|
Query Syntax |
SENSe<cnum>:CORRection:TYPE:CATalog? <char> |
|
Return Type |
Comma-separated string |
|
Not Applicable |
|
Last modified:
|
16-Mar-2015 |
First Release |
![]()