Controls External Triggering .
|
TRIGger: AUX | COUNt CHANnel:AUX | DURation | [ENABle] | INTerval | POSition | TYPE PREFerence | AIGLobal [SEQuence] | SCOPe | SOURce | SLOPe | TYPE |
Click on a Red keyword to view the command details.
See Also
Applicable Models: E5080A
|
(Read-only) Returns the number of AUX trigger output connector in the instrument. |
|
|
Parameters |
|
|
Examples |
TRIG:AUX:COUN? trigger:auxiliary:count? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: E5080A
|
(Read-Write) Specifies the width of the output pulse, which is the time that the Aux trigger output will be asserted. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Rear panel connector used to send or receive signals. If unspecified, value is set to 1. |
|
<num> |
Duration value in seconds. Choose a value between 1us (1E-6) and 1. |
|
Examples |
TRIG:CHAN:AUX:DUR .1 trigger:channel2:aux:duration .01 |
|
Query Syntax |
TRIGger:CHANnel<ch>:AUXiliary<n>:DURation? |
|
Return Type |
Numeric |
|
1E-6 |
|
Applicable Models: E5080A
|
(Read-Write) Turns ON / OFF the trigger output. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Rear panel connector used to send or receive signals. If unspecified, value is set to 1. |
|
<bool> |
ON or 1 - Turns trigger output ON. OFF or 0 - Turns trigger output OFF. |
|
Examples |
TRIG:CHAN:AUX 1 trigger:channel2:aux:enable off |
|
Query Syntax |
TRIGger:CHANnel<ch>:AUXiliary<n>:[ENABle]? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A
|
(Read-Write) Specifies how often a trigger output signal is sent. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Rear panel connector used to send or receive signals. If unspecified, value is set to 1. |
|
<char> |
Choose from:
|
|
Examples |
TRIG:CHAN:AUX:INT POI trigger:channel2:aux:interval sweep |
|
Query Syntax |
TRIGger:CHANnel<ch>:AUXiliary<n>:INTerval? |
|
Return Type |
Character |
|
|
SWEep |
Applicable Models: E5080A
|
(Read-Write) Specifies the polarity of the Aux Output signal being supplied by the VNA. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Rear panel connector used to send or receive signals. If unspecified, value is set to 1. |
|
<char> |
Choose from:
|
|
Examples |
TRIG:CHAN:AUX:OPOL NEG trigger:channel2:aux:opolarity positive |
|
Query Syntax |
TRIGger:CHANnel<ch>:AUXiliary<n>:OPOLarity? |
|
Return Type |
Character |
|
NEGative |
|
Applicable Models: E5080A
|
(Read-Write) Specifies whether the aux trigger out signal is sent BEFore or AFTer the acquisition. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Rear panel connector used to send or receive signals. If unspecified, value is set to 1. |
|
<char> |
Choose from:
|
|
Examples |
TRIG:CHAN:AUX:POS BEF trigger:channel2:aux:position after |
|
Query Syntax |
TRIGger:CHANnel<ch>:AUXiliary<n>:POSition? |
|
Return Type |
Character |
|
AFTer |
|
Applicable Models: E5080A
|
(Read-Write) Specifies the type of Aux input detection that the VNA will employ. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
|
<n> |
Rear panel connector used to send or receive signals. If unspecified, value is set to 1. |
|
<char> |
Choose from: EDGE - VNA responds to the leading edge of a signal. LEVel - VNA responds to the level (HIGH or LOW) of a signal. |
|
Examples |
TRIG:CHAN:AUX:TYPE EDGE trigger:channel2:aux:type level |
|
Query Syntax |
TRIGger:CHANnel<ch>:AUXiliary<n>:TYPE? |
|
Return Type |
Character |
|
EDGE |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and reads the trigger delay for ALL channels (globally). This delay is only applied while TRIG:SOURce = EXTernal and TRIG:SCOP = ALL After an external trigger is applied, the start of the sweep is held off for an amount of time equal to the delay setting plus any inherent latency. To apply a trigger delay for the specified channel ONLY, use SENS:SWE:TRIG:DELay |
|
|
Parameters |
|
|
<num> |
Delay value in seconds. Choose from 0 to 107. |
|
Examples |
TRIG:DEL .0003 Sets the trigger delay to 300 microseconds. The sweep will not start until approximately 300 microseconds after an external trigger is applied. |
|
Query Syntax |
TRIGger:DELay? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A
|
(Read-Write) Sets the Trigger OUT behavior to either Global or Channel. Learn more about this setting. This command will cause the VNA to Preset. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. To send this command using the VNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the VNA took the command. |
|
|
Parameters |
|
|
<bool> |
Choose from:
|
|
Examples |
TRIG:PREF:AIGL 1 trigger:preference:aiglobal 0 |
|
Query Syntax |
TRIGger:PREFerence:AIGLobal? |
|
Return Type |
Boolean |
|
0 |
|
Applicable Models: E5080A
|
(Read-Write) Specifies the polarity of Ready for Trigger output. All existing Ready for Trigger outputs are configured simultaneously with this command. |
|
|
Parameters |
|
|
<char> |
LOW - Outputs a TTL low when the VNA is ready for trigger. HIGH - Outputs a TTL high when the VNA is ready for trigger. |
|
Examples |
TRIG:READ:POL HIGH trigger:ready:polarity low |
|
Query Syntax |
TRIGger:READy:POLarity? |
|
Return Type |
Character |
|
Low |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies whether a trigger signal is sent to all channels or only the current channel. |
|
|
Parameters |
|
|
<char> |
Choose from:
|
|
Examples |
TRIG:SCOP ALL |
|
Query Syntax |
TRIGger[:SEQuence]:SCOPe? |
|
Return Type |
Character |
|
ALL |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies the polarity expected by the external trigger input circuitry. Also specify TRIG:TYPE (Level |Edge). |
|
|
Parameters |
|
|
<char> |
Choose from:
|
|
Examples |
TRIG:SLOP NEG |
|
Query Syntax |
TRIGger[:SEQuence]:SLOPe? |
|
Return Type |
Character |
|
POSitive |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the source of the sweep trigger signal. This command is a super-set of INITiate:CONTinuous which can NOT set the source to External. |
|
|
Parameters |
|
|
<char> |
Choose from:
|
|
Examples |
TRIG:SOUR EXT |
|
Query Syntax |
TRIGger[:SEQuence]:SOURce? |
|
Return Type |
Character |
|
IMMediate |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies the type of EXTERNAL trigger input detection used to listen for signals on the Meas Trig IN connectors. Edge triggers are most commonly used. |
|
|
Parameters |
|
|
<char> |
Choose from: EDGE VNA responds to the rising and falling edge of a signal. LEVel VNA responds to a level (HIGH or LOW). Use TRIG:SLOPe to specify Rising or falling - High or Low. |
|
Examples |
TRIG:TYPE EDGE trigger:sequence:type level |
|
Query Syntax |
TRIGger[:SEQuence]:TYPE? |
|
Return Type |
Character |
|
LEVel |
|
Last modified:
|
18-May-2016 |
First Release |