Specifies the sweep functions of the analyzer.
|
SENSe:SWEep: | AUTO | SDELay GROups | COUNt SLOCal | MAXimum | STATe | AUTO TRIGger | DELAY | MODE
|
Click on a Red keyword to view the command details.
See Also
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the dwell time between each sweep point.
|
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Dwell time in seconds. This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SWE:DWEL .1 |
|
Query Syntax |
SENSe<cnum>:SWEep:DWELl? |
|
Return Type |
Numeric |
|
0 - (Note: dwell time set to 0 is the same as dwell:auto ON) |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies whether or not to automatically calculate and set the minimum possible dwell time. Setting Auto ON has the same effect as setting dwell time to 0. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
ON (or 1) - turns dwell ON. |
|
Examples |
SENS:SWE:DWEL:AUTO ON |
|
Query Syntax |
SENSe<cnum>:SWEep:DWELl:AUTO? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Specifies the time to wait just before acquisition begins for each sweep. This delay is in addition to Dwell Time and the following two External Trigger delays if enabled.
|
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Sweep delay in seconds. This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SWE:DWEL:SDEL .1 |
|
Query Syntax |
SENSe<cnum>:SWEep:DWELl:SDELay? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A
|
(Read-Write) Sets sweep as Stepped or Analog. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Choose from: STEPped - source frequency is CONSTANT during measurement of eah displayed point. More accurate than ANALog. Dwell time can be set in this mode. ANALog (Auto) - source frequency is continuously RAMPING during measurement of each displayed point. Faster than STEPped. Sweep time (not dwell time) can be set in this mode. |
|
Examples |
SENS:SWE:GEN STEP |
|
Query Syntax |
SENSe<cnum>:SWEep:GENeration? |
|
Return Type |
Character |
|
STEPped |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the trigger count (groups) for the specified channel. Set trigger mode to group after setting this count. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Count (groups) number. Choose any number between: |
|
Examples |
SENS:SWE:GRO:COUN 10 |
|
Query Syntax |
SENSe<cnum>:SWEep:GROups:COUNt? |
|
Return Type |
Numeric |
|
1 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the number of trigger signals the specified channel will ACCEPT. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Trigger mode. Choose from: HOLD - channel will not trigger CONTinuous - channel triggers indefinitely GROups - channel accepts the number of triggers specified with the last SENS:SWE:GRO:COUN <num>. This is one of the VNA overlapped commands. Learn more. SINGle - channel accepts ONE trigger, then goes to HOLD. Note: To perform simple, single-triggering, use SINGle which requires that TRIG:SOURce remain in the default (internal) setting. |
|
Examples |
SENS:SWE:MODE CONT |
|
Query Syntax |
SENSe<cnum>:SWEep:MODE? |
|
Return Type |
Character |
|
CONTinuous |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the number of data points for the measurement. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Choose any number between 1 and the VNA maximum number of points. This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. |
|
Examples |
SENS:SWE:POIN 51 |
|
Query Syntax |
SENSe<cnum>:SWEep:POINts? |
|
Return Type |
Numeric |
|
201 |
|
Applicable Models: E5080A
|
(Read-Write) Sets the Shift LO maximum frequency for the selected channel. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Range of shift LO maximum frequency is 1.5E8 to Maximum frequency. |
|
Examples |
SENS:SWE:SCLOC:MAX 1.5E8 |
|
Query Syntax |
SENSe<cnum>:SWEep:SLOCal:MAXimum? |
|
Return Type |
Numeric / Double precision floating point |
|
Maximum frequency |
|
Applicable Models: E5080A
|
(Read-Write) Turns ON or OFF the Shift LO mode for the selected channel. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
Select shoft LO mode from either of the following: ON or 1 - Turns ON the Shift LO mode. OFF or 0 - Turns OFF the Shift LO mode. |
|
Examples |
SENS:SWE:SLOC:STAT ON |
|
Query Syntax |
SENSe<cnum>:SWEep:SLOCal:STATe? |
|
Return Type |
Boolean |
|
OFF or 0 |
|
Applicable Models: M9485A
|
(Read-Write) Sets and returns the state of Fast Sweep mode. Learn more about Fast Sweep. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Fast Sweep mode. Choose from: FAST - turns Fast Sweep Mode ON NORMal - turns Fast Sweep Mode OFF (Normal Mode). |
|
Examples |
SENS:SWE:SPE NORM |
|
Query Syntax |
SENSe<cnum>:SWEep:SPEed? |
|
Return Type |
Character |
|
NORMal |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the step of stimulus |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Value of step for each points in stimulus |
|
Examples |
SENS:SWE:STEP 1e3 |
|
Query Syntax |
SENSe<cnum>:SWEep:STEP? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the time the analyzer takes to complete one sweep. If sweep time accuracy is critical, use ONLY the values that are attained using the up and down arrows next to the sweep time entry box. See Sweep Time. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Sweep time in seconds. To select the fastest sweep speed, either send MIN as an argument to this command, or send SENS:SWE:TIME:AUTO 1. This command will accept MIN or MAX instead of a numeric parameter. See SCPI Syntax for more information. The MAX value will change based on point count, IFBW, and dwell time. |
|
Examples |
SENS:SWE:TIME 1ms |
|
Query Syntax |
SENSe<cnum>:SWEep:TIME? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns the automatic sweep time function ON or OFF. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
ON (or 1) - turns the automatic sweep time ON. OFF (or 0) - turns the automatic sweep time OFF. |
|
Examples |
SENS:SWE:TIME:AUTO |
|
Query Syntax |
SENSe<cnum>:SWEep:TIME:AUTO? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
ON |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and reads the trigger delay for all measurements in the specified CHANNEL. This delay is only applied while TRIG:SOURce EXTernal and TRIG:SCOP CURRent . After an external trigger is applied, the start of the sweep is delayed for the specified delay value plus any inherent latency. To apply a trigger delay for all channels (Global), use TRIG:DEL |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
Trigger delay value in seconds. Range is from 0 to 107 seconds |
|
Examples |
SENS:SWE:TRIG:DELay .003 |
|
Query Syntax |
SENSe<cnum>:SWEep:TRIGger:DELay? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and reads the trigger mode for the specified channel. This determines what EACH signal will trigger. Learn more. Note: Setting Point and Sweep mode forces Trigger:SCOPe = CURRent |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Trigger mode. choose from:
|
|
Examples |
SENS:SWE:TRIG:MODE SWE |
|
Query Syntax |
SENSe<cnum>:SWEep:TRIGger:MODE? |
|
Return Type |
Character |
|
Channel |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the type of analyzer sweep mode. First set sweep type, then set sweep parameters such as frequency or power settings. Note: For SweptIMD channels, use SENS:IMD:SWE:TYPE SEGMent See Also: FCA Segment Sweep commands |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Choose from: LINear | LOGarithmic | POWer | CW | SEGMent Note: SWEep TYPE cannot be set to SEGMent if there are no segments turned ON. A segment is automatically turned ON when the analyzer is started. |
|
Examples |
SENS:SWE:TYPE LIN |
|
Query Syntax |
SENSe<cnum>:SWEep:TYPE? |
|
Return Type |
Character |
|
LINear |
|
Last Modified:
|
18-May-2016 |
First Release |
![]()
![]()