Sweep Settings


A sweep is a series of consecutive data point measurements taken over a specified sequence of stimulus values. You can make the following sweep settings:

See Triggering and other 'Setup Measurements' topics

Sweep Type

How to set Sweep Type

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Sweep > Main > Sweep Type.

  1. Right click on the stimulus range area under grid box.

  2. Click Sweep Setup....

  3. Select Sweep Type tab.

  4. Click Apply to implement the setting changes.

Sweep Type Dialog Box / Sweep > Main > Sweep Type Softtab Help

Note: Sweep Settings are not applied until either OK or Apply is pressed.

Channel - The active channel when Sweep Type was selected. Sweep settings will be applied to this channel.

 

Linear Frequency - Sets a linear frequency sweep that is displayed on a standard grid with ten equal horizontal divisions.

  • Start - Sets the beginning value of the frequency sweep.

  • Stop - Sets the end value of the frequency sweep.

  • Power - Sets the power level for selective port.

  • Points - Sets the number of data points that the VNA measures during a sweep.

  • IF Bandwidth - Sets the IF (Receiver) bandwidth.  

Log Frequency - The source is stepped in logarithmic increments and the data is displayed on a logarithmic X-axis. This is usually slower than a continuous sweep with the same number of points.

  • Start - Sets the beginning value of the frequency sweep.

  • Stop - Sets the end value of the frequency sweep.

  • Power - Sets the power level for selective port.

  • Points - Sets the number of data points that the VNA measures during a sweep.

  • IF Bandwidth - Sets the IF (Receiver) bandwidth.  

Power Sweep - Activates a power sweep at a single frequency that specify. Learn more about power sweep

  • Start Power - Sets the beginning value of the power sweep.

  • Stop Power - Sets the end value of the power sweep.

  • CW Freq - Sets the single frequency where the VNA remains during the measurement sweep.

  • Points - Sets the number of data points that the VNA measures during a sweep.

  • IF Bandwidth - Sets the IF (Receiver) bandwidth.  

CW Time - Sets the VNA to a single frequency and the data is displayed versus time. Learn more.

  • CW Freq - Sets the frequency where the VNA remains during the measurement.F

  • Power - Sets the power level for selective port.

  • Points - Sets the number of data points that the VNA measures during a sweep.

  • IF Bandwidth - Sets the IF (Receiver) bandwidth.  

Segment Sweep - Sets the VNA to sweep through user-defined sweep segments. Learn how to make these settings.

    OK - Applies setting changes and closes the dialog box.

    Cancel - Closes the dialog. Setting changes that have been made do not apply and save, but it remain setting since the last Apply button is clicked. 

    Apply - Applies setting changes and leaves the dialog box open to make more setting changes.

    Help - Display the Sweep Type dialog box help.

    Power Sweep

    A power sweep either increases or decreases source power in discrete steps. Power sweep is used to characterize power-sensitive circuits, with measurements such as gain compression.

    In the Sweep Type dialog, specify Start Power, Stop Power, CW Frequency, Points and IF Bandwidth.

    The remaining power settings apply in power sweep mode:

    Notes:

    Segment Sweep

    Segment Sweep activates a sweep which consists of frequency sub-sweeps, called segments. For each segment can define independent power levels, IF bandwidth, IF bandwidth per port, sweep time, delay.

    Once a measurement calibration is performed on the entire sweep or across all segments, measurements can be calibrated for one or more segments.

    In segment sweep type, the analyzer does the following:

    Restrictions for segment sweep:

    How to make segment sweep settings

    Using Hardkey/SoftTab/Softkey

    Using a mouse

    1. Press Sweep > Segment Table.

    1. Right click on the X-axis label or stimulus display area under grid line.

    2. Click Sweep Setup... > select Segment Sweep under sweep type.

    3. Click Segment Table....

    Segment Table Dialog Box Help / Sweep > Segment Table Softtab Help

    Add Segment - adds a sweep segment at last segment.

    Insert Segment - adds a sweep segment before the selected segment. You can also click the "down" arrow on your keyboard to quickly add many segments.

    Delete Segment - removes the selected segment.

    Delete All Segments - removes all segments.

    Note: At least ONE segment must be ON or Sweep Type is automatically set to Linear.

     

    Segment Table dialog box

    X-Axis Point Spacing - Check to scale the X-axis to include only the segments. Learn more.

    Allow Arbitrary Segments - Check to allow arbitrary frequencies (overlapped or reverse sweep). Learn more.

    Display Center/Span Freq - Check to display the center/span frequency.

     

    Independent Setting Per Segment

    Power Level - Sets the Power level for the segment. Also, the test port power can UNCOUPLE. See Power Coupling.

    IF Bandwidth - Sets the IF Bandwidth for the segment.

    IF Bandwidth Per Port - Sets the different bandwidth with different port for the segment.

    Sweep Time - Sets the Sweep time for the segment.

    Delay - Sets the time to wait just before acquisition begins for each segment.

    Dwell - Specifies the time the source stays at each measurement point before the analyzer takes the data.

    Receiver Atten Per Port - Sets the receiver attenuators by logical receiver notation. Options are 0dB and 35dB. Default setting is 35dB.

     

    Save Table - Saves the setting changes in segment table.

    Load Table - Apply the setting changes in segment table.

     

    To Modify an Existing Segment

    To make the following menu settings available, the segment table must shows first. (Press Sweep > Segment Table)

    The above graphic shows the Segment table with all independent settings selected, including source power uncoupled (two power settings).

    State - Click the box on the segment to be modified. Then, use the up/down arrow to turn the segment ON or OFF.

    Start - Sets start frequency for the segment. Click the box and type a value and the first letter of a suffix (KHz, Mhz, GHz). Or double-click the box to select a value.

    Stop - Sets stop frequency for the segment. Click the box and type a value and the first letter of a suffix (KHz, Mhz, GHz). Or double-click the box to select a value.

    Note: The segment table truncates the frequency resolution. To verify the frequency resolution that you input, create a marker at the start or stop frequency settings.

    Points - Sets number of data points for this segment. Insert a value or double-click the box to select a value.

    To set Power Level, IF Bandwidth/IF Bandwidth Per Port, Sweep Time, Delay, Receiver Attenuator Per Port independently for each segment:

    1. Press Sweep > Main > Sweep Type > Segment Sweep.

    2. Click on Segment Table > Segment Table....

    3. Click the box and type a value or double-click the box and select a value.

    Note: If the following are NOT set, the entire sweep uses the channel IFBW, Power, and Time settings.

    X-Axis Point Spacing - Segment Sweep ONLY

    This feature affects how a segment trace is drawn on the screen.

    How to enable X-axis Point Spacing

    Using Hardkey/SoftTab/Softkey

    Using a mouse

    1. Press Sweep > Segment Table > Segment Table....

    2. Tick on X-Axis Point Spacing.

    1. Right click on the X-axis label or stimulus range area under grid line.

    2. Click Sweep Setup... > select Segment Sweep under sweep type.

    3. Click Segment Table....

    4. Tick on X-Axis Point Spacing.

    For example, given the following two segments:

     

    Without X-Axis Point Spacing

     

    With X-Axis Point Spacing

    Arbitrary Segment Sweep

    This feature allows arbitrary frequencies to be entered into the segment sweep table. With this capability, segments can have:

    However, there are several limitation:

    How to enable Arbitrary Segment Sweep

    Using Hardkey/SoftTab/Softkey

    Using a mouse

    1. Press Sweep > Segment Table > Segment Table....

    2. Tick on Allow Arbitrary Segment Sweep.

    1. Right click on the X-axis label or stimulus range area under grid line.

    2. Click Sweep Setup... > select Segment Sweep under sweep type.

    3. Click Segment Table....

    4. Tick on Allow Arbitrary Segment Sweep.

    Notes:

    Sweep Time

    The VNA automatically maintains the fastest sweep time possible with the selected measurement settings. However, you can increase the sweep time to perform a slower sweep.

    How to set Sweep Time

    Using Hardkey/SoftTab/Softkey

    Using a mouse

    1. Press Sweep > Sweep Timing > Sweep Time to change Manual.

    2. Input the desired sweep time.

    1. Right click on the X-axis label or stimulus range area under grid line.

    2. Click on Sweep Setup....

    3. Select Timing tab.

    4. Turn off the check box of Auto Sweep Time.

    5. Input the desired sweep time.

     

    Sweep > Sweep Timing Softtab Help

    Sweep Time - Specifies the time the VNA takes to acquire data for a sweep. The maximum sweep time of the VNA is depends on various settings (ex, IFBW, Dwell Time, Number of points, etc). Learn about other settings that affect sweep speed.

      Sweep Setup

      How to make Sweep Setup settings

      Using Hardkey/SoftTab/Softkey

      Using a mouse

      1. Press Sweep > Sweep Timing.

      1. Right click on the X-axis label or stimulus range area under grid line.

      2. Click on Sweep Setup....

      3. Select Timing tab.

      Sweep Setup Dialog Box / Sweep > Sweep Timing Softtab Help

      Time

      Sweep Time - same as Sweep Time Softtab Help.

      Dwell Time - Specifies the time the source stays at each measurement point before the analyzer takes the data. Only applies to stepped sweep. The maximum dwell time is 20 seconds. See also Electrically Long Devices.

      Sweep Delay - Specifies the time to wait just before acquisition begins for each sweep. This delay is in addition to Dwell Time (per point) and External Trigger delay if enabled.

      Auto Sweep Time -  Automatic adjust the sweep time and dwell time. When "Auto Sweep Time" is checked, the sweep time and dwell time will disable to edit.

       

      Sweep Mode

      Stepped Sweep - When clicked on Stepped Sweep Mode, the VNA source is tuned, then waits the specified Dwell time, then takes response data, then tunes the source to the next frequency point. This is slower than Analog Sweep, but is more accurate when testing electrically-long devices.

      • For all FOM measurements.

         

        Sweep Sequence

        Standard Sweep - When checked, the VNA sweeps all data points for each source port in turn. For a 2-port VNA, this means that all data points are swept in the forward direction, then all data points are swept in the reverse direction. Even when NO reverse parameters are displayed (S22 or S12), reverse measurements are necessary when a full 2-port calibration is correcting the channel. This is the default behavior. Learn more.


          Last modified:

          18-May-2016

          First Release