Frequency range is the span of frequencies you specify for making a device measurement.
See other 'Setup Measurements' topics
There are two ways to set the frequency range:
Specify the Start and Stop frequencies of the range.
Specify the Center frequency and desired Span of the range.
See the frequency ranges of all VNA models.

|
Start - Specifies the beginning frequency of the swept measurement range. Stop - Specifies the end frequency of the swept measurement range. Center - Specifies the value at the center of the frequency sweep. This value can be anywhere in the analyzer range. Span - Specifies the span of frequency values measured to either side of the center frequency. Points - Specifies number of measurement points. Step - Specifies the step. |
Zoom allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep.
Zoom operates on the Active Trace and all traces in the same channel as the active trace, regardless of the window in which they appear.
|
How to Zoom in a measurement window |
Select from the following:
Notes:
Zoom is NOT available for the following:
|
Measurements with a CW Time sweep or Power sweep are made at a single frequency rather than over a range of frequencies.
How to set CW Frequency |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|

|
CW - Type a value and the first letter of the suffix (k,m,or g) or use the up and down arrows to select any value within the range of the VNA. |
The resolution for setting frequency is 1 Hz.
Last modified:
|
18-May-2016 |
First release |
![]()