It is critical to understand the meaning of the following terms as they are used on the VNA.
Traces are a series of measured data points. There is no theoretical limit to the number of traces. However, the practical limit is the maximum number of windows times the maximum number of traces per window (24). If the traces is exceed the maximum traces per window, it will automatically open another window for the trace.
In addition, one memory trace can be stored and displayed for every data trace. Learn more about Math/Memory traces.
Trace settings affect the presentation and mathematical operations of the measured data.
The following are Trace settings:
Time Domain (Opt 010)
How to display a custom trace title (separate topic)
How to display a wide active trace (separate topic)
How to Add a traceThe only measurements that can be selected are those in the same measurement class as is currently assigned to the channel. To select a measurement other than these, first select the appropriate measurement class to a new or existing channel. Learn how. A trace must be selected (active) before its trace settings can be changed. |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to Select a traceThe only measurements that can be selected are those in the same measurement class as is currently assigned to the channel. To select a measurement other than these, first select the appropriate measurement class to a new or existing channel. Learn how. A trace must be selected (active) before its trace settings can be changed. |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to Delete a trace |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to Move a trace to a different windowYou can DRAG a trace from one window to another, or... |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|

|
Note: Only ONE trace can be move in one time. Move Trace N to window - Transfer the selected trace to any Window that listed. |
How to maximize the active trace - the ONLY trace on the screen display. All other traces are hidden. |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to hold the active trace at the maximum or minimum point. |
|
Using Hardkey/SoftTab/Softkey |
|
Maximum/Minimum trace hold can be applied with several conditions:
Feature is applicable to any data trace, not to memory traces.
When the stimulus or any data post processing setting is changed, the trace hold data will be reset. These settings include:
Smoothing on/off.
Smoothing Aperture.
Gating on/off.
Transform on/off.
Conversion state change, conversion type change.
Data Math Function (Data/Mem) change.
Equation Editor state change, formula change.
Parameter change.
Formatting change.
Minimum/maximum comparison is done with formatted data. For Smith and Polar formats, absolute data is used and not phase.
Trace hold data can be recalled.
Data save files formats
SnP: do not save trace hold data
Citifile, CSV, MDF, PRN: save trace hold data
Note: Citifiles can be recalled and viewed in the VNA.
Use SCPI commands to get trace hold data. If trace hold is active, then the data returned from the remote interfaces will be the trace hold data.
Channels contain traces. Channel settings determine how the trace data is measured. All traces that are assigned to a channel share the same channel settings. The following are channel settings:
Trigger (some settings are global)
How to select a channelA channel must be selected (active) before its settings can be changed. To make a channel active, select a trace in that channel or click the Trace Status button of a Trace in that channel |
Windows are used for viewing traces.
The VNA can show an UNLIMITED number of windows on the screen with the following limitations:
The COM property Maximum Number Of Windows returns 1000 ('unlimited' is not a number).
The SCPI status register can only track the status of up to 576 traces.
Each window can contain up to 24 traces .
Windows are completely independent of channels.
See Customize the VNA screen to learn how to make other window settings.
The following is a window containing two traces. Both traces use the same channel 1 settings as indicated by the annotation at the bottom of the window.

VNA shows the window number in the lower-left corner of the window. The following shows window 5.
![]()
How to make various window settingsNew, Close, Tile, Cascade, Minimize, Maximize |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to Delete a Window |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Sheets are used to group VNA windows. Tabbed sheet provides an easy way to switch multiple display settings quickly.
Features and actions that can performed with tabbed sheets
Add/Delete/Select sheet
Move window to sheet
Measurement can be performed on traces/channels in inactive sheets
Easy setup for channel per window
Easy setup for channel per sheet
How to Delete a Sheet |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to View a Sheet |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
How to Change Sheet Title |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
None |
Last modified:
|
18-May-2016 |
First Release |
![]()