Dynamic range is the difference between the analyzer receiver's maximum input power and the minimum measurable power (noise floor). For a measurement to be valid, input signals must be within these boundaries.
Increasing dynamic range is important if you need to measure very large variations in signal amplitude, such as filter bandpass and rejection. The dynamic range is shown below for an example measurement.

To help reduce measurement uncertainty, the analyzer dynamic range should be greater than the response that the DUT exhibits. For example, measurement accuracy is increased when the DUT response is at least 10 dB above the noise floor. The following methods can help you increase the dynamic range.
Other topics about Optimizing Measurements
Increase the DUT input power so that the analyzer can more accurately detect and measure the DUT output power. However, use caution - too much power can damage the analyzer receiver or cause compression distortion.
Caution! Test Port RF Power input damage level: +27 dBm.
See how to increase input power to the device
Tip: You can further increase dynamic range by using an external booster amplifier to increase the input power to the DUT. See High Power Amplifier Measurements.
You can use the following techniques to lower the noise floor and increase the analyzer's dynamic range.
Reduce crosstalk between the VNA receivers when measuring signals close to the noise floor. See Receiver Crosstalk.)
Use Sweep Averaging - learn more about Sweep Average
Reduce the IF Bandwidth - learn more about IF Bandwidth.
In Segment sweep mode each segment can have its own IF bandwidth. For example, when measuring a filter:
In the passband, the IF bandwidth can be set wider for a fast sweep rate, as long as high-level trace noise is kept sufficiently small.
In the reject band, where noise floor contributes significantly to measurement error, the IF bandwidth can be set low enough to achieve the desired reduction in average noise level.
Last Modified:
|
18-May-2016 |
First Release |
![]()