Note: The EventID's listed below are provided for COM programming. For more information, see Working with VNA Events
For more information on VNA error messages (see Error Messages).
Memory overflow. Trigger state set to Hold. Lower the IF bandwidth, or increase dwell or sweep time.
Severity: Informational
Further explanation: The measurement that you are currently making requires that data be stored faster than it can be processed. Very few customers will experience this situation.
Suggestions: To limit the amount of data to be stored, try lowering the IF Bandwidth, slow the sweep time, increase the dwell time, or limit the number of data points. There are many other settings that can be adjusted to solve this problem.
EventID:
"A secondary parameter (power, IFBW, sweep time, step mode) of the calibrated state has changed."
Severity: Informational
Further explanation: The calibration is questionable when any of these secondary parameters change after the calibration is performed.
Suggestions: If you require an accurate measurement with the new settings, repeat the calibration.
EventID: 68020200 (hex)
"Calibration cannot be completed until you have measured all the necessary standards for your selected Cal Type."
Severity: Informational
Further explanation: You probably received this message because you attempted to turn correction on without first measuring all of the calibration standards
Suggestions: Finish measuring the cal standards
EventID: 68020201 (hex)
"Calibration set has been recalled using a file previously saved on an analyzer that had a different hardware configuration."
Severity: Informational
Further explanation:
Suggestions:
EventID: 68020202 (hex)
"Calibration is required before correction can be turned on. Channel number is <x>, Measurement is <x>."
Severity: Informational
Further explanation: There are no error correction terms to apply for the specified channel and measurement.
Suggestions:Perform or recall a calibration
EventID: 68020203 (hex)
"Critical parameters in your current instrument state do not match the parameters for the calibration set, therefore correction has been turned off. The critical instrument state parameters are sweep type, start frequency, frequency span, and number of points."
Severity: Informational
Further explanation: None
Suggestions: You can either recalibrate using the new settings or change back to the original setting that was used when the calibration was performed.
EventID: 68020204 (hex)
"Interpolation is turned off and you have changed the stimulus settings of the original calibration, so correction has been turned off."
Severity: Informational
Further explanation: The most accurate calibration is maintained only when the original stimulus settings are used.
Suggestions: If reduced accuracy is OK, set interpolation ON to allow stimulus setting changes.
EventID: 68020205 (hex)
"Interpolation is turned off and you have selected correction ON. Correction has been restored with the previous stimulus settings."
Severity: Informational
Further explanation: None
Suggestions: None
EventID: 68020206 (hex)
"Stimulus settings for your current instrument state exceeded the parameters of the original calibration, so correction has been turned off."
Severity: Informational
Further explanation: Correction data outside the stimulus settings does not exist.
Suggestions: Perform a broadband calibration, with increased numbers of points with interpolation ON, to maintain calibration over the widest possible stimulus frequency settings.
EventID: 68020207(hex)
"Cal Type is set to NONE for Channel <x>, Measurement <x>; please select Calibration menu or press Cal hard key."
Severity: Informational
Further explanation: A cal operation can not proceed until a calibration exists or the cal type is selected. This error can occur if the calibration can not be found. Also this error can happen if a calibration type is not specified before attempting to programmatically execute cal acquisitions.
Suggestions To find a calibration, select a Cal Set that contains the calibration needed for the current measurements. OR specify the cal type before beginning a calibration procedure.
EventID: 68020208 (hex)
"The measurement you set up does not have a corresponding calibration type, so correction has been turned off or is not permitted."
Severity: Informational
Further explanation: The calibration for the channel may apply only to certain S-Parameters. For example, a 1-Port calibration for S11 can not be applied to a 1-Port calibration applied to S22.
Suggestions: Select a calibration type, such as full 2-Port cal, that can be applied to all the measurements to be selected.
EventID: 68020209 (hex)
"The calibration type you selected cannot be set up."
Severity: Informational
Further explanation: "Please use the SCPI command ROUTe:PATH:DEFine:PORT <num>,<num> for full 2 port type port assignment."
Suggestions:
EventID: 6802020A (hex)
"The calibration path you selected cannot be set up because it is not valid for the current measurement."
Severity: Informational
Further explanation: "Please use the SCPI command ROUTe:PATH:DEFine:PORT <num>,<num> for full 2 port type port assignment related to your current measurement."
Suggestions:
EventID: 6802020B (hex)
"The source power calibration is complete."
Severity: Informational
Further explanation:
Suggestions:
EventID: 6802020C (hex)
"You have specified more than 7 standards for one or more calibration classes."
Severity: Informational
Further explanation: These have been truncated to 7 selections.
EventID: 6802020D (hex)
"No user calibration found for this channel."
Severity: Informational
Further explanation: A cal operation can not proceed until a calibration exists.
Suggestions: To find a calibration, you can select a Cal Set that contains the calibration needed for the current measurement.
EventID: 6802020E (hex)
"You do not need to acquire this standard for this calibration type."
Severity: Informational
Further explanation: This error can happen as a result of PROGRAMMATICALLY requesting the measurement of an un-needed calibration standard during a calibration procedure.
Suggestions: Check the specified cal type or eliminate the request for the measurement of the standard.
EventID: 6802020F (hex)
"Could not configure the Electronic Calibration system. Check to see if the module is plugged into the proper connector."
Severity: Informational
Further explanation: During an ECal operation, communication could not be established with the ECal module. The calibration will not be initiated until the presence of the ECal module is verified.
Suggestions: Verify the USB cable is connected properly. Disconnect and re-connect the cable to ensure the analyzer recognizes the module.
EventID: 68020210 (hex)
"DATA OUT OF RANGE: Design Limits Exceeded"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020211(hex)
"EXECUTION ERROR: Could not open ECal module memory backup file"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020212 (hex)
"EXECUTION ERROR: Access to ECal module memory backup file was denied"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020213 (hex)
"EXECUTION ERROR: Failure in writing to ECal module memory backup file"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020214 (hex)
"EXECUTION ERROR: Failure in reading from ECal module memory backup file"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020215 (hex)
"EXECUTION ERROR: Array index out of range"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020216 (hex)
"EXECUTION ERROR: Arrays wrong rank"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020217 (hex)
"EXECUTION ERROR: CPU"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020218 (hex)
"EXECUTION ERROR: Cannot ERASE module"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020219 (hex)
"EXECUTION ERROR: Cannot WRITE module"
Severity: Error
Further explanation:
Suggestions:
EventID: E802021A (hex)
"EXECUTION ERROR: Entry Not Found"
Severity: Error
Further explanation:
Suggestions:
EventID: E802021B (hex)
"EXECUTION ERROR: Invalid command while system is busy"
Severity: Error
Further explanation:
Suggestions:
EventID: E802021C (hex)
"Electronic Cal: Unable to orient ECal module. Please ensure the module is connected to the necessary measurement ports."
Severity: Error
Further explanation: There is no RF connection to the ECal module during a calibration step. An ECal orientation measurement has been attempted but the signal was not found.
Suggestions: Connect the ECal module RF connections to ports specified for the calibration step. The ECal module typically requires at least -18dBm for measurements. If your measurement requires the power level to be less than that, clear the Do orientation checkbox to bypass the automatic detection step.
EventID: E802021D (hex)
"EXECUTION ERROR: NO SPACE for NEW CAL, DELETE A CAL"
Severity: Error
Further explanation:
Suggestions:
EventID: E802021E (hex)
"EXECUTION ERROR: No More Room"
Severity: Error
Further explanation:
Suggestions:
EventID: E802021F (hex)
"EXECUTION ERROR: Other array error"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020220 (hex)
"EXECUTION ERROR: Ranks not equal"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020221 (hex)
"EXECUTION ERROR: Too few CONSTANT ranks"
Severity: Error
EventID: E8020222 (hex)
"EXECUTION ERROR: Too few VARYing ranks"
Severity: Error
EventID: E8020223 (hex)
"EXECUTION ERROR: Unknown error"
Severity: Error
EventID: E8020224 (hex)
"EXECUTION ERROR: ecaldrvr.dll bug or invalid module #"
Severity: Error
EventID: E8020225 (hex)
"EXECUTION ERROR: unexpected error code from ecal driver"
Severity: Error
EventID: E8020226 (hex)
"EXECUTION ERROR: unexpected internal driver error"
Severity: Error
EventID: E8020227 (hex)
"HARDWARE ERROR: Can't access ECal Interface Module"
Severity: Error
EventID: E8020228 (hex)
"HARDWARE ERROR: Can't release LPT port, reboot"
Severity: Error
EventID: E8020229 (hex)
"HARDWARE ERROR: VNA Error"
Severity: Error
EventID: E802022A (hex)
"HARDWARE ERROR: not enough data read from ECal module"
Severity: Error
EventID: E802022B (hex)
"OPERATION ABORTED BY HOST COMPUTER"
Severity: Error
EventID: E802022C (hex)
"OPERATION ABORTED BY USER"
Severity: Error
EventID: E802022D (hex)
"OUT OF MEMORY"
Severity: Error
EventID: E802022E (hex)
"QUERY INTERRUPTED:Message(s Abandoned"
Severity: Error
EventID: E802022F (hex)
"QUERY UNTERMINATED: INCOMPLETE PROGRAM Message"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020230 (hex)
"QUERY UNTERMINATED: NOTHING TO SAY"
Severity: Error
Further explanation:
Suggestions:
EventID: E8020231 (hex)
"QUEUE OVERFLOW"
Severity: Error
EventID: E8020232 (hex)
"SETTINGS CONFLICT: ADDITIONAL STANDARDS ARE NEEDED"
Severity: Error
EventID: E8020233 (hex)
"SETTINGS CONFLICT: Adapter Cal is NOT possible"
Severity: Error
EventID: E8020234 (hex)
"SETTINGS CONFLICT: COMMAND OUT OF SEQUENCE"
Severity: Error
EventID: E8020235 (hex)
"SETTINGS CONFLICT: Cal STOPPED - VNA SETUP CHANGED"
Severity: Error
EventID: E8020236 (hex)
"SETTINGS CONFLICT: Calibration is NOT in progress"
Severity: Error
EventID: E8020237 (hex)
"SETTINGS CONFLICT: Can't find specified GPIB board"
Severity: Error
EventID: E8020238 (hex)
"SETTINGS CONFLICT: Can't find/load gpib32.dll"
Severity: Error
EventID: E8020239 (hex)
"SETTINGS CONFLICT: Can't find/load sicl32.dll"
Severity: Error
EventID: E802023A (hex)
"SETTINGS CONFLICT: Can't initialize VNA (bad address?"
Severity: Error
EventID: E802023B (hex)
"SETTINGS CONFLICT: Can't load LPT port driver or USB driver DLL"
Severity: Error
EventID: E802023C (hex)
"SETTINGS CONFLICT: Invalid Calibration Sweep Mode."
Severity: Error
EventID: E802023D (hex)
"SETTINGS CONFLICT: Invalid Calibration Type"
Severity: Error
EventID: E802023E (hex)
"SETTINGS CONFLICT: Invalid Calibration"
Severity: Error
EventID: E802023F (hex)
"SETTINGS CONFLICT: Invalid GPIB board number specified"
Severity: Error
EventID: E8020240 (hex)
"SETTINGS CONFLICT: Invalid GPIB board type specified"
Severity: Error
EventID: E8020241 (hex)
"SETTINGS CONFLICT: Invalid Module Status"
Severity: Error
EventID: E8020242 (hex)
"SETTINGS CONFLICT: Invalid States"
Severity: Error
EventID: E8020243 (hex)
"SETTINGS CONFLICT: LPT port must be between 1 and 4"
Severity: Error
EventID: E8020244 (hex)
"Could not configure the Electronic Calibration system. Check to see if the module is properly connected."
Severity: Error
EventID: E8020245 (hex)
"SETTINGS CONFLICT: Specified LPT port does not exist"
Severity: Error
EventID: E8020246 (hex)
"SETTINGS CONFLICT: Use frequency domain for cal"
Severity: Error
EventID: E8020247 (hex)
"SETTINGS CONFLICT: Use step sweep type for cal."
Severity: Error
EventID: E8020248 (hex)
"SETTINGS CONFLICT: VNA address must be between 0 and 30"
Severity: Error
EventID: E8020249 (hex)
"SETTINGS CONFLICT: Wrong LPT port driver or USB driver DLL"
Severity: Error
EventID: E802024A (hex)
"SYNTAX ERROR: ECAL:DELAY command must have 2 numbers"
Severity: Error
EventID: E802024B (hex)
"SYNTAX ERROR: INCORRECT SYNTAX"
Severity: Error
EventID: E802024C (hex)
"SYNTAX ERROR: UNKNOWN COMMAND"
Severity: Error
EventID: E802024D (hex)
"Wrong port of module in RF path"
Severity: Error
EventID: E802024E (hex)
"User characterization not found in module"
Severity: Error
EventID: E802024F (hex)
Severity:Informational
"No source power calibration found for the channel and source port of the current measurement."
Further explanation: You tried to turn on source power cal but there is no source power cal data.
Suggestions: Perform a source power calibration
EventID: 68020250 (hex)
Severity:Informational
"A source power calibration sweep was not performed, so there is no correction for the channel and source port of the current measurement."
Further explanation: You tried to turn on source power cal but there is incomplete source cal data.
Suggestions:Perform a complete source power calibration
EventID: 68020251 (hex)
Severity: Informational
"A new trace could not be added to the active window for viewing the source power cal sweep, because it would have exceeded the limit on number of traces/window. Please remove a trace from the window before proceeding with source power cal."
Further explanation: The source power cal attempts to add a data trace to the active window. The active window already contains four traces.
Suggestions:Make the active window contain less than four traces.
EventID: 68020252 (hex)
Severity: Informational
"A new measurement could not be added for performing the source power cal sweep, because the limit on number of measurements has been reached. Please remove a measurement before proceeding with source power cal."
Further explanation: The source power cal attempts to add a measurement. The VNA already has the maximum number of measurements.
Suggestions: Delete a measurement.
EventID: 68020253 (hex)
Severity: Informational
"The calibration power value associated with the source power calibration of Port %1 on Channel %2 was changed with the calibration on. The calibration was not turned off, but the power value might no longer represent the calibration."
Further explanation: The source power cal accuracy is questionable.
Suggestions: If high accuracy is required, perform another source power calibration.
EventID: 68020254 (hex)
Severity: Informational
- Message that is passed from the power meter driver for a source power calibration. -
Further explanation: This error is generated by the power meter driver and passed through the VNA.
EventID: 68020255 (hex)
"During the acquisition of the sliding load standard, the slide was not properly moved to perform a circle fit. The standard's raw impedance was used to determine the directivity for one or more points."
Severity: Informational
Further Explanation: To accurately characterize the standard, the sliding load must be move sufficiently to ensure enough samples around the complex circle or Smith Chart. Under-sampling will cause an inaccurate result.
Suggestions: For best results when using a sliding load, be sure to use multiple slide positions that cover the full range of movement from front to back of the slot.
EventID: 68020256 (hex)
"This feature requires an unused channel, but could not find one. Please free up a channel and try again."
Severity: Informational
Further Explanation: You attempted to view an item within a calset. However, the calset viewer requires that the result be displayed in a channel that is not currently in use. All the channels are currently used. The view can not display the requested item.
Suggestions: You must delete at least one channel that is currently in use.
EventID: 68020257 (hex)
"Interpolation of the original calibration is not allowed since it was performed using Segment Sweep. Correction has been turned off."
Severity: Informational
EventID: 68020258 (hex)
"Cal preferences saved. Cal preference settings can be changed from the 'Cal Preferences' drop down Cal menu."
Severity: Informational
Further explanation: See Save Preference
EventID: 68020259 (hex)
"CalType not set."
Severity: Error
Further explanation: A cal operation can not proceed until a calibration exists or the proper cal type is selected.
Suggestions: This error can happen if the calibration can't be found. To find a calibration, you can select a Cal Set that contains the calibration needed for the current measurements. This error can also happen if a calibration type is not specified before attempting to programmatically execute cal acquisitions. Specify the cal type before beginning a calibration procedure.
EventID: E8020260 (hex)
"The Calibration feature requested is not implemented."
Further explanation: The specified cal type can be one of many choices. For example, response calibrations require single standards, 1-Port calibrations require 3 standards, and 2-Port calibrations require up to 12 standards.
Suggestions: Be sure to measure only the standards needed for the specified cal type.
EventID: E8020261 (hex)
"The Calibration Class Acquisition requested is not valid for the selected Calibration Type. Please select a different acquisition or a different Calibration Type."
EventID: E8020262 (hex)
"The Calibration Standard data required for the selected caltype was not found."
Severity: Error
Further explanation: An unsuccessful attempt was made to retrieve a specified standard from the raw measurement buffer. The buffer should contain the raw measurements of cal standards stored during a calibration procedure.
Suggestions: Be sure the requested standard is required for the current cal type. Not all standards are needed for all cal types.
EventID: E8020263 (hex)
" The Error Term data required for the selected caltype was not found."
Severity: Error
Further explanation: An unsuccessful attempt was made to retrieve a specified error term from the error correction buffer. The buffer should contain the error correction arrays for the current calibration.
Suggestions: Be sure the requested error term is required for the current cal type. Not all error terms are needed for all cal types.
EventID: E8020264 (hex)
The Calibration data set was not found.
Severity: Error
Further explanation: An unsuccessful attempt to access a cal set has been made. This may indicate a calset has been deleted or has been corrupted.
Suggestions: Try again or select another cal set. If the cal set appears in the cal set list, it may need to be deleted.
EventID: E8020265 (hex)
"The specified measurement does not have a calibration valid for Confidence Check. Please select a different measurement, or recall or perform a different Calibration Type."
Severity: Error
Further explanation: The measurement choice is prevented so that calibration will not be turned off. Not all cal types support all measurements. For example, an 1-Port cal on S11 can not be used to calibrate an S12 measurement. When a measurement is selected that does not have a calibration which can be applied, an informational message is displayed and calibration is turned off.
Suggestions: Use a full 2-Port calibration to be compatible with any S-Parameter.
EventID: E8020266 (hex)
" New calset created."
Severity: Informational message.
Further explanation: The newly created cal set will be automatically named and time stamped. If this is the beginning of a calibration procedure, the cal set will not be stored to memory until the calibration has completed successfully. The new cal set will be deleted if the calibration is canceled or does not otherwise complete successfully.
Suggestions: Informational
EventID: 68020267
The calset file: <x> appears to be corrupted and cannot be removed. Exit the application, remove the file, and restart.
Severity: Error
Suggestions: The cal set file is stored in the application home directory C:/Program Files/Keysight/Network Analyzer/PNACalSets.dat. Remove this file, then restart the application.
EventID: E8020269 (hex)
"The calset file: <x> load failed."
Severity: Error
Further explanation: The calset file contains a collection of calsets. The file resides on the hard drive.
Suggestions: Try restarting the application. If the failure persists, you may have to delete the cal set data file and restart the application. The cal set file is stored in the application home directory. C:/Program Files/Keysight/Network Analyzer/PNACalSets.dat. Remove this file, then restart the application.
EventID: E802027A (hex)
"The calset file: <x> save failed."
Severity: Error
Further explanation: The file operation detected an error. The save operation was aborted.
Suggestions: Retry.
EventID: E802027B (hex)
"A calset was deleted."
Severity: Informational
Further explanation: One of the calsets has been successfully deleted from the collection of calsets available. This can happen as the result of a user request or intentional operation.
Suggestions: None
EventID: 6802027C (hex)
"The version of the calset file: <x> is not compatible with the current instrument."
Severity: Error
Further explanation: A versioning error can prevent a calset from being used. This can happen as a result of instrument firmware upgrades.
Suggestions: If the versioning error is the result of firmware upgrade, you will have to re-install the old version of firmware to re-use the calset file. Or you can re-create the calsets with the current version of firmware.
The cal set file is stored in the application home directory C:/Program Files/Keysight/Network Analyzer/PNACalSets.dat. Remove this file, then restart the application.
EventID: E802027D (hex)
"Incompatible CalSets found: <x> of <y> stored calsets have been loaded."
Severity: Error
Further explanation: Errors were found on some of the calsets stored in the calset file. The errors may have been caused by versioning issues that may have corrupted the various calset keys.
Suggestions: Use the calset viewer to look at the contents of calset files. Delete the files that are corrupted.
EventID: 6802027E (hex)
"The Calset file: <x> was not found. A new file has been created."
Severity: Informational
Further explanation: The calset file should be stored on the hard drive. When the application is started, a search is done and the file is loaded if it can be found. If the file is not found, the analyzer will create a new file and display this message.
Suggestions: None
EventID: 6802027F (hex)
"The Calset specified is currently in use."
Severity: Error
Further explanation: This may indicate a conflict between multiple calset users attempting calibration tasks.
Suggestions: Save the instrument state. Preset the analyzer and recall the instrument state. This may abort any processes that may be in progress.
EventID: E8020280 (hex)
"The calset specified has not been opened."
Severity: Error
Further explanation: Multiple users may be attempting to access the calset.
Suggestions: Close multiple calset users so that only one user will access the calset.
EventID: E8020281 (hex)
"The maximum number of cal sets has been reached. Delete old or unused cal sets before attempting to create new ones."
Severity: Error
Suggestions: You may also delete the calsets data file.
The cal set file is stored in the application home directory. C:/Program Files/Keysight/Network_Analyzer/PNACalSets.dat. Remove this file, then restart the application.
EventID: E8020282 (hex)
The requested power loss table segment was not found.
Severity: Error
EventID: E8020283 (hex)
"A valid calibration is required before correction can be turned on."
Severity: Error
Further explanation: This usually indicates a calibration procedure has not run to completion or that the selected measurement does not have a valid calibration available from within the currently selected cal set.
Suggestions: To find a calibration, you can select a Cal Set that contains the calibration needed for the current measurements. This error can happen if a calibration type is not specified before attempting to programmatically execute cal acquisitions. Specify the cal type before beginning a calibration procedure.
EventID: E8020284 (hex)
The cal data for <x> is incompatible and was not restored. Please recalibrate."
Severity: Warning
Further explanation: None
Suggestions: None
EventID: A8020285 (hex)
"CalSet not loaded, version is too new."
Severity: Error
Further explanation: An old version of firmware is attempting to run with a new calset version. The version is incompatible.
Suggestions: The calset can be removed. You may also delete the calsets data file if you are migrating between various firmware revisions often and you would like to avoid this error. The cal set file is stored in the application home directory. C:/Program Files/Keysight/Network Analyzer/PNACalSets.dat. Remove this file, then restart the application.
EventID: E8020286 (hex)
"Custom cal type not found."
Severity: Error
Further explanation:
Suggestions:
EventID: E8020287 (hex)
"Custom correction algorithm defers to the client for interpolation."
Severity: Informational
EventID: 68020288 (hex)
"Custom cal dll threw an exception."
Severity: Error
EventID: E8020289 (hex)
"Could not load the ecal.dll library"
Severity: Error
EventID: E802028A (hex)
"The argument specified is not a valid cal type."
Severity: Error
EventID: E8020290 (hex)
"The function found existing interpolated data"
Severity: Informational
EventID: 68020291 (hex)
"The function computed new interpolation values."
Severity: Informational
EventID: 68020292 (hex)
"The source power measurement failed."
Severity: Error
Suggestions: Please check GPIB, power meter settings and sensor connections.
EventID: E8020293 (hex)
"Duplicate session found. Close session and retry."
Severity: Error
EventID: E8020294 (hex)
"The session does not exist. Open the session and try again."
Severity: Error
Further explanation:
EventID: E8020295 (hex)
"Attempt to launch a custom calibration failed."
Severity: Error
Further explanation:
EventID: E8020296 (hex)
"Request to measure a cal standard failed."
Severity: Error
Further explanation: Please ensure you are requesting to measure standards which are defined for this calibration.
EventID: E8020297 (hex)
"Since Electronic Calibration Kit is selected, Mechanical Cal Kit parameter cannot be changed."
Severity: Error
Further explanation:
EventID: E8020298 (hex)
"Frequencies of the active channel are below minimum or above maximum frequencies of the ECal module factory characterization."
Suggestions: Change the channel frequencies, or select another ECal module.
Severity: Error
EventID: E8020299 (hex)
"Calset chosen for characterizing the ECal Module Ports %1 does not contain a calibration for VNA Ports %2."
Severity: Error
Suggestions: Go back to select another calset or to perform another cal.
EventID: E802029A (hex)
"ECal module only has sufficient memory remaining to store a maximum of %1 points in User Characterization %2."
Severity: Error
Suggestions: Decrease your number of points, or choose to overwrite another user characterization.
EventID: E802029B (hex)
Input values are non-monotonic. Cannot interpolate.
Severity: Error
EventID: E802029C (hex)
Interpolation target is out of range. Cannot interpolate.
Severity: Error
EventID: E802029D (hex)
Guided Calibration Error: <>
Severity: Error
EventID: E802029E (hex)
The first call to the guided calibration interface must be Initialize.
Severity: Error
EventID: E802029F (hex)
The selected thru cal method was not recognized.
Severity: Error
EventID: E80202A0 (hex)
Could not generate the error terms.
Severity: Error
EventID: E80202A1 (hex)
Guided calibration must be performed on the active channel
Severity: Error
EventID: E80202A2 (hex)
You can not start using calibration steps until you have successfully called generate steps.
Severity: Error
EventID: E80202A3 (hex)
The step number given is out of range. Step numbers should be between 1 and the number of steps. 0 is not a valid step number.
Severity: Error
EventID: E80202A4 (hex)
A calset was selected for channel: <n> without restoring stimulus.
Severity: Informational
EventID: 680202A5 (hex)
A calset was selected for channel: <n> restoring stimulus.
Severity: Informational
EventID: 680202A6 (hex)
The selected calset stimulus could not be applied to the channel.
Severity: Informational
EventID: 680202A7 (hex)
You attempted to measure power at a frequency outside the frequency range defined for the specified power sensor. Select another sensor or adjust the range for this sensor.
Severity: Error
EventID: E80202A8 (hex)
Specified frequency is outside the frequency ranges currently defined for the power meter's sensors.
Severity: Error
EventID: E80202A9 (hex)
Additional Calibration Standards need to be acquired in order to calibrate over the entire frequency range currently being measured.
Severity: Informational
EventID: 680202AA (hex)
The VNA failed to convert cal kits for use by unguided calibrations. The recommended action is to restore Cal Kit defaults.
Severity: Error
EventID: E80202AB (hex)
The VNA failed to convert cal kits for use by unguided calibrations. CalKit defaults have been restored.
Severity: Error
EventID: E80202AC (hex)
Power meter is reserved by a source power cal acquisition already in progress.
Severity: Error
EventID: E80202AD (hex)
Source power calibration has not been performed or uploaded for the specified channel and source port.
Severity: Error
EventID: E80202AE (hex)
Source power calibration data array size for the specified channel and source port does not match it's associated stimulus number of points.
Severity: Error
EventID: E80202AF (hex)
Source power calibration of Port <n> on Channel <n> was turned off because the correction array no longer exists.
Severity: Error
EventID: E80202B0 (hex)
This command can only be used on a measurement created with a specified calibration loadport.
Severity: Error
EventID: E80202B1 (hex)
Interpolation is turned off and you have changed the stimulus settings of the original calibration, so correction has been turned off.
Severity: Error
EventID: E80202B2 (hex)
Stimulus settings for your current instrument state exceeded the parameters of the original calibration, so correction has been turned off.
Severity: Error
EventID: E80202B3 (hex)
Fixturing: the requested S2P file cannot be read. Possible formatting problem.
Severity: Error
EventID: E80202B4 (hex)
Fixturing: the requested S2P file cannot be opened.
Severity: Error
EventID: E80202B5 (hex)
Fixturing: the requested S2P file cannot be interpolated. This is usually because the frequency range in the file is a subset of the current channel frequency range.
Severity: Error
EventID: E80202B6 (hex)
Cal Registers can only be used by one channel: the channel conveyed in the name of the cal register. The name cannot be changed.
Severity: Error
Further explanation: See Cal Registers
EventID: E80202B7 (hex)
Fixturing: cannot be enabled with Response Calibrations and has been turned off.
Severity: Error
EventID: E80202B8 (hex)
The selected calibration cannot be performed for this measurement.
Severity: Error
EventID: E80202B9 (hex)
Fitting: RemoveAllConnectors() should be called prior to calling AddConnector after a fit has been attempted.
Severity: Error
EventID: E80202BA (hex)
An attempt was made to acquire calibration data before the system was properly initialized.
Severity: Error
EventID: E80202BB (hex)
Use IGuidedCalibration for multiport calibration types.
Severity: Error
EventID: E80202BC (hex)
Guided calibration requires number of thru measurement paths be at least equal to the number of calibration ports minus 1.
Severity: Error
EventID: E80202BD (hex)
A thru path was specified that includes a port which the calibration was not specified to include.
Severity: Error
EventID: E80202BE (hex)
One or more of the ports to be calibrated was not found in the set of specified thru paths.
Severity: Error
EventID: E80202BF (hex)
Input power too high. Source power is off.
Severity: Warning
EventID: A8030302 (hex)
Source power restored.
Severity: Informational
EventID: 68030303 (hex)
"The spampnp.sys driver is not working. Check system hardware. ! Data will be simulated. !"
Severity: Error
Further explanation: The Network Analyzer application cannot locate the DSP board. Hardware or a driver may be malfunctioning. This is also common when attempting to run the Network Analyzer on a workstation.
EventID: E8030304 (hex)
"Instrument Serial Bus Not Working."
Severity: Error
Further explanation: The instrument EEPROM appears to contain either all ones or all zeros. A serial bus hardware failure prevents reading the EEPROM.
EventID: E8030305 (hex)
Unleveled, source <n>, out <n>.
Severity: Error
Further explanation: The VNA was unable to set the power on port <n> to the desired level
"Phase lock lost"
Severity: Error
Further explanation: The instrument source was not able to lock properly. This can be the result of broken hardware, poor calibration, or bad EEPROM values.
Suggestions: Perform source calibration. Click System / Service / Adjustments / Source Calibration
EventID: E8030350 (hex)
Phaselock restored.
Severity: Success
EventID: 0x28030351 (hex)
"Unknown hardware error."
Severity: Error
Further explanation: Hardware malfunctioned prevents communication with the DSP.
EventID: E8030352 (hex)
DSP communication lost.
Severity: Error
EventID: E8030353 (hex)
RF power off.
Severity: Error
EventID: E8030354 (hex)
RF power on.
Severity: Success
EventID: 28030355 (hex)
Hardware OK.
Severity: Success
EventID: 28030356 (hex)
"Source unleveled."
Severity: Error
Further explanation: The source was unable to properly level at the requested power. The indicated power may not be accurate.
Suggestions: Try a different power level. Recalibrate source, if problem persists.
EventID: E8030357 (hex)
Source leveled.
Severity: Success
EventID: 28030358 (hex)
Input overloaded.
Severity: Error
EventID: E8030359 (hex)
Input no longer overloaded.
Severity: Success
EventID: 2803035A (hex)
"Yig calibration failed."
Severity: Error
Further explanation: Internal self-calibration of YIG oscillator tuning failed.
EventID: E803035B (hex)
Yig calibrated.
Severity: Success
EventID: 2803035C (hex)
"Analog ramp calibration failed."
Severity: Error
Further explanation: Internal analog sweep ramp calibration has failed.
EventID: E803035D (hex)
Analog ramp calibrated.
Severity: Success
EventID: 2803035E (hex)
Source temperature high.
Severity: Error
EventID: E803035F (hex)
Source temperature OK.
Severity: Success
EventID: 28030360 (hex)
"EEPROM write failed."
Severity: Error
Further explanation: Attempt to store calibration data to EEPROM has failed. There is a possible hardware failure.
EventID: E8030361 (hex)
EEPROM write succeeded.
Severity: Success
EventID: 28030362 (hex)
Attempted I/O write while port set to read only.
Severity: Error
Further explanation: Attempt to write to an I/O data port while the port set to input/read only.
Suggestions: Set data port to write/output before attempting to write to port.
EventID: E8030363 (hex)
" Attempted I/O read from write only port.
Severity: Error
Further explanation: Attempt to read from an I/O data port while the port set to output/write only.
Suggestions: Set data port to read/input before attempting to read from port.
EventID: E8030364 (hex)
Invalid hardware element identifier.
Severity: Error
EventID: E8030365 (hex)
Invalid gain level setting.
Severity: Error
EventID: E8030366 (hex)
Device driver was unable to allocate enough memory. Please try rebooting.
Severity: Error
EventID: E8030367 (hex)
DSP Error. Please Contact Keysight Support. Technical Information: DSP Type 1
Severity: Error
EventID: E8030368 (hex)
DSP Error. Please Contact Keysight Support. Technical Information: DSP Type 2
Severity: Error
EventID: E8030369 (hex)
DSP Error. Please Contact Keysight Support. Technical Information: DSP Type 3
Severity: Error
EventID: E803036A (hex)
DSP Error. Please Contact Keysight Support. Technical Information: DSP Type 4
Severity: Error
EventID: E803036B (hex)
DSP Error. Please Contact Keysight Support. Technical Information: DSP Type 5
Severity: Error
EventID: E803036C (hex)
The trigger connection argument was not recognized as valid by the firmware.
Severity: Error
EventID: 0xE803038E (hex)
The trigger connection specified does not support this trigger behavior
Severity: Error
EventID: E803038F (hex)
The trigger behavior specified was not recognized as valid by the firmware.
Severity: Error
EventID: E8030390 (hex)
The trigger connection specified does not physically exist on this network analyzer
Severity: Error
EventID: E8030391 (hex)
Cannot set "Accept Trigger Before Armed", since this hardware configuration does not support edge triggering.
Severity: Error
EventID: E8030392 (hex)
Cannot set "Trigger Output Enabled", since this hardware configuration does not support BNC2.
Severity: Error
EventID: E8030393 (hex)
Exceeded maximum trigger delay.
Severity: Error
EventID: E8030394 (hex)
Exceeded minimum trigger delay.
Severity: Error
EventID: E8030395 (hex)
If you are going to display or otherwise use a memory trace, you must first store a data trace to memory.
Severity: Warning
EventID: A8040400 (hex)
"The measurement failed to shut down properly. The application is in a corrupt state and should be shut down and restarted."
Severity: Error
Further explanation: This message is displayed if the VNA application becomes corrupt. If you continue to get this error, please call customer service
EventID: E8040401 (hex)
The measurement failed to shut down properly. The update thread failed to exit properly.
Severity: Warning
EventID: A8040402 (hex)
"Group Delay format with CW Time or Power sweeps produces invalid data."
Severity: Warning
Further explanation: Group Delay format is incompatible with single-frequency sweeps. Invalid data is produced.
Suggestions: Ignore the data or choose a different format or sweep type.
EventID: A8040403 (hex)
Severity: Informational
"MSG_LIMIT_FAILED"
Further explanation: Limit line test failed.
EventID: 68040404 (hex)
Severity: Informational
"MSG_LIMIT_PASSED"
Further explanation: Limit line test passed.
EventID: 68040405 (hex)
"Exceeded the maximum number of measurements allowed."
Severity: Warning
Further explanation: See Traces, Channels, and Windows on the VNA for learn about maximum measurements.
EventID: A8040406 (hex)
"Network Analyzer Internal Error. Unexpected error in AddNewMeasurement."
Severity: Warning
Further explanation: If you continue to get this message, contact product support.
EventID: A8040407 (hex)
"No measurement was found to perform the selected operation. Operation not completed."
Severity: Warning
Further explanation: None
Suggestions:Create a measurement before performing this operation.
EventID: A8040408 (hex)
The Markers All Off command failed.
Severity: Warning
EventID: A8040409 (hex)
"A memory trace has not been saved for the selected trace. Save a memory trace before attempting trace math operations."
Severity: Warning
Further explanation: Must have a memory trace when trying to do Trace Math,
EventID: A804040A (hex)
"MSG_SET_AVERAGE_COMPLETE"
Severity: Informational
Further explanation: Informational for COM programming. Averaging factor has been reached.
EventID: 6804040B (hex)
"MSG_CLEAR_AVERAGE_COMPLETE"
Further explanation: Informational for COM programming. Averaging factor has NOT been reached.
EventID: 6804040C (hex)
"Time Domain transform requires at least 3 input points. The transform has been deactivated."
Severity: Informational
Further explanation: None
Suggestions:Increase the number of points.
EventID: 6804040D (hex)
Smoothing requires a scalar format, and has been deactivated.
Severity: Informational
EventID: 6804040E (hex)
A receiver power calibration in this instrument state file cannot be recalled into this firmware version.
Severity: Warning
EventID: A804040F (hex)
Could not achieve target power.
Severity: Error
Further explanation: This indicates that the VNA was unable to find a source power during the THRU step of the cal sufficiently high to boost the measured noise power on port 2 to 6 dB above the noise floor.
"Exceeded limit on number of measurements."
Severity: Error
Further explanation: See Traces, Channels, and Windows on the VNA for measurement limits.
EventID: E8040450 (hex)
"Parameter not valid."
Severity: Error
Further explanation: A measurement parameter that was entered programmatically is not valid.
EventID: E8040451 (hex)
"Measurement not found."
Severity: Error
Further explanation: Any of these could be the cause:
Trying to calibrate but already have maximum measurements.
Trying to do a confidence check but there is not a measurement.
Trying to create, activate, or alter a measurement through COM that has been deleted through the front panel.
Trying to use a trace name through programming that is not unique.
EventID: E8040452 (hex)
"No valid memory trace."
Severity: Error
Further explanation: Must have a memory trace when trying to do Trace Math,
Suggestions: Store a memory trace.
EventID: E8040453 (hex)
"The reference marker was not found."
Severity: Error
Further explanation: Attempted to create a delta marker without first creating a reference marker (COM only).
EventID: E8040454 (hex)
"Data and Memory traces are no longer compatible. Trace Math has been turned off."
Severity: Error
Further explanation: Warning - channel setting has changed while doing trace math.
Suggestions:Store another memory trace and turn trace math back on.
EventID: A8040455 (hex)
"Data and Memory traces are not compatible. For valid trace math operations, memory and data traces must have similar measurement conditions."
Severity: Error
Further explanation: Tried to do trace math without compatible data and memory traces.
Suggestions: Store another memory trace.
EventID: E8040456 (hex)
"Marker Bandwidth not found."
Severity: Error
Further explanation: Could not find a portion of trace that meets the specified bandwidth criteria.
EventID: E8040457 (hex)
"The peak was not found."
Severity: Error
Further explanation: Could not find portion of trace that meets peak criteria.
Suggestions: See Marker Peak criteria.
EventID: E8040458 (hex)
"The target search value was not found."
Severity: Error
Further explanation: Could not find interpolated data point that meets search value.
EventID: E8040459 (hex)
"Reflection measurement, such as S11, must supply an auxiliary port to disambiguate 2-port measurements on multiport instruments."
Severity: Error
Further explanation:
EventID: E804045A (hex)
"The receiver power calibration has been turned off because the type of measurement or source port has changed, so the calibration is no longer valid."
Severity: Warning
Further explanation:
EventID: A804045B (hex)
"Receiver power cal requires the active measurement to be of unratioed power."
Severity: Warning
Further explanation:
EventID: A804045C (hex)
"There is currently no source power calibration associated with the channel and source port of the active measurement. A source power cal should be performed or recalled before performing a receiver power calibration."
Severity: Warning
Further explanation:
EventID: A804045D (hex)
"The attempted operation can only be performed on a standard measurement type."
Severity: Error
Further explanation:
EventID: E804045E (hex)
"The custom measurement cannot be loaded because it is not compatible with the Network Analyzer hardware."
Severity: Error
Further explanation:
Suggestions:
EventID: E804045F (hex)
"The custom measurement cannot be loaded because it is not compatible with the Network Analyzer software."
Severity: Error
Further explanation:
EventID: E8040460 (hex)
"The custom measurement load operation failed for an unspecified reason."
Severity: Error
Further explanation:
EventID: E8040461 (hex)
"The custom measurement data processing has generated an unhandled exception, and will be terminated. The VNA software may be in an unstable state and it is recommended that the VNA software be shutdown and restarted."
Severity: Error
Further explanation:
EventID: E8040462 (hex)
"The attempted operation can only be performed on a custom measurement type."
Severity: Error
Further explanation:
EventID: E8040463 (hex)
"The requested custom measurement is not available."
Severity: Error
Further explanation:
EventID: E8040464 (hex)
"The requested custom algorithm was not found."
Severity: Error
Further explanation:
EventID: E8040465 (hex)
"Normalization cannot be turned on because the measurement does not have a valid divisor buffer."
Severity: Error
Further explanation:
EventID: E8040466 (hex)
"The Raw Data requested by the measurement could not be provided."
Severity: Warning
Further explanation:
EventID: A8040467 (hex)
"The selected Sweep Type does not allow Transform and Gating. Transform and Gating disabled. "
Severity: Error
Further explanation:
EventID: E8040468 (hex)
Memory trace can not be applied to this measurement
Severity: Error
EventID: E8040469 (hex)
Normalization can not be applied to this measurement
Severity: Error
EventID: E804046A (hex)
The data provided has an invalid number of points. It could not be stored
Severity: Error
EventID: E804046B (hex)
The measurement stored in the save/recall state has an invalid version. It could not be loaded
Severity: Error
EventID: E804046C (hex)
This data format argument for this operation must be "naDataFormat_Polar"
Severity: Error
EventID: E804046D (hex)
This data format argument for this operation must be a scalar data format
Severity: Error
EventID: E804046E (hex)
The memory trace is not valid for the current measurement setup.
Severity: Error
EventID: E804046F (hex)
This measurement is incompatible with existing measurements in this channel. Choose another channel.
Severity: Error
EventID: E8040470 (hex)
Port extension correction is not available for offset frequency measurements. Port extension correction has been disabled.
Severity: Error
EventID: E8040471 (hex)
Physical port number assignments for logical port mappings must be unique.
Severity: Error
EventID: E8040472 (hex)
"You have sent a read command to the analyzer without first requesting data with an appropriate output command. The analyzer has no data in the output queue to satisfy the request."
Severity: Error
EventID: 68050501 (hex)
"You must remove the active controller from the bus or the controller must relinquish the bus before the analyzer can assume the system controller mode."
Severity: Error
EventID: E8050502(hex)
"The analyzer did not receive a complete data transmission. This is usually caused by an interruption of the bus transaction."
Severity: Error
EventID: E8050503 (hex)
"The instrument status byte has changed."
Severity: Informational
EventID: 68050504 (hex)
"The SCPI command received has caused error number %1: "%2"."
Severity: Informational
EventID: 68050505 (hex)
"The INET LAN server has been started as process number %1."
Severity: Informational
EventID: 68050506 (hex)
"Execution of the SCPI command has failed"
Severity: Error
EventID: E8050550 (hex)
" The INET/LAN device is not accessible."
Severity: Error
EventID: E8050551 (hex)
"The INET/LAN driver was not found. "
Severity: Error
EventID: E8050552 (hex)
"The INET/LAN driver was not found."
Severity: Error
EventID: E8050553 (hex)
"The INET/LAN device is unable to acquire the necessary resources. "
Severity: Error
EventID: E8050554 (hex)
"The INET/LAN device generated a generic system error. "
Severity: Error
EventID: E8050555 (hex)
"Invalid address for the INET/LAN device."
Severity: Error
EventID: E8050556 (hex)
"The INET I/O library was not found. "
Severity: Error
EventID: E8050557 (hex)
"An error occured in the INET system. "
Severity: Error
EventID: E8050558 (hex)
"Access to the INET/LAN driver was denied. "
Severity: Error
EventID: E8050559 (hex)
"Could not load error system message dll."
Severity: Error
EventID: E805055A (hex)
"ErrorSystemMessage.dll does not export the right function."
Severity: Error
EventID: E805055B (hex)
"Custom scpi library was not able to be knitted"
Severity: Error
EventID: E805055C (hex)
"Could not knit the scpi error messages from the ErrorSystemMessage lib"
Severity: Error
EventID: E805055D (hex)
Command is obsolete with this software version.
Severity: Error
EventID: E808055E (hex)
CALC measurement selection set to none. Use Calc:Par:Sel
Severity: Error
EventID: E808055F (hex)
"Parser got command: %1."
Severity: Informational
EventID: 680505FF (hex)
"Exceeded the maximum of 4 traces in each window. The trace for <x> will not be added to window <x>."
Severity: Warning
Further explanation: None
Suggestions: Create the trace in another window. See the VNA window limits.
EventID: A8060600 (hex)
"Exceeded the maximum of 16 data windows. New window will not be created."
Severity: Warning
Further explanation: None
Suggestions: Create the trace in an existing window. See the VNA window limits.
EventID: A8060601 (hex)
"No Data Windows are present. Unable to complete operation."
Severity: Warning
Further explanation: Your remote SCPI operation tried to create a new measurement while there were no windows present
Suggestions: Create a new window before creating the measurement. See example Create a measurement using SCPI
EventID: A8060602 (hex)
"No data traces are present in the selected window. Operation not completed."
Severity: Warning
Further explanation: None
EventID: A8060603 (hex)
"Cannot complete request to arrange existing measurements in <x> windows due to the limit of <x> traces per window."
Severity: Informational
Further explanation: The arrange window feature cannot put the existing traces into the number of windows you requested because only 4 traces per window are allowed. See Arranging Existing Measurements
Suggestions:Either create more windows or delete some traces.
EventID: 68060604 (hex)
"Unable to establish a connection with the specified printer."
Severity: Warning
Further explanation: None
Suggestions: Refer to Printer Help
EventID: A8060605 (hex)
"Printout canceled."
Severity: Informational
EventID: 68060606 (hex)
"Window not found."
Severity: Error
Further explanation: A window was specified in your program which does not exist.
Suggestions: Query the name of your window before specifying.
EventID: E8060650 (hex)
"Duplicate window ID specified."
Severity: Error
Further explanation: None
EventID: E8060651 (hex)
"Exceeded limit on number of windows."
Severity: Error
Further explanation: There is a limit of 4 windows per screen.
EventID: E8060652 (hex)
"Exceeded limit on number of traces/window."
Severity: Error
Further explanation: There is a limit of 4 traces per window. See the Traces, Channels, and Windows on the VNA.
Suggestions: Create the trace in another window
EventID: E8060653 (hex)
"Trace not found."
Severity: Error
Further explanation: Your program tried to communicate with a non-existing trace.
Suggestions:Query the trace ID before writing to it.
EventID: E8060654 (hex)
"The operating system does not recognize this printer."
Severity: Warning
EventID: A8060655 (hex)
Duplicate trace ID specified.
Severity: Error
EventID: E8060656 (hex)
"Sweep Complete."
Severity: Informational
Further explanation: None
Suggestions:None
EventID: 68070700 (hex)
"All triggerable acquisitions have completed."
Severity: Informational
Further explanation:
EventID: 68070701 (hex)
"The last trigger produced an aborted sweep."
Severity: Informational
Further explanation:
EventID: 68070702 (hex)
"The segment list must be adjusted to have at least one active segment with more than 0 points to use segment sweep."
Severity: Informational
Further explanation: You attempted to change Sweep type to Segment sweep, but there is either no segments defined or no sweep points in the defined segments
Suggestions: Define at least one segment with at least one measurement point. See Segment sweep for more information
EventID: 68070703 (hex)
"MSG_SET_CHANNEL_DIRTY"
Severity: Informational
Further explanation: This informational message occurs when a channel setting has changed but the channel still has data that was taken with the previous setting. The following CLEAR message occurs when new channel data is taken.
EventID: 68070704 (hex)
"MSG_CLEAR_CHANNEL_DIRTY"
Severity: Informational
Further explanation: The previous SET message occurs when a channel setting has changed but the channel still has data that was taken with the previous setting. This CLEAR message occurs when new channel data is taken.
EventID: 68070705 (hex)
Sweep time has changed from Auto to Manual mode. If desired to return to Auto mode, enter sweep time value of 0.
Severity: Informational
EventID: 68070706 (hex)
"Set Sweep Completed"
Severity: Informational
Further explanation: This event occurs when a sweep and it's associated sweep calculations finish. This is typically when all sweeps on a channel complete.
EventID: 68070707 (hex)
"Clear Sweep Completed"
Severity: Informational
Further explanation: This event occurs immediately after the SET SWEEP COMPLETED event. These two events set and clear the "Sweep Completed" bit (bit 4) on the SCPI Device Status register.
EventID: 68070708 (hex)
"All Sweeps Completed and Processed"
Severity: Informational
Further explanation: This event occurs when all of the sweeps and sweep calculations are complete for a channel.
EventID: 68070709 (hex)
Low Pass : Frequency limits have been changed.
Severity: Informational
EventID: 6807070A (hex)
Low Pass : Number of points have been changed.
Severity: Informational
EventID: 6807070B (hex)
Low Pass : Frequency limits and number of points have been changed.
Severity: Informational
EventID: 6807070C (hex)
"Channel created"
Severity: Informational
EventID: 6807070D (hex)
"Channel deleted"
Severity: Informational
EventID: 6807070E (hex)
"Channel not found."
Severity: Error
Further explanation: A non-existent channel is being referenced under program control.
Suggestions: Query the channel number, then refer to it by number.
EventID: E8070750 (hex)
"The requested sweep segment was not found."
Severity: Error
Further explanation: A non-existent sweep segment is being referenced under program control.
EventID: E8070751 (hex)
"The sweep segment list is empty."
Severity: Error
Further explanation: Segment Sweep cannot be specified unless there is at least one defined segment. This error will only occur under remote control.
EventID: E8070752 (hex)
"The number of points in active sweep segment list segments is 0."
Severity: Error
Further explanation: Segment Sweep cannot be specified unless there is at least data point specified in a segment. This error will only occur under remote control.
EventID: E8070753 (hex)
"The specified source attenuator is not valid."
Severity: Error
Further explanation: You tried to set the Attenuator property on the Channel object on a VNA that doesn't have a source attenuator.
EventID: E8070754 (hex)
"Log Frequency sweep cannot be selected with the current Number of Points. Please reduce Number of Points."
Severity: Error
Further explanation: The maximum number of points that can be used for Log sweep is 401.
EventID: E8070755 (hex)
"The requested Number of Points is greater than can be selected for Log Frequency sweep."
Severity: Error
Further explanation: The maximum number of points that can be used for Log sweep is 401.
EventID: E8070756 (hex)
"Response frequencies exceeded instrument range so Frequency Offset has been turned off."
Severity: Error
Further explanation: This error is returned whenever the instrument detects that the stimulus sweep setup and Frequency Offset settings result in computed response frequencies that exceed instrument limits. When this occurs, the instrument automatically turns off Frequency Offset to avoid the out-of-range conditions.
Suggestions: When this condition has occurred, change settings for either the stimulus frequencies or Frequency Offset so that the Response frequencies are within instrument bounds. Once this is done, Frequency Offset can once again be turned on.
EventID: E8070757 (hex)
The total number of points for all the given segments exceeds the maximum number of points supported. The segments were not changed.
Severity: Error
EventID: E8070758 (hex)
This instance of the Channels object was not used to place the channels in Hold, so no channels were resumed.
Severity: Error
EventID: E8070759 (hex)
The port number was outside the range of allowed port numbers.
Severity: Error
EventID: E807075A (hex)
More ports than are present are required for this operation.
Severity: Error
EventID: E807075B (hex)
"The function you requested requires a capability provided by an option to the standard analyzer. That option is not currently installed."
Severity: Error
Further explanation: None
Suggestions:To view the options on your analyzer, click Help / About Network Analyzer. For more information see VNA Options
EventID: 68080800 (hex)
"The feature you requested is not available on the current instrument."
Severity: Error
Further explanation: None
EventID: 68080801 (hex)
"The feature you requested is incompatible with the current instrument state."
Severity: Error
Further explanation: None
Suggestions: None
EventID: 68080802 (hex)
"File<x> has been saved."
Severity: Informational
Further explanation: None
EventID: 68080803 (hex)
"Attempt to save <x> failed."
Severity: Error
Further explanation: None
Suggestions: If using a floppy disk, ensure it is inside the drive and the disk is not full. Check the filename for special characters.
EventID: E8080804 (hex)
"Attempt to recall file failed because <x> was not found."
Severity: Error
Further explanation: None
EventID: E8080805 (hex)
"<x> has a bad header."
Severity: Error
Further explanation: None
Suggestions: Recopy the file and / or delete the file.
EventID: E8080806 (hex)
"Request to enter hibernate state."
Further explanation: None
EventID: 68080808 (hex)
"Power up from automatic hibernate state. Program received PBT_APMRESUMEAUTOMATIC Message."
Further explanation: None
EventID: 68080809 (hex)
"Power up from suspend hibernate state. Program received PBT_APMRESUMESUSPEND Message."
Further explanation: None
EventID: 6808080A (hex)
"Power up from suspend hibernate state. Program received PBT_APMRESUMECRITICAL Message."
Severity: Warning
Further explanation: None
EventID: A808080B (hex)
"Power up from unknown hibernate state UI recovery called. Program received no PBT_Message within the time allotted and is attempting recovery."
Severity: Warning
Further explanation: None
EventID: A808080C (hex)
"<x> already exists. File is being overwritten."
Further explanation: Used only for remote applications
EventID: 6808080D (hex)
"File has not been saved."
Severity: Error
Further explanation: Used only for remote applications
EventID: E808080E (hex)
"File <x> has been recalled."
Further explanation: Used only for remote applications
EventID: 6808080F (hex)
"State version in <x> is considered obsolete by this version of this code."
Severity: Error
Further explanation: You attempted to recall a file that is no longer valid.
Suggestions: You must recreate the file manually.
EventID: E8080810 (hex)
"State version in <x> is newer than the latest version supported by this code."
Severity: Error
Further explanation: You attempted to recall a file that was created by a later version of the VNA application.
Suggestions: You must recreate the file manually.
EventID: E8080811 (hex)
"Error occurred while reading file <x>"
Severity: Error
Further explanation: The file may be corrupt.
Suggestions: Try to recreate the file.
EventID: E8080812 (hex)
"Windows shell error: <x>"
Severity: Error
Further explanation: None
EventID: E8080813 (hex)
Send message timed out returning: <x>.
Severity: Error
Further explanation: None
EventID: E8080814 (hex)
"Changing GPIB mode to System Controller."
Severity: Informational
Further explanation: None
EventID: 68080815 (hex)
"Changing GPIB mode to Talker Listener."
Severity: Informational
Further explanation: None
EventID: 68080816 (hex)
"The Network Analyzer can not be put in GPIB System Controller mode until the GPIB status is Local. Stop any remote GPIB programs which may be using the Network analyzer, press the Macro/Local key and try again. "
Severity: Informational
Further explanation: See LCL and RMT Operation
Suggestions: Press the Macro/Local key and try again.
EventID: 68080817 (hex)
"This method can not be invoked through a late-bound COM call."
Severity: Error
Further explanation: None
Suggestions: Use the alternate method described in the COM programming documentation
EventID: E8080878 (hex)
"The specified format is invalid."
Severity:Error
Further explanation: None
EventID: E8080850 (hex)
"WINNT exception caught by Automation layer."
Severity: Error
Further explanation: None
EventID: E8080851 (hex)
"Bad port specification."
Severity: Error
Further explanation: None
EventID: E8080852 (hex)
"Failed to find a printer."
Severity: Error
Further explanation: None
Suggestions: See Connecting to a Printer
EventID: E8080853 (hex)
"Manual trigger ignored."
Severity: Error
Further explanation: None
EventID: E8080854 (hex)
"Attempt to set trigger failed."
Severity: Error
Further explanation: None
EventID: E8080855 (hex)
"Macro execution failed."
Severity: Error
Further explanation: None
EventID: E8080856 (hex)
"Specified macro definition is incomplete."
Severity: Error
Further explanation:
EventID: E8080857 (hex)
"Block data length error."
Severity: Error
Further explanation: See Getting Data from the Analyzer
EventID: E8080859 (hex)
"Requested data not found."
Severity: Error
Further explanation: None
EventID: E808085B (hex)
"The parameter supplied was out of range, so was limited to a value in range before being applied to the instrument."
Severity: Success
Further explanation: None
Suggestions: View range limits before sending programming commands.
EventID: 2808085E (hex)
The parameter supplied was out of range, so was limited to a value in range before being applied to the instrument.
Severity: Error
EventID: E808085F (hex)
"Request failed. The required license was not found."
Severity: Error
Further explanation: None
EventID: E8080860 (hex)
"A remote call to the front panel has returned hresult <x>"
Severity: Error
Further explanation: This may indicate a problem with the front panel
Suggestions: Contact Technical support
EventID: E8080861 (hex)
The recall operation failed.
Severity: Error
Further explanation:
EventID: E8080862 (hex)
Attempt to save file failed.
Severity: Error
Further explanation:
EventID: E8080863 (hex)
Recall attempt failed because file was not found.
Severity: Error
Further explanation:
EventID: E8080864 (hex)
Recall file has a bad header.
Severity: Error
Further explanation:
EventID: E8080865 (hex)
Recall file version is obsolete and no longer compatible with this instrument.
Severity: Error
Further explanation:
EventID: E8080866 (hex)
The recall file contains an istate version newer than this instrument. A remote call to the front panel has returned hresult %1
Severity: Error
Further explanation:
EventID: E8080867 (hex)
"Front Panel <x>
Severity: Error
Further explanation: None
EventID: E8080868 (hex)
"Front Panel message"
Severity: Informational
Further explanation: None
EventID: 68080869 (hex)
"Power Service <x>
Severity: Error
Further explanation: There is more than 1 instance of powerservice running. There should only be one running. This might happen after running install shield - especially when upgrading the CPU board.
Suggestions: Try rebooting. If this persists, please call Customer Support.
EventID: E808086A (hex)
"Power Service <x>
Severity: Informational
Further explanation: None
EventID: 6808086B (hex)
"The Keysight Technologies GPIB driver can not be loaded or unloaded."
Severity: Error
Further explanation: None
Suggestions: If the problem persists, from the VNA desktop, right-click on My Computer. Click Properties, Click Hardware Tab. Click Device Manager Button. Expand GPIB Devices. Right-click and click Uninstall all GPIB interfaces devices. Reboot the VNA.
EventID: E808086C (hex)
"The National Instruments GPIB driver can not be loaded or unloaded."
Severity: Error
Further explanation: None
Suggestions: If the problem persists, from the VNA desktop, right-click on My Computer. Click Properties, Click Hardware Tab. Click Device Manager Button. Expand GPIB Devices. Right-click and click Uninstall all GPIB interfaces devices. Reboot the VNA.
EventID: E808086D (hex)
"The Keysight GPIB driver is loaded but it can not start its parser."
Severity: Error
Further explanation: None
EventID: E808086E (hex)
The front panel is in remote mode.
Severity: Warning
EventID: A808086F (hex)
The Registry Key specified could not be found.
Severity: Error
EventID: E8080870 (hex)
An overcurrent condition has been detected on a probe plugged into the front panel.
Severity: Warning
EventID: A8080871 (hex)
The operation timed out.
Severity: Error
EventID: E8080872 (hex)
"The Network Analyzer executed a preset."
Severity:Informational
Further explanation: None
EventID: 68080873 (hex)
"Access to file denied."
Severity: Error
Further explanation: This means that the system can not open an output file for writing. Most likely because the file is write protected.
Suggestions: Pick another file name or file directory, check floppy disk hard disk write access.
EventID: E8080874 (hex)
"File type is structured storage."
Severity: Informational
Further explanation: None
EventID: 68080875 (hex)
"The trigger operation failed."
Severity: Error
Further explanation: None
EventID: E8080876 (hex)
"Argument out of range error."
Severity: Error
Further explanation: None
Suggestions: None
EventID: E8080877 (hex)
The given COM object is not a custom application
Severity: Error
EventID: E8080879 (hex)
The eventID supplied was not recognized as a valid VNA eventID
Severity: Error
EventID: E808087A (hex)
The operation was canceled.
Severity: Error
EventID: E808087B (hex)
High security level cannot be disabled directly. Only an instrument preset or recall of lower security instrument state will reset this security level.
Severity: Error
EventID: E808087C (hex)
Local lockout mode is on. The VNA application will not accept input from front panel, keyboard or mouse until this mode is turned off from a remote interface.
Severity: Error
EventID: E808087D (hex)
The SnP request is not valid for the selected measurement.
Severity: Error
EventID: E808087E (hex)
Preset is not supported while this dialog or wizard is open. Close the dialog or wizard and then try again.
Severity: Error
EventID: E808087F (hex)
The function you requested requires a capability provided by an option to the standard analyzer. That option is not currently installed.
Severity: Error
EventID: E8080880 (hex)
Catastrophic error. Crash dump recorded at <n>
Severity: Error
EventID: E8080881 (hex)
In the context of a noise calibration, this would occur if the VNA was unable to set the state of the tuner Ecal module.
Severity: Error
EventID: E8080882 (hex)
Failed to open gen.lic.
Severity: Error
EventID: E8080883 (hex)
Last modified:
|
18-May-2016 |
First Release |
![]()