Data Setup

 

Data

Numeric Format

Choices: Two's Complement, Offset Binary
Default: Two's Complement

Selects the binary format used to represent the transmitted data values.

Two's Complement

This choice selects the N5102A module data format to a two’s complement representation of the data values.Closed
Representation…

Twos complement is a method for representing data as a signed number. Using two's complement:

  • Positive two's complement numbers are represented as simple binary.

  • Negative two's complement numbers are represented as the binary number that when added to a positive number of the same magnitude equals zero.

Integer

Twos Complement Representation

32767

0111 1111 11111111   

16384

0100 0000 00000000   

1

0000 00000000 0001   

0

0000 000000000000   

–1

1111 111111111111   

–16384

1100 0000 00000000   

–32768

1000 0000 00000000   

Offset Binary

This choice selects the N5102A module data format to an offset binary representation of the data values.Closed
Representation…

Offset binary is a method for representing data as a signed number. Using binary code, half of the largest possible number is assigned as the zero value. A positive integer is the absolute value added to the zero number and a negative integer is subtracted. Offset binary is popular in A/D and D/A conversions.

Integer

Offset Binary
Representation

32767

1111 111111111111   

16384

1100 0000 00000000   

1

1000 0000 0000 0001   

0

1000 0000 00000000   

–1

0111 1111 11111111   

–16384

0100 0000 00000000   

–32768

0000 000000000000   

This selection may be changed even while the waveform is playing.

 

IQ Polarity

Choices: Positive, Negative
Default: Positive

Selects the logic level for I and Q data.

Positive

This choice selects a high logic level at the output as a digital one.

Negative

This choice selects a low logic level at the output as a digital one.

This selection may be changed even while the waveform is playing.

 

Return to Top

 

Word Size

Range: 4 to 16
Default: 16
Resolution: 1

Sets the number of bits in each sample transmitted through the N5102A module. A word is defined as an integer number of bits from 4 to 16. For parallel and parallel interleaved data, word is synonymous with sample. Any unused data lines are driven low. The word size is coupled with Word Alignment. When this value is changed, the Data Format Graph is updated to reflect the changed value. Refer to Digital Lines, Digital Signals, and Data Format for examples of this change.

 

Word Alignment

Choices: LSB, MSB
Default: LSB
Dependency: Displayed only when Port Configuration is set to Parallel and available only when Word Size is set to less than 16

Selects the bit alignment of words smaller than 16 bits to begin at either boundary of the data bus. The word alignment is coupled with the word size and the word order. This command is only valid in parallel mode. When this value is changed, the Data Format Graph is updated to reflect the changed value. Refer to Data Format for examples of this change.

LSB

With this choice, the data will be aligned with the left data boundary (data line zero) for both I and Q.

MSB

With this choice, the data will be aligned with the right data boundary (data line 15) for both I and Q.

 

Bit Order

Choices: LSB, MSB
Default: LSB

Selects the bit order for data transmitted through the N5102A module. In serial mode, data can be in least significant (LSB) bit first or most significant (MSB) bit first (data line zero). In parallel mode, you can assign the bit order of the data words to either the lowest or highest lines of the data word. When this value is changed, the Data Format Graph is updated to reflect the changed value. Refer to Digital Signals and Data Format for examples of this change.

LSB

With this choice, for a serial port configuration, the LSB of the data will be the first bit (data line zero) in a sample. In parallel or parallel interleaved port configuration, the LSB of the data word will appear on the lowest lines of the data word.

MSB

For a serial port configuration, the MSB will be the first bit in a sample. In parallel or parallel interleaved port configuration, the MSB of the data word will appear on the lowest lines of the data word.

 

Return to Top

 

I Negation

Choices: ON, OFF
Default: OFF

Enables or disables negation of the value of each sample of the I data. Negation changes the affected sample by expressing it in two's complement form, multiplying by negative one, and converting back to the selected numeric format. Negation can be done for I samples, Q samples, or both.

On

With this choice, the I data is negated.

Off

With this choice, no negation is performed.

This selection may be changed even while the waveform is playing.

 

Q Negation

Choices: ON, OFF
Default: OFF

Enables or disables negation of the value of each sample of the Q data. Negation changes the affected sample by expressing it in two's complement form, multiplying by negative one, and converting back to the selected numeric format. Negation can be done for I samples, Q samples, or both.

On

With this choice, the Q data is negated.

Off

With this choice, no negation is performed.

This selection may be changed even while the waveform is playing.

 

Swap IQ

Choices: ON, OFF
Default: OFF

Enables or disables swapping of the I and Q data. When enabled, the ’I’ data is sent to the Q bus and the ’Q’ data is sent to the I bus on the N5102A module. When this value is changed, the Data Format Graph is updated to reflect the changed value. Refer to Digital Signals for examples of this change. 

On

With this choice, the I data is available on the Q data bus and the Q data is available on the I data bus.

Off

With this choice, I and Q data are not swapped.

This selection may be changed even while the waveform is playing.

 

Return to Top

 

Related Topics:

General Settings
Port Configuration

Clock Setup

Clock Connection Graph

Data Format Graph