Choices:
LVDS, LVTTL, CMOS33, CMOS25, CMOS18, CMOS15
Default: CMOS33
Selects the logic data type used by the device being tested.
|
LVDS |
sets the logic type for the N5102A module to low voltage differential signaling (LVDS) as the logic data type. |
|
LVTTL |
sets the logic type for the N5102A module to a low voltage TTL signal as the logic data type. |
|
CMOS33 |
sets a 3.3 volt CMOS signal as the logic data type. |
|
CMOS25 |
sets a 2.5 volt CMOS signal as the logic data type. |
|
CMOS18 |
sets a 1.8 volt CMOS signal as the logic data type. |
|
CMOS15 |
sets a 1.5 volt CMOS signal as the logic data type. |
|
|
Changing the logic type changes the voltage levels. To avoid potential damage to your DUT or the N5102A module, first verify that the new logic type and voltage are appropriate. |
Choices:
Serial, Parallel
Default: Parallel
Configures the Output port of the N5106A for parallel or serial data transmission with the N5102A module. When this value is changed, the Data Format Graph is updated to reflect the changed value.
The available clock range and output sample rates for the module depends on the port configuration settings, such as Logic Type, Port Configuration, and Serial/Parallel Mapping.
Choices: IQ to IQ, IQ to Interleaved QI,
IQ to Interleaved IQ
Default: IQ to IQ
Dependency: Displayed only when Port Configuration is set to Parallel
Selects the port mapping type for parallel transmission. When this value is changed, the Data Format Graph is updated to reflect the changed value. Refer to Digital Lines and Digital Signals for examples of this change.
|
IQ to IQ |
Samples are transmitted as 16 bits of ’r;I’ followed by 16 bits of ’r;Q’ ; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 bits of ’r;I’ are on the 16 ’r;I’ parallel lines; the 16 bits of ’r;Q’ are on the 16 ’r;Q’ parallel lines. Both I and Q are transmitted in one clock cycle. |
|
IQ to Interleaved QI |
Samples are transmitted as 16 bits of 'I’ followed by 16 bits of 'Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 bits of 'I’ and the 16 bits of 'Q’ are both on the 16 'I’ parallel lines. The 'I’ and 'Q’ bits are interleaved, with the 'Q’ bits coinciding with the rising edge of the clock, and the 'I’ bits occurring with the falling edge of the clock. The 'Q’ bits for a given sample precede the 'I’ bits for that sample. |
|
IQ to Interleaved IQ |
Samples are transmitted as 16 bits of 'I’ followed by 16 bits of 'Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 bits of 'I’ and the 16 bits of 'Q’ are both on the 16 'I’ parallel lines. The 'I’ and 'Q’ bits are interleaved, with the 'I’ bits coinciding with the rising edge of the clock, and the 'Q’ bits occurring with the falling edge of the clock. The 'I’ bits for a given sample precede the 'Q’ bits for that sample. |
Choices:
IQ to IQ, IQ to Sample Interleaved IQ, IQ to Bit Interleaved IQ
Default: IQ to IQ
Dependency: Displayed only when Port Configuration is set to Serial
Selects the port mapping type for serial transmission. When this value is changed, the Data Format Graph is updated to reflect the changed value. Refer to Digital Lines and Digital Signals for examples of this change.
|
IQ to IQ |
Samples are transmitted as 16 bits of ’r;I’ followed by 16 bits of ’r;Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 ’r;I’ bits of a sample appear as a serial stream on the I0 line. The 16 ’r;Q’bits of a sample appear on the I1 line. Accompanying these two data lines are separate lines for clock and frame signals. The frame signal goes high for one clock cycle during I0 and Q0; for the rest of the sample, the frame is low. |
|
|
|
|
|
|
IQ to Sample Interleaved IQ |
Samples are transmitted as 16 bits of ’r;I’ followed by 16 bits of ’r;Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 ’r;I’ bits as well as the 16 ’r;Q’ bits of a sample appear as a single serial stream on the I0 line. The ’r;I’ bits of a given sample precede the associated 16 ’r;Q’ bits. The frame signal goes high for one clock cycle during the first ’r;I’ bit of a sample; for the rest of the sample, the frame signal is low. |
|
|
|
|
|
|
IQ to Bit Interleaved IQ |
Samples are transmitted as 16 bits of ’r;I’ followed by 16 bits of ’r;Q’; a complete sample is 32 bits or 4 bytes. At the device interface, the 16 ’r;I’ bits as well as the 16 ’r;Q’ bits of a sample appear as a single serial stream on the I0 line, with each ’r;I’ bit preceding the associated ’r;Q’ bit. The frame signal goes high for one clock cycle during the first ’r;I’ bit of a sample; during the rest of the sample, the frame signal is low. |
|
|
|
|
|
Choices:
Negative, Positive
Default: Positive
Dependency: Displayed only when Port Configuration is set to Serial
Selects the polarity of the frame marker for serial transmission. The frame marker indicates the beginning of each sample or byte of data.
|
Positive |
The frame marker is set high during the first data sample. |
|
Negative |
The frame marker is set low during the first data sample. |
This setting may be changed even while the waveform is playing.
Range: 0
to 15
Default: 0
Dependency: Displayed only when DSIM is configured as an input
Delays the serial frame boundary marker in one-bit increments.
General Settings
Clock Setup
Data Setup
Clock Connection Graph
Data Format Graph