General Settings (N5102A Digital Signal Interface Module)

 

Settings

Direction

Displays the location in the system that the N5102A module is being used. Output is displayed when the module is configured to connect to one of the PXB's external output ports. Input is displayed when the module is configured to connect to one of the PXB's external input ports. This parameter is defined when the external instruments are assigned to the configuration block diagram and may not be set in this window.

 

 

Output Sample Rate

Range: 1 kHz to 200 MHz
Default: 100 MHz
Resolution: 1 Hz
Dependency: Displayed only when DSIM is configured as an output
 

Sets the output sample rate for the N5102A module. The available range depends on the Port Configuration settings. The output sample rate is limited by the maximum clock rate. The sample rate is recalculated if the Clock Rate, Clocks per Sample, or Port Configuration is changed.

 

Return to Top

 

Related Topics:

Port Configuration
Clock Setup

Data Setup

Clock Connection Graph

Data Format Graph