Dynamic Fading

Dynamic fading uses a scenario that you define ahead of time to dynamically change the dwell time, path delay, relative path loss, and UE speed for up to 24 paths. These settings simulate the UE moving through different fading environments.

How do I apply a dynamic fading scenario to my waveform?

  1. Select and load your configuration.

  2. Create a dynamic fading scenario file (Using an Excel Spreadsheet Template for Dynamic Fading Setup).

  3. Turn dynamic fading on in the Fader Setup view of your configuration.

  4. Enable all fading paths that you want to simulate in the Fader Paths settings of the Master Setup for your configuration. When dynamic fading scenarios are imported, the dynamic fading settings from the dynamic fading file are used instead of the values set in the fading user interface.

  5. Select the dynamic fading file that you want to use.

  6. Download the dynamic fading file that will be used.

  7. Play the waveform.

Related Topics

Using an Excel Spreadsheet Template for Dynamic Fading Setup

Entering Data into the Excel Spreadsheet Template

Dynamic Fading File Format Using a Text Editor