Go to topic Go to topic

Fader Setup (MIMO)

Not all of the parameters listed below are displayed simultaneously. For some channel models, the Fader settings for the associated parameter are displayed above the Fader Setup parameters when the channel model is selected. When multiprobe MIMO OTA channel models are selected, the Cluster Weighting tab replaces the Power Imbalance tab.

Fader Setup Tab

Displayed only when LTE High Speed Train is the selected Channel Model

Fader Settings - High Speed Train

Base Station Initial Distance

Base Station Minimum Distance

Train Speed

Maximum Doppler Frequency

Fader Birth-Death Settings

Displayed only when a W-CDMA BS or W-CDMA MS Birth-Death profile is the selected Channel Model.

Minimum Delay

Maximum Delay

Delay Bin Spacing

Dwell Time

Fader Setup

Dynamic Fading File

Dynamic Fading

Mode

MIMO Settings

Correlation Type and Power Azimuth Spectrum are not displayed simultaneously.

Channel Model

Fader n Carrier Frequency

Correlation Type

Rx/Tx Power Azimuth Spectrum

Antenna Rotation Mode

Correlation Source

Path Configuration Source

Echo Delay

Echo Loss

HSPA Precoding Matrix

Random Seed

Random Seed (Hex)

High (Hex)

Middle (Hex)

Low (Hex)

 

Fader High Speed Train Settings

Dependency: Displayed only when LTE High Speed Train is selected as the Channel Model

Base Station Initial Distance (Ds/2)

Default: Tunnel: 150 m; Open Space: 500 m
Range: 10 m to 100 km

Sets the initial distance (Ds/2) that the mobile must travel before passing the base station (assuming that the initial distance is much larger than Dmin) when using the LTE high speed train channel model. 

Base Station Minimum Distance (Dmin)

Default: Tunnel: 2 m; Open Space: 50 m
Range: 0 to 1 km 

Sets the minimum distance from the mobile to the base station (BS-Railway track distance) when using the LTE high speed train channel model.

Train Speed

Default: Tunnel: 300 km/h; Open Space: 350 km/h
Range: 0 to 1000 km/h

Sets the train speed when using the LTE high speed train channel model.

Maximum Doppler Frequency

Default: Tunnel: 1.15 kHz; Open Space: 1.34 kHz
Range: 0 to 1.6 kHz 

Sets the maximum Doppler frequency for the channel when using the LTE high speed train channel model.


Fader Birth-Death Settings

Dependency: Displayed only when a W-CDMA BS or W-CDMA MS Birth-Death profile is the selected Channel Model.

Minimum Delay

Range: –25 to –0.1 ms
Default: –5.0
ms

Sets the minimum birth-death path delay when you select a Birth-Death delay profile for W-CDMA BS/MS. Although the minimum delay property is a negative value, the delay bins are actually shifted to the positive while maintaining the same bin spacing.

Maximum Delay

Range: 0.1 to 25 ms

Default: 5.0 ms

Sets the maximum birth-death path delay when you select a Birth-Death delay profile for W-CDMA BS/MS.

Delay Bin Spacing

Range: 1 to 5 ms

Default: 1 ms

Sets the minimum step size of the random hops when you select a Birth-Death delay profile for W-CDMA BS/MS.

Dwell Time

Range: 0.1 to 1 s

Default: 0.191 s

Sets the duration for each birth-death state when you select a Birth-Death delay profile for W-CDMA BS/MS.


Return to Top

 

Fader Setup

Mode

Choices: On, Pass Through, Off,

Accesses a Closeddialog box where you can turn fading on, off, or allow the faded signal to pass through a fader block. Mixed is displayed if not all faders use the same mode.

On

Applies fading to the signal on the selected fader block in the configuration.

Pass Through

Passes the signal through the fader block without applying fading. This allows easier synchronization between the device-under-test (DUT) and the PXB with the same fader backoff as with the fader enabled.

Off

Turns the fader off; no signal is transmitted through the selected fader block.

Return to Top

Dynamic Fading

Choices: On, Off

Turns dynamic fading on or off. With dynamic fading on, the dynamic fading feature will be started the next time the waveform is played. (Dynamic fading is not available for the following profiles: W-CDMA Birth Death, W-CDMA Moving Propagation, or High Speed Train.)

Dynamic fading uses data that you define to dynamically change the relative path loss, path delay, and UE speed for up to 24 paths for each fading channel. The data for dynamic fading is entered from a dynamic fading scenario file.

Dynamic Fading File

This cell is only visible when dynamic fading is enabled.

Accesses a window from which you can browse to select a previously saved file that contains the fading scenarios to use for dynamic fading.

A Microsoft Excel spreadsheet template is provided to create the dynamic fading scenario file. The Agilent Dynamic Fading Template can be found at the following places:

Refer to Dynamic Fading for complete instructions on how to create the dynamic fading scenario file.

 

MIMO Settings

Channel Model

Choices: See table

Selects a default or standard-based fading model. The standard models cover general propagation environments that allow you to test whether your device meets the performance requirements as defined by their respective standard. Path configurations, antenna setup, and correlation are automatically populated for the selected standard model.

After selecting a model, the firmware provides options to customize path configurations, antenna setups, or the correlation matrix. Since MIMO system performance is known to deteriorate substantially if the antenna spacing is insufficient or the scattering environment does not provide completely uncorrelated signals, these options allow you to thoroughly test your DUT or subsystem operation under a wide variety of environmental conditions.

Fader n Carrier Frequency

Default: 2.4 GHz

Range: 1 to 44 GHz

Sets the carrier frequency to be used for Doppler effects in the fading simulations. The carrier frequency is coupled either to the Doppler frequency or the vehicle speed as selected under Carrier Frequency Coupling in the Fader Path Setup view.

Each fading channel has its own carrier frequency setting. It is set to couple to the external input device by default, although coupling is user-selectable in the System > Get Carrier Frequency From menu. See the Menu Bar topic for more information.

Return to Top
 

Correlation Type

Dependency: Only active when using standard path configurations and correlation source
Choices: Low, Medium, High, Beamforming

Selects the correlation that best typifies the antenna relationships between the base station and mobile station when using a standard channel model.

 

Mobile WiMAX

LTE

Low

Selects a spatial and polarization correlation (BS 4λ, MS λ/2 cross-polarized) in a 2x2 configuration.

Selects a low correlation matrix as defined in Table B.2.3.2-4 of the specification.

Medium

Selects a polarization correlation (BS, MS cross-polarized). It is usually obtained from a cross polarized mobile station antenna and a slant cross-polarized base station antenna in a 2x2 configuration.

Selects a medium correlation matrix as defined in Table B.2.3.2-3 of the specification.

High

 

Selects a spatial correlation obtained from a BS uniform linear array with four wavelength spacing and an MS uniform linear array with a half-wavelength spacing (BS 4λ, MS λ/2) in a 2x2 configuration.

Selects a high correlation matrix as defined in Table B.2.3.2-2 of the specification.

Beamforming

Selects a correlation that optimizes communication to the intended receiver for 2x4 (uplink) or (4x2) downlink* configurations.

* N7615B Signal Studio for WiMAX does not currently support 4x2 configurations; however, user-created files can be used, for example, for diversity test.

Selects a correlation that optimizes communication to the intended receiver for 2x4 (uplink) or 4x2 (downlink) configurations.

Rx/Tx Power Azimuth Spectrum

Dependency: Only available when using a custom antenna source.
Choices: Laplacian, Gaussian, Uniform

Selects the statistical model that best fits the spatial distribution that characterizes the per-path amount of power arriving at the base/mobile station for a specific location as determined by the environment. In all WiMAX and LTE standard models, the power azimuth spectrum (PAS) is fixed to Laplacian. If the correlation source is From Antenna Setup, the PAS model may be selected.

The statistical model selected will vary depending on the scattering pattern and environment that you want to characterize. In general, for rural locations, with fewer objects in the environment, the power of azimuth spectrum would be concentrated around the angle pointing toward the nearest base/mobile station. Urban locations would have an azimuth spectrum with power nearly evenly distributed through all angles, though slightly stronger in the direction of the base/mobile station.

Laplacian

Selects Laplacian as the best fit for the per-path power distribution. Laplacian (double exponential) distribution is a symmetrical distribution with a mean higher than that of normal and is best suited for outdoor propagation in urban and rural areas. If all antenna elements’ orientations are aligned and the azimuth angle spread is the same, Laplacian distribution will result in the highest correlation at the base/mobile station.

Gaussian

Selects a Gaussian (normal) distribution to model the per-path power distribution for the transmitted/received signals. Gaussian distribution characterizes a spatial distribution of the scatterers' location geometry that is both various and random and not restricted to any constrained region. If all antenna elements’ orientations are aligned and the azimuth angle spread is the same, a Gaussian distribution will result in average correlation at the base/mobile station.

Uniform

Selects a uniform (constant) distribution to model the per-path power distribution for the transmitted/received signals. Uniform distribution characterizes a spatial distribution of scatterers clustered within a confined region. If all antenna elements’ orientations are aligned and the azimuth angle spread is the same, a uniform distribution will result in the lowest correlation at the base/mobile station.

Return to Top
 

Antenna Rotation Mode

Dependency: Only available when using a custom antenna source.
Choices: Tx or Rx

Selects the transmit antenna or the receiver antenna for angle rotation.

The Rx antenna rotation mode is not available when a multiprobe MIMO OTA channel model is selected.

 

Correlation Source

Choices: From Standard, From Custom Antenna Setup, Custom Correlation Matrix

Selects the source that will be used to calculate the correlation matrix.

In multiprobe test (multiprobe MIMO OTA channel model selected), the Correlation Source setting only applies to Tx correlation, since the Rx antennas are replaced by the Rx probes in the chamber.

From Standard

Calculates the correlation matrix using standard paths, antenna configurations, and PAS as specified by the respective standard. The correlation type may be selected.

This choice is not available when a multiprobe MIMO OTA channel model is selected.

From Custom Antenna Setup

Activates the antenna parameters for editing and calculates the correlation matrix from the user-defined antenna setup. This allows you to adjust antenna parameters to achieve optimal channel capacity for your DUT or subsystem. You can use either standard paths or custom paths with this selection.

Custom Correlation Matrix

Activates the correlation matrix for manual editing on a per path or per channel basis. No antenna topologies or path configurations are applied; the firmware does not generate the correlation matrix.

Path Configuration Source

Choices: From Standard, Custom

Selects the source for the path configuration parameters.

From Standard

Selects the path configurations as specified by the standard for the selected channel model.

Custom

Activates all paths for editing in the path configuration view. Using a Custom Path configuration will automatically select a Custom Correlation Matrix where channel correlations can be user-defined.

Return to Top
 

Echo Delay

Dependency: Displayed only when a DVB/DVB-H/Mobile SFN/<echo type> channel model is selected.
Default: 0 s
Range: 0 s to 1 ms

Sets the additional time delay (in seconds) for DVB fading paths 712 that are part of the echo signal. Use this command only after changing the Channel Model to DVB and selecting the Mobile SFN profile echo type.–

Echo Loss

Dependency: Displayed only when a DVB/DVB-H/Mobile SFN/<echo type> channel model is selected.
Default: 0 dB
Range: 0 dB to 20 dB

Sets the additional loss for DVB fading paths 712 that are part of the Weak long Echo signal. Use this setting only after changing the Channel Model to DVB and selecting the Mobile SFN profile echo type.–

HSPA Precoding Matrix

Dependency: Displayed only when an HSPA Single Stream, Dual Stream, or Static Orthogonal channel model is selected.
Choices: W1, W2, W3, W4
Default: W1

Sets the conjugate transpose WH for the selected HSPA transfer matrix channel model.

The Single Stream, Dual Stream, and Static Orthogonal channel models conform to 3GPP TS 34.121-1 sections D.2.9.1, D.2.9.2, and D.2.9.3.

Random Seed

Random Seed

Range: 0 to 289 – 1

Sets the random number generation seed of the fading channel. If it is set to zero, the generated fading will be different for each playback to provide randomness for each test. To reproduce the same fading environment for the same configuration as the last time it was played, use the same seed value (other than 0) each time.

You can enter the entire 89-bit sequence directly into the random seed cell or use the high, medium, and low cells to designate the number in three segments for easier data entry.

High

Specify the upper bits (0x0 to 0x1FFFFFF).

Middle

Specify the middle bits (0x0 to 0xFFFFFFFF).

Low

Specify the lowest bits (0x0 to 0xFFFFFFFF).

Return to Top