Signal Studio applications provide software to generate statistically correct waveforms as defined by their respective standards. Each Signal Studio technology requires a license to enable connectivity to the PXB and a license for the associated software option or options. Several convenience bundles are available that enable MIMO channel configurations; others provide complete LTE or WiMAX™ software and channel model capabilities.
Although several Signal Studio applications are preloaded on the PXB when it is shipped, you can install or update Signal Studio software on the PXB or on a remote PC at any time. To ensure that you have the latest version of the software:
If you are connected to the internet, you can download the latest version of the software (.exe) directly to the instrument's hard drive from: www.agilent.com/find/signalstudio/.
If you do not have internet access, you can transfer the software executable from a USB memory storage device using the USB slot on the front panel of the instrument.
At the prompt, select Run to install the software directly, or select Save to save a copy to your PC.
The Signal Studio installation process will create a desktop shortcut and store the required files in C:\<Program Files for Win XP><Program Files (x86) for Win 7>\Agilent\Signal Studio.
In the PXB, select and load the predefined configuration that you want to use. Ensure that the PXB number of channels matches the number of antennas or output signals desired from the Signal Studio Application. If they are not the same, the Signal Studio Application will generate an error when downloading waveforms to the PXB.
Start the Signal Studio software on the PXB or from a remote PC.
In the Signal Studio software, select the
Run System Configuration Wizard
in the Signal Studio software tool bar to select the PXB hardware that
you want to use. Waveforms will be automatically downloaded to the PXB
according to this configuration and saved in the appropriate D:\Waveforms\ChannelN
predefined directories. (ChannelN
corresponds to the antenna or channel number; for example, Antenna 1 is
saved to D:\Waveforms\Channel1.)
Create the waveforms that you want to use. Refer to the Signal Studio application help system if you need information on its usage or functionality.
Click Generate and Download in the Signal Studio software. The firmware verifies that a valid license for the waveform technology is installed on the PXB before generating and downloading the waveforms to baseband memory. An error message is displayed if there is a conflict between the configuration as set up in the software and the currently loaded configuration on the PXB.
|
|
|
Power Considerations
During download, the PXB runtime scaling is automatically adjusted to keep this relative amplitude on the output signal. Each of the external signal generators should be set to the power of the highest signal in the group.
Marker Considerations
|
To play the waveforms on the PXB
Click Download Panel in the PXB tool bar. The Waveform Table that appears displays the associated file path, waveform name, and download status of the waveform for each baseband generator in your configured setup.
If the download status displays "Up-to-Date" and the waveforms are correctly assigned, proceed to step 7. If you need to make changes to any of the waveforms that are currently downloaded, or assign a new waveform source file name to a baseband generator, proceed to steps 3 through 7 below.
To update a waveform before playing
Generate and download the updated waveform from the Signal Studio software. You can also replace an existing file with one from the PXB hard drive or from a network drive by selecting a new waveform file in the Waveform Source Name cell in the respective BB Gen General Settings pane.
Click Download Panel and notice that the Waveform Table now shows an "Out-of-Date" status for any waveforms that have changed.
In the Waveform table, enable (check) the baseband generators to be reloaded with new or updated waveforms. Clear any that you do not wish to reload or that already display "Up-to-Date".
Click Start to begin the download process. After a waveform file has been completely downloaded, the Waveform Status displays "Up-to-Date" and the Download Status column displays "Completed". Download times vary depending on the size and complexity of the waveforms being downloaded.
|
|
Waveforms must be downloaded to baseband memory after recalling settings, or executing a preset, or a power cycle. Waveform data is not saved as part of the PXB settings file; only file path information is saved. |
Click Play in
the tool bar to play the waveforms on the enabled channels. Play is enabled
once you have completely downloaded your waveform files to each BB Gen
block in the PXB.
|
|
To ensure accurate power calibration during play, set the desired amplitude on either the signal generator or in the PXB Signal Generator General Settings pane. (Setting parameters in the signal generator requires an Update From Instrument to reset the user interface.) The RF Output must be set to On in order for the signal to be visible out of the signal generator. |