Data (Basic)

Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the burst type (Timeslot Type) for the selected timeslot as defined in the Timeslots window. The Data node (Basic) provides a list of the pre-defined timeslot configurations for the SM/EDGE/EGPRS2-A and EGPRS2-B carriers

Data (Access Burst)

Data (Custom 8PSK Burst)

Data (Custom GMSK Burst)

Data (Dummy Burst)

Data (Frequency Correction Burst)

Data (HSR 16QAM Burst)

Data (HSR 32QAM Burst)

Data (HSR QPSK Burst)

Data (HSR Custom 16QAM Burst)

Data (HSR Custom 32QAM Burst)

Data (HSR Custom QPSK Burst)

Data (Normal 8PSK Burst)

Data (Normal 16QAM Burst)

Data (Normal 32QAM Burst)

Data (Normal GMSK Burst)

Data (Synchronization Burst)

Data (Advanced)