Real Time

Standard Combined BCH (Coded Control Channels - Advanced)

The Standard Combined BCH (Control Channels) are coded channels that are available with Option QFP.To open the Data node, click Data in the tree view. Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the Channel Type for the selected timeslot as defined in the Timeslot window.

There are two kinds of ClosedStandard Combined Broadcast Channels (BCH):

Refer to Multiframe Structure of BCH.

BCH Pre-Defined Carrier Configurations

There are different pre-defined carrier configurations for the BCH:

The different BCH configurations require different Carrier setups. Refer to the Closedexamples.

Examples of Standard BCH (Control Channels) and Waveform Pre-configurations

The order of the Carrier setups is optional.

Example 1: FCCH + SCH + BCCH + CCCH and GSM BCH + TCH/FS + PDTCH Pre-Configuration

FCCH + SCH + BCCH + CCCH Waveform Setup Requirements

Tree View Node

Parameter: Configuration or Channel Type (Radio Format)

Waveform Setup1

GSM BCH + TCH/FS + PDTCH

WFMn

No action is required.

Carrier 1

Control Channels (1.GSM/EDGE):

FCCH + SCH + BCCH + CCCH

Timeslot

Standard Combined BCH (on TS0)2

Carrier 2

Advanced GSM/EDGE/EGPRS2-A (1.GSM/EDGE):

TCH/FS 1 Timeslot On TS3 and PDTCH 1 Timeslot On TS4

Timeslot

  • Coded TCH/FS (on TS3 or TS4) and

  • Coded Downlink/Uplink MCS-53 (on TS3 or TS4)4

1 Use the Insert New Waveform button to select the correct WFMn. type. The software then selects the default Carriers for this waveform.

2 Verify TS3 and TS4 states are off.

3 Optional: Choose one of the Coded Downlink or Uplink MCS-5 to MCS-9 (PDTCH) data types (Software defaults to Coded Downlink MCS-5).

4 Verify TS3 and TS4 are on.

Example 2: FCCH + SCH + BCCH + CCCH + SDCCH + SACCH and GSM BCH + TCH/HR + PDTCH Pre-Configuration

FCCH + SCH + BCCH + CCCH + SDCCH + SACCH Waveform Setup Requirements

Tree View Node

Parameter: Configuration or Channel Type (Radio Format)

Waveform Setup1

GSM BCH + TCH/HS + PDTCH

WFMn

No action is required.

Carrier 1

Control Channels (1.GSM/EDGE):

FCCH + SCH + BCCH + CCCH + SDCCH + SACCH2

Timeslot

Standard Combined BCH (on TS0)3

Carrier 2

Advanced: Half Rate GSM/EDGE/EGPRS2-A: (1. GSM/EDGE):

TCH/HS 1 Timeslot On TS3

Timeslot

Coded TCH/HS (on TS3)4

Carrier 3

Advanced GSM/EDGE/EGPRS2-A (1. GSM/EDGE):

PDTCH 1 Timeslot On TS4 

Timeslot

Coded Downlink MCS-5 (on TS4)5,6

1 Use the Insert New Waveform button to select the correct WFMn. type.

2 Use the Configuration parameter's dropdown to select this BCH.

3 Verify TS3 and TS4 states are off. If not, use the State parameter's down arrow to turn off.

4 Verify TS3 is on.

5 Verify TS4 is on.

6 Optional: Choose one of the Coded Downlink or Uplink MCS-5 to MCS-9 (PDTCH) data types (Software defaults to Coded Downlink MCS-5)

Figure: FCCH + SCH + BCCH + CCCH + SDCCH + SACCH

FCCH + SCH + BCCH + CCCH choices are similar, but without SDCCH and SACCH.

Once turned on On, function tables Closed5. SDCCH contents and Closed6. SACCH contents have additional parameters (default state is Dummy Burst).

Standard Combined BCH parameter description links:

Change Data Values Button

Click to display a drop-down menu in which you can copy a timeslot configuration from one timeslot to another.

Data Node Parameters

Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the burst type (Timeslot Type) for the selected timeslot as defined in the Timeslots window. In the window shown above, Timeslots 0 is set up for a data cell with a Broadcast Channel (BCH) Burst.

1. FCCH contents

FCCH State

State is always ON. This setting is not editable.

FCCH Tail bits

Tail Bits (3+3 bits)

Tail bits are set by the software at 000. This setting is not editable.

FCCH Fixed bits

Choice: PN9| PN15 | User

Default: User X"000...000"

This is a 142 bits field.

FCCH Guard period (n bits)

The software sets the Guard period (bits). This setting is not editable.

Figure: Guard Period Lengths Between Different Timeslots

Burst Transition

Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods)

TS0 and TS1 or

TS4 and TS5

Any other timeslot pair

normal symbol period to

normal symbol period

9 (111111111)

8 (11111111)

2. SCH contents

SCH State

State is always ON. This setting is not editable.

SCH Tail bits

Tail Bits (3+3 bits) are set by the software at 000. This setting is not editable.

SCH Encrypted Bits

Choice: STD | PN9| PN15 | User Defined Bits

Default: STD

If the Closeddata source is STD (standard) then the PLMN (Pubic Land Mobile Network) color code, BTS (Base Transeiver Station) color code and frame number will be used to generate the SCH (Synchronization Channel) data source.

Click the Details button in this cell to open the ClosedData Source Selection window.

Select STD, PN9, PN15 or User Defined Bits to use for the encrypted bits.

Select User Defined Bits, to create an encrypted data string. (See the Closeddrop-down figure.)

The buttons in this window are described in Marker Source Selection.

SCH PLMN color code

Choice: 0 to 7

Default: 1

This sets the value of the Public Land Mobile Network (PLMN) for the waveform.

SCH BTS color code

Choice: 0 to 7

Default: 0

The Base Transeiver Station (BTS) color code is broadcasted on SCH. The TSC (Training Sequence Code) that is used on the downlink channel has a logical relationship to the BTS. If the BTS color code is 0, then TSC0 should be used in BCCH and CCCH; if BTS color code is 1, then TSC1 should be used in BCCH and CCCH.

The signal studio software does not automatically couple the BTS color code and TSC parameters, so it is important to verify that there is no conflict between these two parameters. Refer to Table 1.

Table 1: BTS color code and TSC values

BTS color code

TSC value used in BCCH and CCCH:

0

TSC0

1

TSC1

SCH Initial Frame Number

Range: 0 to 2715647

Default:1

Initial Frame Number is used to calculate the first initial SCH frame. The frame number is incremental. The frame number is used to generate T1, T2 and T3 which are parts of the original data of the encrypted bits for Synchronization Channel (SCH).

The Frame Number is only sent on SCH. And it is sent 5 times every 51 frames.

The system information may not follow the standard 3GPP 45002-6b0, section 6.3.1.3 when the initial frame number is set to a specific value.

SCH Extended Training Sequence

Choice: PN9 |PN15 | User Defined Bits

Default: X"B962040F2D45761B" (64 bits)

Enter 64 bits to use for the fixed bits of the extended training sequence bits.

SCH Guard period (n bits)

The software sets the Guard period (bits). This setting is not editable.

Figure: Guard Period Lengths Between Different Timeslots

Burst Transition

Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods)

TS0 and TS1 or

TS4 and TS5

Any other timeslot pair

normal symbol period to

normal symbol period

9 (111111111)

8 (11111111)

3. BCCH contents

BCCH State

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to set the channel state. If state is On, GMSK burst shall be used; If the state is Off, Dummy burst shall be used.

BCCH Tail bits

Tail bits (3+3 bits) are set by the software at 000. This setting is not editable.

BCCH Encrypted Bits

Choice: STD | PN9| PN15 | User Defined Bits

Default: STD

If the Closeddata source is set to STD (standard) then System Information Type 3 message will be sent on BCCH.

Click the Details button in this cell to open the ClosedData Source Selection window.

Select STD, PN9, PN15 or User Defined Bits to use for the encrypted bits.

Select User Defined Bits, to create an encrypted data string. (See the Closeddrop-down figure.)

The buttons in this window are described in Marker Source Selection.

BCCH Cell Identity

Range: 0 to 65535

Default: 0

Enters a value to set the cell identity.

BCCH Mobile Country Code

Range: 0 to 999

Default: 1

Enter a value to set the Mobile Country Code where the base station is located.

BCCH Mobile Network Code

Range: 0 to 99

Default: 1

Enter a value to set the Mobile Network Code.

BCCH Location Area Code

Range: 0 to 65535

Default: 1

Enters a value to set the Location Area Code.

BCCH MS_TXPWR_MAX_CCH

Range: 0 to 31

Default: 0

Enter a value to set the MS_TXPWR_MAX_CCH value.

The BCCH MS_TXPWR_MAX_CCH field is the binary representation of the "power control level" mentioned in 3GPP TS 45.005. This value corresponds to the maximum TX (Transmitter) power level a MS (Mobile Station) may use when accessing on a Control Channel (CCH). Refer to 3GPP TS 45.008.

BCCH Stealing Flags (1+1) (1 bit entry)

Stealing Flag for BCCH. It is always 1. This setting is not editable.

BCCH External Training Sequence

Choice: TSC0 to TSC7 or User Defined Bits

Default: TSC0

Select TSC0 to TSC7 or User Defined Bits to use for the training sequence bits.

The training sequences are defined as follows:

TSC0: 0970897

TSC1: 0B778B7

TSC2: 10EE90E

TSC3: 11ED11E

TSC4: 06B906B

TSC5: 13AC13A

TSC6: 29F629F

TSC7: 3BC4BBC

BCCH Guard period (n bits)

The software sets the Guard period (bits). This setting is not editable.

Figure: Guard Period Lengths Between Different Timeslots

Burst Transition

Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods)

TS0 and TS1 or

TS4 and TS5

Any other timeslot pair

normal symbol period to

normal symbol period

9 (111111111)

8 (11111111)

4. CCCH contents

CCCH State

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to set the channel state. If state is On, GMSK burst shall be used; if the state is Off, Dummy burst shall be used.

CCCH Tail bits

Tail Bits (3+3 bits) are set by the software at 000. This setting is not editable.

CCCH Encrypted Bits

Choice: PN9 | PN15 | User Defined Bits

Default: PN9

Click the Details button in this cell to open the ClosedData Source Selection window.

The buttons in this window are described in Marker Source Selection.

Select Import, Export, Insert PN9, Insert PN15 or User Defined Bits to use for the encrypted bits.

The Encrypted Bits parameters are only shown if the State is On.

CCCH Stealing Flags (1+1) (1 bit entry)

Stealing Flag for CCCH. It is always 1. This setting is not editable.

CCCH External Training Sequence

Choice: TSC0 to TSC7 or User Defined Bits

Default: TSC0

Select TSC0 to TSC7 or User Defined Bits to use for the training sequence bits.

The training sequences are defined as follows:

TSC0: 0970897

TSC1: 0B778B7

TSC2: 10EE90E

TSC3: 11ED11E

TSC4: 06B906B

TSC5: 13AC13A

TSC6: 29F629F

TSC7: 3BC4BBC

CCCH Guard period (n bits)

The software sets the Guard period (bits). This setting is not editable.

Figure: Guard Period Lengths Between Different Timeslots

Burst Transition

Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods)

TS0 and TS1 or

TS4 and TS5

Any other timeslot pair

normal symbol period to

normal symbol period

9 (111111111)

8 (11111111)

5. SDCCH contents (FCCH+SCH+BCCH+CCCH+SDCCH+SACCH only)

SDCCH State

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to set the channel state. If state is On, GMSK burst shall be used; if the state is Off, Dummy burst shall be used.

SDCCH Tail bits

Tail bits (3+3 bits) are set by the software at 000. This setting is not editable.

SDCCH Encrypted Bits

Choice: PN9 | PN15 | User Defined Bits

Default: PN9

Click the Details button in this cell to open the ClosedData Source Selection window.

The buttons in this window are described in Marker Source Selection.

Select Import, Export, Insert PN9, Insert PN15 or User Defined Bits to use for the encrypted bits.

The Encrypted Bits parameters are only shown if the State is On.

SDCCH Stealing Flags (1+1) (1 bit entry)

Stealing Flag for SDCCH. It is always 1. This setting is not editable.

SDCCH External Training Sequence

Choice: TSC0 to TSC7 or User Defined Bits

Default: TSC0

Select TSC0 to TSC7 or User Defined Bits to use for the training sequence bits.

The training sequences are defined as follows:

TSC0: 0970897

TSC1: 0B778B7

TSC2: 10EE90E

TSC3: 11ED11E

TSC4: 06B906B

TSC5: 13AC13A

TSC6: 29F629F

TSC7: 3BC4BBC

SDCCH Guard period (n bits)

The software sets the Guard period (bits). This setting is not editable.

Figure: Guard Period Lengths Between Different Timeslots

Burst Transition

Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods)

TS0 and TS1 or

TS4 and TS5

Any other timeslot pair

normal symbol period to

normal symbol period

9 (111111111)

8 (11111111)

6. SACCH contents (FCCH+SCH+BCCH+CCCH+SDCCH+SACCH only)

SACCH State

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to set the channel state. If state is On, GMSK burst shall be used; If the state is Off, Dummy burst shall be used.

SACCH Tail bits

Tail Bits (3+3 bits) are set by the software at 000. This setting is not editable.

SACCH Encrypted Bits

Choice: STD | PN9 | PN15 | User Defined Bits

Default: STD

If the Closeddata source is set to STD, SACCH contents will be generated by user settings.

Click the Details button in this cell to open the ClosedData Source Selection window.

Select STD, PN9, PN15 or User Defined Bits to use for the encrypted bits.

Select User Defined Bits, to create an encrypted data string. (See the Closeddrop-down figure.)

The buttons in this window are described in Marker Source Selection.

The Encrypted Bits parameters are only shown if the State is On.

SACCH Validity Check

Choice: Valid | Invalid

Default: Valid

If Invalid is selected, a wrong CRC will be generated so that MS cannot decode the SACCH correctly.

SACCH Power Control Level

Range: 0 to 31

Default: 15

Enter a value to set power control level.

SACCH Timing Advance

Range: 0 to 255

Default: 0

Enter a value to set timing advance for mobile station (MS).

SACCH Layer 2 Frame

Choice: PN9 | PN15 | User Defined Bits

Default: PN9

This is the content of the Closed21 octets field in downlink SACCH block structure.

Slow Associated Control Channel (SACCH) Blocks (Downlink) Frame Structure

The 23 octets of SACCH blocks are used in the downlink in the following way:

Figure: SACCH downlink block format for mobile station (MS) operating in A/Gb mode

SACCH Spare

SACCH spare bit is always 0. This setting is not editable.

SACCH SR0

SACCH SR0 bit is always 0. This setting is not editable.

SACCH FPC_EPC

SACCH FPC_EPC bit is always 0. This setting is not editable.

SACCH Stealing Flags (1+1) (1 bit entry)

You can enter 1 (control channel burst) or 0 (data channel burst). This setting is not editable.

SACCH External Training Sequence

Choice: TSC0 to TSC7 or User Defined Bits

Default: TSC0

Select TSC0 to TSC7 or User Defined Bits to use for the training sequence bits.

The training sequences are defined as follows:

TSC0: 0970897

TSC1: 0B778B7

TSC2: 10EE90E

TSC3: 11ED11E

TSC4: 06B906B

TSC5: 13AC13A

TSC6: 29F629F

TSC7: 3BC4BBC

SACCH Guard period (n bits)

The software sets the Guard period (bits). This setting is not editable.

Figure: Guard Period Lengths Between Different Timeslots

Burst Transition

Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods)

TS0 and TS1 or

TS4 and TS5

Any other timeslot pair

normal symbol period to

normal symbol period

9 (111111111)

8 (11111111)

Multiframe Structure of BCH

Waveform Generation Log

Advanced Downlink TDMA

Timeslot (Advanced)