Transport Channel (Basic LTE-A TDD Downlink)

The Transport Downlink configuration has several different possible channel setups (e.g. DL-SCH and BCH). The screen shot below shows the parameter choices for a DL-SCH channel. Click a different channel to view that channel's parameter choices. The links for all of the channel's parameters and their descriptions are listed in the table below.

Before adding a transport channel as described below, delete any existing transport channel, physical channel, or resource block collection that occupies the resource blocks that your new transport channel will occupy. If you add a new transport channel without first deleting a conflicting channel or resource block collection, a "code conflicted" error occurs when you generate the waveform.

To add a new transport channel, click the Add New Channel button and select the transport channel to add. The software adds the new channel above the currently selected channel in the list. The software assigns a channel identifying number to the new channel that corresponds to its position in the list and increments the identifying numbers of subsequent channels in the list.  

When you add a DL-SCH channel, the Configure DL-SCH window opens so that the settings are available.

Similarly, if you delete the selected channel using the Delete Selected Channel(s) button , the software adjusts the identifying numbers of the subsequent channels according to their new positions in the list.

You can make changes to an already configured DL-SCH channel by selecting the channel and clicking this button to launch the Configure DL-SCH window.

Transport Channel Parameters Figure–Descriptions Below

General Settings

Transport Channel Number

Name

State

Power

RNTI

Physical Channels

Coding State

Data

UE-Specific Reference Signals (DM-RS)

DM-RS State

DM-RS Power

DM-RS Antenna Configuration

DM-RS Antenna Port

Scramble ID  

General Settings

Transport Channel Number

Displays the number of the selected transport channel.

Name

Displays the name of the selected transport channel.

BCH = Broadcast Channel     

DL-SCH = Downlink Shared Channel     

State

Choice: Off | On

Default: On

Double-click or use the drop-down menu to turn the channel On or Off.

Power

Range: -60.000 to 20.000 dB

Default: 0.000 dB

Enter a power level in dB for the selected channel. See Power Settings (Downlink) for a description of how the software applies your power setting.

RNTI

Range: 0 to 65535

Default: 0

Enter a value for the Radio Network Temporary Identifier (RNTI). See 3GPP TS 36.211.

Physical Channels

Displays the number(s) of the physical channel(s) associated with the selected transport channel.

Coding State

This is read only parameter and always set to Off.

Displays the coding state (Off) for the selected channel. Transport channel coding is not available in the Basic LTE Carrier. Use the Advanced LTE Carrier to configure a signal with transport channel coding.

Data

Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits to use for the data.

UE Specific Reference Signals (DM-RS)

UE specific reference signals are intended for a specific user and are used for channel estimation and demodulation.

DM-RS State

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to turn the channel state on or off.

DM-RS State is coupled to the DL-SCH State. When DL-SCH is On, DM-RS State is active and is settable.

DM-RS Power

Range: -60 to 20 dB

Default: 0 dB

Enter a power level in dB for the selected channel. See Power Settings (Downlink) for a description of how the software applies your power setting.

DM-RS Antenna Configuration

Choice: Auto | Manual

Default: Auto

Double-click or use the drop-down menu to select the DM-RS Antenna Configuration.

This parameter indicates the setting of the DM-RS Antenna parameter. The possible settings are either Auto (automatically set by the software) or Manual (you can set them).

DM-RS Antenna Port

Choice: Auto | Port 5 | Port 7 | Port 8 | Port 9 | Port 10 | Port 11 | Port 12 | Port 13 | Port 14

Default: Auto

Double-click or use the drop-down menu to select the antenna port for UE-Specific Reference Signal (DM-RS).

For extended cyclic prefix, UE-specific reference signals are not supported on antenna ports 9 to 14.

Total Number of Antennas

DM-RS Antenna Configuration

DM-RS Antenna Port

1

Manual

Port 5, 7, 8

2

Manual

Port 7, 8

4

Manual

Port 7, 8, 9, 10

8

Manual

Port 7, 8, 9, 10, 11, 12, 13, 14.

 

Auto

(Antenna Port) + 7

Scramble ID

Range: 0 to 1

Default: 0

Enter a value of the Scramble ID for UE-specific Reference Signals. This parameter indicates the Scramble ID for UE-specific RS.

This is only available when DM-RS Antenna Port = Port 7 or Port 8 and Total Number of Antennas = 2 Antennas or 4 Antennas.

For more detail, refer to 3GPP TS 36.211.