The Embedded LO feature allows you to make SMC measurements of mixers that have a FIXED LO inside the DUT.
Note: This feature is available as Opt S9x084A/B, and must be enabled.
In this topic:
Measurements of these devices are challenging for a couple of reasons:
All Embedded LO measurements require the VNA receivers to be tuned to the correct frequency to measure the mixer output, which is highly dependent on the exact LO frequency.
The nominal frequency of the embedded LO is input into the Mixer Setup dialog. This is used as a starting point for the measurement.
Before each DUT measurement sweep, background sweeps are made to determine the frequency of the embedded LO to a configurable degree of accuracy.
Background sweeps...
Broadband Sweep - rough measurement of the embedded LO frequency, made around a selectable data point over a selectable frequency span. The input signal to the DUT is tuned to a selectable CW frequency. The B receiver is swept across a selectable span around the anticipated output frequency. The difference between the frequency of the found signal and the desired output frequency is then applied as an adjustment.
Precise Sweep The B receiver is measured at the selectable data point. Measurements of phase versus time are made, from which the exact offset frequency is computed, until either the tolerance value or maximum iterations are met.
To measure a DUT with an Embedded LO:
How to Launch the Embedded LO Mode dialog box |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
The Tuning Settings balance LO measurement speed versus accuracy. You can see that accuracy is becoming compromised when noise starts to appear on the measurement trace. Scroll up to learn more about the Embedded LO measurement process. Enable Embedded LO Check to enable measurement of the Embedded LO. Tuning Method These settings determine the amount of time spent versus the degree of accuracy to which the LO Frequency is measured. You can see that accuracy is becoming compromised when noise starts to appear on the measurement trace. Broadband and Precise Does the entire tuning process for each background sweep. See the Overview for more information. Precise only Does NOT perform broadband tuning on each sweep. Use this setting when the embedded LO is stable. The signal (after broadband) must be within ½ the tuning IFBW. If the signal will always be within ½ the IFBW, broadband tuning is not needed. Most satellite components are within 3 kHz absolute so might not need broadband tuning. Disable tuning Only the previously measured LO Frequency Delta is applied to the reference mixer LO and VNA receivers. Tuning Point Select, or specify, the data point in the mixer sweep that will be used to find the embedded LO frequency. If a marker is enabled, that data point can be used. For broadband and Precise sweeps, choose a point in the mixer sweep where noise is least likely to be found, such as the point of highest gain. This is generally the center of a sweep or the center of a filter if used. Tune every Set the interval at which tuning is performed before a measurement sweep. 'Tune every 3 sweeps' means that every third measurement sweep is preceded by tuning sweeps. If the embedded LO drifts, or if regularly changing DUTs, use 'Tune every 1 sweep'. Broadband Search - Set the frequency span over which to measure the embedded LO frequency. IFBW IF Bandwidth used for Broadband and Precise tuning sweeps. This sets the resolution in the Broadband sweeps and sets the max error (1/2 IFBW) for precise tuning. The larger the IFBW, the faster the sweep, but the signal may not be found. Max Iterations The maximum number of Precise sweeps to make. When this number is reached, the final measurement is used. Tolerance When two consecutive Precise measurements are made within this value, the final measurement is used. If this is not achieved within the Max Iterations value, then the last measurement is used. This is the best of the 'Tunings settings' to change to improve accuracy. LO Frequency Delta The absolute difference between the measured embedded LO frequency and the LO setting that is entered in the Mixer Setup dialog. This value is updated each time the embedded LO frequency is measured. Entering a value is a way to change the LO frequency on the mixer setup without invalidating the calibration. Find Now The VNA finds and measures the actual LO frequency using the current dialog settings. This data is displayed in the Status box. Status window Displays textual and graphical representation of the Embedded LO measurement sweeps. Default Resets the LO Frequency Delta and Tuning parameters to their default settings. Graph... Launches the graphical (spectrum analyzer type) display sweeps of the latest embedded LO measurement.
|
This dialog appears when Graph is clicked on the Embedded LO dialog. Presents a graphical (spectrum analyzer type) display of the latest embedded LO measurement. Click Previous and Next to view available Broadband and Precise sweeps. The LO Frequency is displayed in the Marker annotation. |