The Intermodulation Distortion (IMD) App is offered for both Amplifiers and Converters, and also can be viewed in Swept IMD channels.
Swept IMD channels are used to measure over 150 different IMD parameters. These parameters are built from various selections such as: IMD products, tone power levels, intercept points, at the input and/or output of a DUT. In addition, each parameter can be swept using several different methods.
Learn all about the IMD App (Opt S93087A/B) in the following topics:
FOM (Opt S9x080A)
Opt S9x087A/B (software option only) must be enabled.
External combiner to combine f1 (from internal source of the DRA port) and f2 (from another internal or external source)
At least two sources and 5 test ports
App Note 1408-17 - Making Accurate Intermodulation Distortion Measurements with the PNA-X.