File  |  Instrument  |  Response  |  Stimulus  |  Utility  |  Cal  |  Apps  |  Remote ONLY


 

Description

SCPI

FCA Configure Measurements

Create an FCA measurement

CALCulate:MEASure:DEFine

Change an FCA measurement

CALCulate:MEASure:PARameter

Sweep type

SENSe:SWEep:TYPE

Map DUT ports to PNA ports

SENSe:MIXer:PMAP

Read Input port map

SENSe:MIXer:PMAP:INPut

Read Output port map

SENSe:MIXer:PMAP:OUTPut

Avoid Spurs

SENSe:MIXer:AVOidspurs

 

Minimum required FCA (SMC and VMC) Cal commands

SCPI and COM examples.

Create Cal object

None

Begin Cal

SENSe:CORRection:COLLect:GUIDed:INITiate

Set connector type for each port

SENSe:CORRection:COLLect:GUIDed:CONNector:PORT:SELect

Set Cal Kit for each port

SENSe:CORRection:COLLect:GUIDed:CKIT:PORT:SELect

Returns the number of steps required by the Calibration

SENSe:CORRection:COLLect:GUIDed:STEPs?

Returns the step description.

SENSe:CORRection:COLLect:GUIDed:DESCription?

Measure a standard

SENSe:CORRection:COLLect:GUIDed:ACQuire

Generate Error Terms

SENSe:CORRection:COLLect:GUIDed:SAVE

 

Optional FCA (SMC and VMC) commands

See SMC and VMC specific optional commands

Set THRU method

SENSe:CORRection:COLLect:GUIDed:PATH:TMEThod

Sets ECAL auto-orientation ON or OFF

SENSe:CORRection:PREFerence:ECAL:ORIentation

Sets ECAL port map when orientation is off.

SENSe:CORRection:PREFerence:ECAL:PMAP

Perform or Omit Isolation

SENSe:CORRection:COLLect:GUIDed:ISOLation

 

SMC Optional commands

SMC network embed/deembed

SENSe:CORRection:COLLect:GUIDed:SMC:FSIMulator:NETWork:MODE

SMC filename

SENSe:CORRection:COLLect:GUIDed:SMC:FSIMulator:NETWork:FILename

Import existing Phase Ref Cal or Source Power Cal

SENSe:CORRection:COLLect:GUIDed:SMC:IMPort

Use Thru or perform separate power cals

SENSe:CORRection:COLLect:GUIDed:SMC:PWRCal:SEParate

Include Reverse SC12 sweep

SENSe:MIXer:REVerse

Include input/output match correction

CALCulate:MEASure:CORRection:TYPE

Use Nominal Incident Power

SENSe:MIXer:INPut:POWer:USENominal

Enable LO Power Cal

SENSe:CORRection:COLLect:GUIDed:SMC:LO:PCAL

Save to s2p and s2px file

MMEMory:STORe

Load Power Table (used with mmWave)

SENSe:CORRection:COLLect:GUIDed:PSENsor:POWTable

 

SMC Include Phase

Enable Phase

SENSe:MIXer:PHASe

Enable Absolute Phase

SENSe:MIXer:PHASe:ABSolute[:STATe]

Set normalize point

SENSe:MIXer:NORMalize:POINt

Choose known delay or S2P

SENSe:CORRection:COLLect:GUIDed:SMC:PHASe:METHod

Set known delay

SENSe:CORRection:COLLect:GUIDed:SMC:PHASe:DELay

Set Cal Mixer Char S2P filename

SENSe:CORRection:COLLect:GUIDed:SMC:PHASe:MIXer

Use Phase Ref Cal Set

SENSe:CORRection:COLLect:GUIDed:SMC:IMPort

 

Perform SMC Phase Reference Cal

SCPI

Reset

SYSTem:CALibrate:PHASe:RESet

Start Freq

SYSTem:CALibrate:PHASe:FREQuency:STARt

Stop Freq

SYSTem:CALibrate:PHASe:FREQuency:STOP

Read channel number

SYSTem:CALibrate:PHASe:GUIDed:CHANnel?

Read all Phase Reference IDs

SYSTem:CALibrate:PHASe:REFerence:CATalog?

Set Phase Reference

SYSTem:CALibrate:PHASe:REFerence

Set Source Attenuator

SYSTem:CALibrate:PHASe:POWer:ATTenuator

Set Cal Set name

None

Perform Cal

Guided Cal commands

Use Phase Ref Cal Set

SENSe:CORRection:COLLect:GUIDed:SMC:IMPort

Unknown Mixer calibration state

SYSTem:CALibrate:PHASe:UNKNown:INCLude

Unknown mixer LO frequency

SYSTem:CALibrate:PHASe:UNKNown:LO:FREQuency

Unknown mixer LO power

SYSTem:CALibrate:PHASe:UNKNown:LO:POWer

Input power level to the unknown mixer

SYSTem:CALibrate:PHASe:UNKNown:INPut:POWer

Connector type and gender of your Cal Kit.

SYSTem:CALibrate:PHASe:CONNector

Cal Kit to be used to perform the S-parameter Cal

SYSTem:CALibrate:PHASe:CKIT

Set the ports to be calibrated.

SYSTem:CALibrate:PHASe:PORT[X]

Reverse Port2 Coupler

SYSTem:CALibrate:PHASe:DEEMbed

VMC Optional commands

VMC network embed/deembed

SENSe:CORRection:COLLect:GUIDed:VMC:FSIMulator:NETWork:MODE

VMC filename

SENSe:CORRection:COLLect:GUIDed:VMC:FSIMulator:NETWork:FILename

Enable LO Power Cal

SENSe:CORRection:COLLect:GUIDed:VMC:LO<n>:PCAL

 

FCA Segment Sweep

SCPI examples.

Recalculate

SENSe:MIXer:RECalculate

Segment Calculate

SENSe:MIXer:SEGMent:CALCulate

Query Count

SENSe:MIXer:SEGMent:COUNt?

Add Segments

SENSe:MIXer:SEGMent:ADD

Delete Segments

SENSe:MIXer:SEGMent:DEL

Remove All Segments

SENSe:MIXer:SEGMent:DELete:ALL

State

SENSe:MIXer:SEGMent[:STATe]

Number Of Points

SENSe:MIXer:SEGMent:POINts

IFBW

SENSe:MIXer:SEGMent:BWIDth

Input Fixed Freq

SENSe:MIXer:SEGMent:INPut:FREQuency:FIXed

Input Start Freq

SENSe:MIXer:SEGMent:INP:FREQuency:STARt

Input Stop Freq

SENSe:MIXer:SEGMent:INP:FREQuency:STOP

Input Fixed/Swept

SENSe:MIXer:SEGMent:INP:FREQuency:MODE

Input Power

SENSe:MIXer:SEGMent:INPut:POWer

Output Fixed Freq

SENSe:MIXer:SEGMent:OUTP:FREQuency:FIXed

Output Start Freq

SENSe:MIXer:SEGMent:OUTP:FREQuency:STARt

Output Stop Freq

SENSe:MIXer:SEGMent:OUTP:FREQuency:STOP

Output Fixed/Swept

SENSe:MIXer:SEGMent:OUTP:FREQuency:MODE

Output (+/-)

SENSe:MIXer:SEGMent:OUTP:FREQuency:SIDeband

Output Power

SENSe:MIXer:SEGMent:OUTPut:POWer

LO Fixed Freq

SENSe:MIXer:SEGMent:LO<x>:FREQuency:FIXed

LO Start Freq

SENSe:MIXer:SEGMent:LO<x>:FREQuency:STARt

LO Stop Freq

SENSe:MIXer:SEGMent:LO<x>:FREQuency:STOP

LO Fixed/Swept

SENSe:MIXer:SEGMent:LO<x>:FREQuency:MODE

Input >LO

SENSe:MIXer:SEGMent:LO<x>:FREQuency:ILTI

LO Power

SENSe:MIXer:SEGMent:LO<x>:POWer

IF (+/-)

SENSe:MIXer:SEGMent:IF:FREQuency:SIDeband

Embedded LO (used with FCA, NFX, GCX, MODX, and Swept IMDx)

Embedded LO ON | OFF

SENSe:MIXer:ELO:STATe

Select  tuning point

SENSe:MIXer:ELO:NORMalize:POINt

Set tuning mode

SENSe:MIXer:ELO:TUNing:MODE

Set broadband sweep span

SENSe:MIXer:ELO:TUNing:SPAN

Set precise tuning  tolerance

SENSe:MIXer:ELO:TUNing:TOLerance

Set precise tuning iterations

SENSe:MIXer:ELO:TUNing:ITERations

LO delta frequency

SENSe:MIXer:ELO:LO:DELTA

Resets tuning parameters

SENSe:MIXer:ELO:TUNing:RESet

Reset LO Delta frequency

SENSe:MIXer:ELO:LO:RESET

Resets the LO Frequency Delta and Tuning parameters to their default settings.

SENSe:MIXer:ELO:RESET

Sets and returns the Noise Bandwidth for Broadband and Precise tuning sweeps.

SENSe:MIXer:ELO:TUNing:NBW

Embedded LO Diagnostics (Available with Swept IMDx using COM ONLY)

Clear current diagnostic information

SENSe:MIXer:ELO:DIAGnostic:CLEAr

Get result of the last tuning sweeps.

SENSe:MIXer:ELO:DIAGnostic:STATus?

Get number of tuning sweeps.

SENSe:MIXer:ELO:DIAGnostic:SWEep:COUNt?

Was a marker was used for a tuning sweep?

SENSe:MIXer:ELO:DIAGnostic:SWEep:MARKer:STATe?

Get the marker X-axis position.

SENSe:MIXer:ELO:DIAGnostic:SWEep:MARKer:POSition?

Get the marker annotation.

SENSe:MIXer:ELO:DIAGnostic:SWEep:MARKer:ANNotation?

Get the tuning sweep X axis annotation.

SENSe:MIXer:ELO:DIAGnostic:SWEep:X:ANNotation?

Get the tuning sweep Y axis annotation.

SENSe:MIXer:ELO:DIAGnostic:SWEep:Y:ANNotation?

Get the Start sweep value.

SENSe:MIXer:ELO:DIAGnostic:SWEep:X:STARt?

Get the Stop sweep value.

SENSe:MIXer:ELO:DIAGnostic:SWEep:X:STOP?

Returns the tuning sweep parameter name.

SENSe:MIXer:ELO:DIAGnostic:SWEep:PARameter?

Returns the tuning sweep title.

SENSe:MIXer:ELO:DIAGnostic:SWEep:TITLe?

Returns the LO frequency delta from this tuning sweep

SENSe:MIXer:ELO:DIAGnostic:SWEep:LO:DELTa?

Gain Compression Setup

Create a GCA Meas

CALCulate:MEASure:DEFine

Change a GCA Parameter

CALCulate:MEASure:PARameter

Sweep Type

SENSe:SWEep:TYPE

Number of frequency points

SENSe:GCSetup:SWEep:FREQuency:POINts

Number of power points

SENSe:GCSetup:SWEep:POWer:POINts

Maximum number of points

None

Total number of points

None

Acquisition mode

SENSe:GCSetup:AMODe

Smart tolerance

SENSe:GCSetup:SMARt:TOLerance

Smart Iterations

SENSe:GCSetup:SMARt:MITerations

Smart settling time

SENSe:GCSetup:SMARt:STIMe

Smart show iterations

SENSe:GCSetup:SMARt:SITerations

Read DC at compression point

SENSe:GCSetup:SMARt:CDC

Read compression failures

SENSe:GCSetup:SFAilures?

Write port map

SENSe:GCSetup:PMAP

Read Port Map (Input)

SENSe:GCSetup:PMAP:INPut

Read Port Map (Output)

SENSe:GCSetup:PMAP:OUTPut

Remaps the source port to Port 1.

SENSe:GCSetup:PMAP:SOURce:OVERride

End of Sweep

SENSe:GCSetup:EOSoperation

Linear input power

SENSe:GCSetup:POWer:LINear:INPut:LEVel

Reverse Power

SENSe:GCSetup:POWer:REVerse:LEVel

Start power

SENSe:GCSetup:POWer:STARt:LEVel

Stop power

SENSe:GCSetup:POWer:STOP:LEVel

Compression algorithm

SENSe:GCSetup:COMPression:ALGorithm

Compression Level

SENSe:GCSetup:COMPression:LEVel

Backoff Level

SENSe:GCSetup:COMPression:BACK:LEVel

X Delta

SENSe:GCSetup:COMPression:DELTa:X

Y Delta

SENSe:GCSetup:COMPression:DELTa:Y

Saturation level

SENSe:GCSetup:COMPression:SATuration:LEVel

Interpolation

SENSe:GCSetup:COMPression:INTerpolate[:STATe]

Set and read the desired phase to measure compression.

SENSe:GCSetup:COMPression:PHASe:LEVel

Set and read compression format to be either magnitude, phase, or magnitude and phase.

SENSe:GCSetup:COMPression:PHASe:MODE

Safe Sweep enable

SENSe:GCSetup:SAFE:ENABle

Safe Sweep coarse

SENSe:GCSetup:SAFE:CPADjustment

Safe Sweep fine

SENSe:GCSetup:SAFE:FPADjustment

Safe Sweep threshold

SENSe:GCSetup:SAFE:FTHReshold

Safe Sweep max power

SENSe:GCSetup:SAFE:MLIMit

Set and read the name of the external DC device.

SENSe:GCSetup:SAFE:DC:PARameter

Set and read the maximum limit of the external DC device.

SENSe:GCSetup:SAFE:DC:MLimit

Set and read the DC readings at the compression point in the last iteration of a smart sweep

SENSe:GCSetup:SMARt:CDC

GCA/GCX Phase Commands

Set and read the state of the mixer reference.

SENSe:GCSetup:MIXer:REFerence

Set and read the aperture to use when computing the linear input power.

SENSe:GCSetup:POWer:LINear:INPut:COMPute:APERture

Set and read the state of the power smoothing.

SENSe:GCSetup:SWEep:POWer:SMOoth

Set and read the power smoothing aperture in percent.

SENSe:GCSetup:SWEep:POWer:SMOoth:APERture

Read GCA Data

Read all GCA data

CALCulate:MEASure:GCData:DATA?

Read real GCA data

CALCulate:MEASure:GCData:REAL?

Read imaginary GCA data

CALCulate:MEASure:GCData:IMAG?

Read number of iterations

CALCulate:MEASure:GCD:ITERations?

Gain Compression Analysis

Enable a compression analysis trace

CALCulate:MEASure:GCMeas:ANALysis:ENABle

Set CW frequency

CALCulate:MEASure:GCMeas:ANALysis:CWFRequency

Set to discrete or interpolated CW frequencies

CALCulate:MEASure:GCMeas:ANALysis:DISCrete

Sets X-axis display

CALCulate:MEASure:GCMeas:ANALysis:XAXis

GCA Cal

Read about GCA Cal

Gain Compression Cal

Set power for source power cal

SENSe:CORRection:GCSetup:POWer

Set connector type for power sensor.

SENSe:CORRection:GCSetup:SENSor:CONNector

Set cal kit for power sensor connector.

SENSe:CORRection:GCSetup:SENSor:CKIT

Guided Cal commands

SENSe:CORRection:COLLect:GUIDed

 

Noise Figure Setup

Create Noise Figure meas

CALCulate:CUSTom:DEFine

Change Noise Figure meas

CALCulate:CUSTom:MODify

Sets the number of impedance states to use

 SENSe:NOISe:IMPedance:COUNt

Select Noise Receiver

SENSe:NOISe:RECeiver

Noise averaging ON and OFF

 SENSe:NOISe:AVERage:STATe

Set averaging of noise receiver.

 SENSe:NOISe:AVERage

Set narrowband state

SENSe:NOISe:NARRowband

Set bandwidth of noise receiver.

 SENSe:NOISe:BWIDth

Set gain state of noise receiver.

 SENSe:NOISe:GAIN

Sets the port identifier of the ECal noise tuner that is connected to the PNA Source.

 SENSe:NOISe:TUNer:INPut

Sets the port identifier of the ECal noise tuner that is connected to the DUT.

 SENSe:NOISe:TUNer:OUTPut

Set and read a custom noise tuner file to be used instead of the one generated automatically based on the state.

SENSe:NOISe:TUNer:FILE:NAME

Sets the state of the custom noise tuner file.

SENSe:NOISe:TUNer:FILE[:STATe]

Set the excess noise source ON or OFF.

 CONTrol:NOISe:SOURce or

 OUTPut:MANual:NOISe[:STATe]

Set mechanical switches

SENSe:PATH:CONFig:ELEMent

 

Port Mapping - Noise Figure Opt 028

Write port mapping

SENSe:NOISe:PMAP

Read input port mapping

SENSe:NOISe:PMAP:INPut?

Read output port mapping

SENSe:NOISe:PMAP:OUTPut?

 

Noise Figure Cal - all other cal settings use standard commands.

Create Noise Cal object

N/A

Set Noise Calibration method

 SENSe:NOISe:CALibration:METHod

Set Noise Tuner identifier

SENSe:NOISe:TUNer:ID

Set Noise Recvr Method

SENSe:NOISe:CALibration:RMEThod

Noise source ENR filename

 SENSe:NOISe:ENR:FILename

Set noise source Cal Kit type

 SENSe:NOISe:SOURce:CKIT

Set ambient temperature

 SENSe:NOISe:TEMPerature:AMBient

Enables/disables the use of 302K as the ambient temperature.

SENSe:NOISe:TEMPerature:AMBient:AUTO

Sets the temperature at which the current noise measurement is occurring.

SENSe:NOISe:TEMPerature:SOURce[:VALue]

Enables/disables the use of 302K as the source temperature.

SENSe:NOISe:TEMPerature:SOURce:AUTO

Sets noise source connector type

 SENSe:NOISe:SOURce:CONNector

Set noise source connector temp

SENSe:CORRection:TCOLd:USER:VALue

 

Get/Save Noise Parameters SNP Data

SCPI

Read noise parameter SNP data

SENSe:NOISe:SNP?

Write noise parameters to SNP file

SENSe:NOISe:SNP:SAVE

 

Set and read the state of the thru adapter de-embedding.

SENSe:CORRection:COLLect:NOISe:THRU:ADAPter:DEEMbed[:STATe]

 

Noise Figure ENR File Data Management

Set ENR calibration data.

SENSe:CORRection:ENR:CALibration:TABLe:DATA

PutENRData

Read ENR calibration data.

SENSe:CORRection:ENR:CALibration:TABLe:DATA?

GetENRData

Get/set ID of ENR table.

SENSe:CORRection:ENR:CALibration:TABLe:ID:DATA

ENRID

Get/set serial number of noise source.

SENSe:CORRection:ENR:CALibration:TABLe:SERial:DATA

ENRSN

Sets/Returns the value of the temperature in the ENR file in Kelvin.

SENSe:CORRection:ENR:CALibration:TABLe:TEMPerature:DATA

NoiseCalTemperature

Load ENR table from file.

MMEMory:LOAD:ENR

LoadENRFile

Save ENR table to file.

MMEMory:STORe:ENR

SaveENRFile

 

Differential IQ

Create/Change DIQ Measurement

SCPI

COM

CALCulate:CUSTom:DEFine

CALCulate:CUSTom:MODify

 

Diff IQ Setup Dialog

SENSe:DIQ:FREQuency:RANGe:ADD

SENSe:DIQ:FREQuency:RANGe:DELete

 

DIQ Range Settings Dialog

 

SCPI

Frequency

SENSe:DIQ:FREQuency:RANGe:STARt

SENSe:DIQ:FREQuency:RANGe:STOP

SENSe:DIQ:FREQuency:RANGe:IFBW

Coupling

SENSe:DIQ:FREQuency:RANGe:COUPle:STATe

SENSe:DIQ:FREQuency:RANGe:COUPle:ID

SENSe:DIQ:FREQuency:RANGe:COUPle:OFFSet

SENSe:DIQ:FREQuency:RANGe:COUPle:UCONvert

SENSe:DIQ:FREQuency:RANGe:COUPle:MULTiplier

SENSe:DIQ:FREQuency:RANGe:COUPle:DIvisor

 

DIQ Source Configuration Dialog

SCPI

 

SENSe:DIQ:PORT:STATe

SENSe:DIQ:PORT:RANGe

SOURce:PHASe:EXTernal:CATalog?

SOURce:PHASe:EXTernal:PORT

Power

SENSe:DIQ:PORT:POWer:SWEep

SENSe:DIQ:PORT:POWer:STARt

SENSe:DIQ:PORT:POWer:STOP

SENSe:DIQ:PORT:POWer:ALC:MODE

SENSe:DIQ:PORT:POWer:ATTenuation

SENSe:DIQ:PORT:POWer:ATTenuation:AUTO

Phase

SENSe:DIQ:PORT:PHASe:STATe

SENSe:DIQ:PORT:PHASe:SWEep

SENSe:DIQ:PORT:PHASe:STARt

SENSe:DIQ:PORT:PHASe:STOP

SENSe:DIQ:PORT:PHASe:REFerence

SENSe:DIQ:PORT:PHASe:PARameter

SOURce:PHASe:CONTrol:TOLerance

SOURce:PHASe:CONTrol:ITERation

Match Correction

SENSe:DIQ:PORT:MATCh:STATe

SENSe:DIQ:PORT:MATCh:TRECeiver

SENSe:DIQ:PORT:MATCh:RRECeiver

SENSe:DIQ:PORT:MATCh:RANGe

 

DIQ Edit Parameters Dialog

SCPI

SENSe:DIQ:PARameter:DEFine

SENSe:DIQ:PARameter:DELete

SENSe:DIQ: PARameter:CATalog?

 

DIQ Select X-Axis Dialog

SCPI

CALCulate:X:AXIS:DOMain

CALCulate:X:AXIS

 

SA Application - SA Setup tab

SENSe:SA:BANDwidth:RESolution:CATalog?

SENSe:SA:BANDwidth:[RESolution]

SENSe:SA:BANDwidth:[RESolution]:AUTO

SENSe:SA:BANDwidth:RESolution MIN

SENSe:SA:BANDwidth:RESolution MAX

SENSe:SA:BANDwidth:VIDeo

SENSe:SA:BANDwidth:VIDeo:AUTO

SENSe:SA:BANDwidth:VIDeo MIN

SENSe:SA:BANDwidth:VIDeo MAX

SENSe:SA:DETector:FUNCtion

SENSe:SA:DETector:BYPass:[STATe]

SENSe:SA:BANDwidth:VIDEO:AVERage:TYPE

SENSe:SA:BANDwidth:VIDEO:AVERage:COUNt?

 

Source Setup tab

SENSe:SA:SOURce:SWEep:TYPE

SENSe:SA:SOURce:FREQuency:STARt

SENSe:SA:SOURce:FREQuency:STOP

SENSe:SA:SOURce:FREQuency:CW

SENSe:SA:SOURce:POW:SWEep:POINt:COUNt

SENSe:SA:SOURce:POW:SWEep:REPeat:COUNt

SENSe:SA:SOURce:POWer:STARt

SENSe:SA:SOURce:POWer:STOP

SENSe:SA:SOURce:POWer[:VALue]

SOURce:PHASe:ITERation

SOURce:PHASe:STARt

SOURce:PHASe:STOP

SOURce:PHASe[:FIXed]

SENSe:SA:SOURce:SWEep:FIRst[:DIMension]

SENSe:SA:SOURce:SWEep:POINt:COUNt

SENSe:SA:SOURce:SWEep:REPeat:COUNt

 

Coherence Setup tab

SENSe:SA:COHerence:MULTitone[:STATe]

SENSe:SA:COHerence:MULTitone:DATA

SENSe:SA:COHerence:MULTitone:NYQReject

SENSe:SA:COHerence:MULTitone:SPACing

SENSe:SA:COHerence:MULTitone:PERiod

SENSe:SA:COHerence:MULTitone:REFerence

SENSe:SA:COHerence:MULTitone:HREJect

SENSe:SA:COHerence:MULTitone:VALid

SENSe:SA:COHerence:VECTor:AVERage[:STATe]

SENSe:SA:COHerence:VECTor:AVERage:VALue

SENSe:SA:COHerence:PHASe[:STATe]

SENSe:SA:COHerence:PHASe:STITching:HWTStamp[:STATe]

SENSe:SA:COHerence:PHASe:DISPlay:LEVel

SENSe:SA:COHerence:PHASe:STITching:COMmon[:STATe]

SENSe:SA:COHerence:PHASe:STITching:LEVel

SENSe:SA:COHerence:PHASe:STITching:RECeiver:AUTO[:STATe]

SENSe:SA:COHerence:PHASe:STITching:RECeiver:NAME

SENSe:SA:COHerence:PHASe:STITching[:STATe]

SENSe:SA:DATA:IQ:ALIgned[:STATe]

SENSe:SA:DATA:IQ[:STATe]

SENSe:SA:DATA:IQ:AUTOfill

SENSe:VSA:DATA:SA:RECievers

 

(see VSA Setup commands)

 

SENSe:SA:COHerence:PULSe:SEARch:COUNt

SENSe:SA:COHerence:PULSe:SEARch:DUTY:TOLerance

SENSe:SA:COHerence:PULSe:SEARch:EXECute

SENSe:SA:COHerence:PULSe:SEARch:INITialize

SENSe:SA:COHerence:PULSe:SEARch:ITEM:COUNt?

SENSe:SA:COHerence:PULSe:SEARch:ITEM:PERiod?

SENSe:SA:COHerence:PULSe:SEARch:ITEM:SELect

SENSe:SA:COHerence:PULSe:SEARch:ITEM:WIDTh?

SENSe:SA:COHerence:PULSe:SEARch:PERiod:TOLerance

SENSe:SA:COHerence:PULSe:SEARch:PERiod[:VALue]

SENSe:SA:COHerence:PULSe:SEARch:PRIority

SENSe:SA:COHerence:PULSe:SEARch:WIDTh:TOLerance

SENSe:SA:COHerence:PULSe:SEARch:WIDTh[:VALue]

 

Advanced Setup tab

SENSe:SA:BANDwidth:SHAPe

SENSe:SA:IMAGe:REJect

SENSe:SA:IMAGe:STRENgth

SENSe:SA:BANDwidth:VIDeo:RATio

SENSe:SA:FREQuency:SPAN:BANDwidth[:RESolution]:RATio

SENSe:SA:BANDwidth:SEARch:OCCupied:MIN

SENSe:SA:SOURce:DC:SWEep[:STATe]

SENSe:SA:SOURce:DC:SWEep:POINt

SENSe:SA:SOURce:DC:SWEep:FIRst[:DIMension]

SENSe:SA:FREQuency:CONVerter[:STATe]

SENSe:SA:FREQuency:CONVerter:INPut:SOURce

SENSe:SA:FREQuency:CONVerter:INPut:PORT

SENSe:SA:FREQuency:CONVerter:INPut:CENTer

SENSe:SA:FREQuency:CONVerter:OUTPut:INVerted

SENSe:SA:FREQuency:CONVerter:OUTPut:PORT

SENSe:SA:FREQuency:CONVerter:OUTPut:CENTer

SENSe:SA:FREQuency:CONVerter:OUTPut:OFFSet

(see Embedded LO setup commands)

 

IF Setup tab

SENSe:SA:ADC:FILTer

SENSe:SA:ADC:FILTer:AUTO

SENSe:SA:DFT:BANDwidth:AUTO

SENSe:SA:DFT:BANDwidth:NARRow:MIN

SENSe:SA:DFT:BANDwidth:NARRow:MAX

SENSe:SA:DFT:BANDwidth:WIDE:MIN

SENSe:SA:DFT:BANDwidth:WIDE:MAX

 

Trig. & Pulse Setup tab

SENSe:SA:TRIGer:LEVel[:STATe]

SENSe:SA:TRIGer:LEVel:VALue

SENSe:SA:TRIGer:PERCounter[:STATe]

SENSe:SA:TRIGer:PERCounter:VALue

 

Processing Setup tab

SENSe:SA:DATA:KEEP:FREQuencies:COUNt?

SENSe:SA:DATA:KEEP:RECeivers:COUNt?

SENSe:SA:DATA:KEEP:RECeivers[:CURRent]

SENSe:SA:DATA:KEEP:RECeivers:LIST

SENSe:SA:DATA:KEEP:SCALar:GET?

SENSe:SA:DATA:KEEP[:STATe]

SENSe:SA:DATA:KEEP:VECTor:GET?

SENSe:SA:DFT:TYPE

SENSe:SA:DATA:IQ:CARRier:FREQuency

SENSe:SA:DATA:IQ:DURation?

SENSe:SA:DATA:IQ:ERRor[:CODE]?

SENSe:SA:DATA:IQ:ERRor:TEXT?

SENSe:SA:DATA:IQ:GET?

SENSe:SA:DATA:IQ:SAMPle:COUNt

SENSe:SA:DATA:IQ:SAMPle:RATE

SENSe:SA:TRACe:IMAGe[:STATe]

SENSe:SA:ADC:ACQTime?

SENSe:SA:LO:COUNt?

SENSe:SA:SPAN:BINS:COUNt?

SENSe:SA:DFT:RESolution?

SENSe:SA:DFT:RECord:SIZE?

SENSe:SA:ADC:RECord:SIZE:VALue?

 

ADC & LO Setup tab

SENSe:SA:ADC:OVERload:COUNt?

SENSe:SA:ADC:OVERload:LIST?

SENSe:SA:ADC:OVERload:PERCent

SENSe:SA:ADC:RANGe:PERCent[:MAXimum]?

SENSe:SA:ADC:RANGe:PERCent:MINimum?

SENSe:SA:ADC:RANGe:PERCent:RECeiver?

SENSe:SA:ADC:SAMPle:RATE

SENSe:SA:ADC:SAMPle:RATE:AUTO

SENSe:SA:ADC:SAMPle:DECimation:FIR

SENSe:SA:ADC:DITHer:[STATe]

SENSe:SA:ADC:RECord:SIZE:VALue?

SENSe:SA:ADC:RECord:SIZE:FORCe:VALue

SENSe:SA:ADC:RECord:SIZE:MAX?

SENSe:SA:ADC:RECord:SIZE:MIN?

SENSe:SA:ADC:RECord:SIZE:FORCe[:STATe]

SENSe:SA:ADC:STACking:VALue

SENSe:SA:ADC:STACking:STATe

SENSe:SA:ADC:MREC:SIZE

SENSe:SA:ADC:MREC:PERiod

SENSe:SA:ADC:MREC[:STATe]

SENSe:SA:LO:RANDom[:STATe]

SENSe:SA:LO:BASeband[:STATe]

SENSe:SA:LO:FORCe:OFFSet:DIVider

SENSe:SA:LO:FORCe:OFFSet:MULtiplier

SENSe:SA:LO:FORCe:OFFSet:SOURce

SENSe:SA:LO:FORCe:FREQuency

SENSe:SA:LO:FORCe[:STATe]

SENSe:SA:LO:FREQ:FORCe (obsolete)

SENSe:SA:LO:FREQ:VALue (obsoliete)

 

Data tab

SENSe:SA:DATA:TYPE

SENSe:SA:DATA:STARt?

SENSe:SA:DATA:RECeivers?

SENSe:SA:DATA:RECeivers:LIST

SENSe:SA:DATA:RECeivers:COUNt?

SENSe:SA:DATA:BINs:COUNt?

SENSe:SA:DATA:SIZE?

SENSe:SA:DATA:SIZE:BIN?

SENSe:SA:DATA:SIZE:LOW?

SENSe:SA:DATA:SIZE:HIGH?

SENSe:SA:DATA:FILE:BINary[:STATe]

SENSe:SA:DATA:FILE:TEXT:MARKers[:STATe]

SENSe:SA:DATA:FILE:TEXT[:STATe]

SENSe:SA:DATA:FILE:TEXT:VERBose[:STATe]

SENSe:SA:DATA:FILE:ERASe[:STATe]

SENSe:SA:DATA:FILE:PREFix

SENSe:SA:DATA:FIFO[:STATe]

SENSe:SA:DATA:SHARed[:STATe]

SENSe:SA:DATA:SHARed:NAME

SENSe:SA:DATA:THReshold[:STATe]

SENSe:SA:DATA:THReshold:VALue

SENSe:SA:DATA:WFACtor

SENSe:SA:DATA:IQ:FILE:BINary[:STATe]

SENSe:SA:DATA:IQ:FILE:TEXT[:STATe]

 

SA Marker Settings

Sets and reads the bandwidth of the band density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:BW

CALCulate:SA:MARKer:BDENsity:BW

Returns the band density level in dBm/Hz from the band density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:DATA?

CALCulate:SA:MARKer:BDENsity:DATA?

Marker to SA

CALCulate:MEASure:MARKer:SET SA

Read Band Power

CALCulate:MEASure:SA:MARKer:BPOWer:DATA?

Read/Set Band Power Span

CALCulate:MEASure:SA:MARKer:BPOWer:SPAN

Read/Set Band Power State

CALCulate:MEASure:SA:MARKer:BPOWer:STATe

Sets and reads the state of the band density noise marker.

CALCulate:MEASure:SA:MARKer:BDENsity:NOISe[:STATe]

CALCulate:SA:MARKer:BDENsity:NOISe[:STATe]

Sets and reads the bandwidth of the band power density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:POWer:BW

CALCulate:SA:MARKer:BDENsity:POWer:BW

Sets and reads the state of the band power density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:POWer[:STATe]

CALCulate:SA:MARKer:BDENsity:POWer[:STATe]

Sets and reads the bandwidth of the band tone density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:TONE:BW

CALCulate:SA:MARKer:BDENsity:TONE:BW

Sets and reads the state of the band tone density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:TONE[:STATe]

CALCulate:SA:MARKer:BDENsity:TONE[:STATe]

Sets and reads the spacing of the band tone density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:TONE:TSPacing

CALCulate:SA:MARKer:BDENsity:TONE:TSPacing

Sets and reads the frequency span used by Power Density to normalize the power.

CALCulate:MEASure:SA:MARKer:BDENsity:EQSPan

CALCulate:SA:MARKer:BDENsity:EQSPan

Read occupied bandwidth center frequency

CALCulate:MEASure:SA:MARKer:OCCBand:CENTer?

Set and read occupied bandwidth percentage of span

CALCulate:MEASure:SA:MARKer:OCCBand:PERCent

Read the occupied bandwidth power.

CALCulate:MEASure:SA:MARKer:OCCBand:POWer?

Read occupied bandwidth span

CALCulate:MEASure:SA:MARKer:OCCBand:SPAN?

Set occupied bandwidth state

CALCulate:MEASure:SA:MARKer:OCCBand[:STATe]

 

IQMod - Modulation Settings for NPR Measurements

SOURce:MODulation[:STATe]

SOURce:MODulation:LOAD

Create/Edit Mod File...

SOURce:MODulation:AUTO:SA[:STATe]

SOURce:MODulation:AUTO:IMMediate

SOURce:MODulation:AUTO:NPR[:STATe]

SOURce:MODulation:AUTO:NPR:GBANd

SOURce:MODulation:AUTO:ACPR[:STATe]

SOURce:MODulation:AUTO:ACPR:GBANd

SOURce:MODulation:CORRection[:STATe]

Calibrate Modulation...

SENSe:SA:SOURce:POWer[:VALue]

Source Path Amplification (= Power Offset)

 

Miscellaneous SA Commands

Zooms in on signal within a SA sweep.

SENSe:SA:FREQuency:TUNE:IMMediate

 

Mixer Setup commands

Used for FCA, Swept IMDx, IMx Spectrum, NFx, and GCx applications.

See the Mixer / Converter Setup topic

Create or Change a Custom (Application) Measurement

Create a custom measurement

CALCulate:CUSTom:DEFine

Change a custom measurement

CALCulate:CUSTom:MODify

Return handle to a converter object

None

Mixer Bottom Buttons and X-Axis display

Load a mixer setup

SENSe:MIXer:LOAD

Save a mixer setup

SENSe:MIXer:SAVE

Apply mixer settings

SENSe:MIXer:APPLy

Discard Changes

SENSe:MIXer:DISCard

X-axis display

CALCulate:MEASure:MIXer:XAXis

 

Mixer Frequency Tab

Calculate Input and Output frequencies

SENSe:MIXer:CALCulate

Input to swept or fixed

SENSe:MIXer:INPut:FREQuency:MODE

Input start frequency

SENSe:MIXer:INPut:FREQuency:STAR

Input stop frequency

SENSe:MIXer:INPut:FREQuency:STOP

Input power level

SENSe:MIXer:INPut:POWer

Input fixed frequency

SENSe:MIXer:INPut:FREQuency:FIXed

Set LO

LO freq fixed or swept

SENSe:MIXer:LO:FREQuency:MODE

LO fixed frequency

SENSe:MIXer:LO:FREQuency:FIXed

LO start frequency

SENSe:MIXer:LO:FREQuency:STARt

LO stop frequency

SENSe:MIXer:LO:FREQuency:STOP

Input Greater / Less that LO

SENSe:MIXer:LO:FREQuency:ILTI

Set IF

Sideband (high or low)

SENSe:MIXer:IF:FREQuency:SIDE

IF start frequency

SENSe:MIXer:IF:FREQuency:STARt

IF stop frequency

SENSe:MIXer:IF:FREQuency:STOP

Set Output

Sideband (high or low)

SENSe:MIXer:OUTPut:FREQuency:SIDE

Output start frequency

SENSe:MIXer:OUTPut:FREQuency:STARt

Output stop frequency

SENSe:MIXer:OUTPut:FREQuency:STOP

Output to swept or fixed

SENSe:MIXer:OUTPut:FREQuency:MODE

Output fixed frequency

SENSe:MIXer:OUTPut:FREQuency:FIXed

 

Mixer (LO)Power tab

LO power

SENSe:MIXer:LO:POW

LO power start

SENSe:MIXer:LO:POW:STARt

LO power stop

SENSe:MIXer:LO:POW:STOP

Source Attenuator

SOURce:POWer:ATTenuation

Receiver Attenuator

SENSe:POWer:ATTenuator

Leveling Mode

 

 

Mixer Setup tab

Number of LOs (1 or 2)

SENSe:MIXer:STAGe

Recall a previously-configured external source.

SENSe:MIXer:LO:NAME

Assign a source to mixer input or LO.

SENSe:MIXer:ROLE:DEVice

Read all assigned roles

SENSe:MIXer:ROLE:CATalog?

Read the source assigned to a role.

SENSe:MIXer:ROLE:DEVice

Input Numerator Frac.Mult

SENSe:MIXer:INPut:FREQuency:NUMerator

Input Denominator Frac.Mult

SENSe:MIXer:INPut:FREQuency:DENominator

LO Numerator Frac. Mult.

SENSe:MIXer:LO:FREQuency:NUMerator

LO Denominator Frac.Mult

SENSe:MIXer:LO:FREQuency:DENominator

Enhanced Time Domain Analysis (TDR)

Setup and execution of TDR measurement Commands

Sets the type of parameter and format allocation for each trace.

 

CALCulate:TDR:ALLocate

Sets the DUT topology.

 

CALCulate:TDR:DEVice

Sets the emphasis post1 level.

 

CALCulate:TDR:EMPHasis:CURSor:POST1

Sets the emphasis post2 level.

 

CALCulate:TDR:EMPHasis:CURSor:POST2

Sets the emphasis pre1 level.

 

CALCulate:TDR:EMPHasis:CURSor:PRE1

Turns the emphasis function state ON or OFF.

 

CALCulate:TDR:EMPHasis:STATe

Sets the equalization CTLE DC gain parameter.

 

CALCulate:TDR:EQUalization:CTLE:DC

Sets the equalization CTLE Pole1 parameter.

 

CALCulate:TDR:EQUalization:CTLE:POLE1

Sets the equalization CTLE Pole2 parameter.

 

CALCulate:TDR:EQUalization:CTLE:POLE2

Sets the equalization CTLE zero parameter.

 

CALCulate:TDR:EQUalization:CTLE:ZERO1

Sets the filename of the equalization equation user file.

 

CALCulate:TDR:EQUalization:FILename

Turns the equalization function state ON or OFF.

 

CALCulate:TDR:EQUalization:STATe

Sets the equalization type.

 

CALCulate:TDR:EQUalization:TYPE

Executes the calculation for the simulated eye diagram for the active trace.

 

CALCulate:TDR:EYE:EXECute

Sets the bits' power of 2 for a PRBS pattern.

 

CALCulate:TDR:EYE:INPut:BPATtern:LENGth

Sets the bit pattern type for the simulated eye function.

 

CALCulate:TDR:EYE:INPut:BPATtern:TYPE

Sets the bit rate in bits/sec for the simulated eye function.

 

CALCulate:TDR:EYE:INPut:DRATe

Sets the display limit value.

 

CALCulate:TDR:EYE:INPut:JITTer:DLIMit

Sets the periodic jitter frequency.

 

CALCulate:TDR:EYE:INPut:JITTer:PERiodic:FREQuency

Sets the periodic jitter magnitude in rms.

 

CALCulate:TDR:EYE:INPut:JITTer:PERiodic:MAGNitude

Sets the random jitter magnitude in rms

 

CALCulate:TDR:EYE:INPut:JITTer:RANDom:MAGNitude

Turns the jitter function state with simulated eye ON or OFF.

 

CALCulate:TDR:EYE:INPut:JITTer:STATe

Sets the jitter function type for the simulated eye function.

 

CALCulate:TDR:EYE:INPut:JITTer:TYPE

Sets the voltage level for bit "1" for the simulated eye function.

 

CALCulate:TDR:EYE:INPut:OLEVel

Sets the rise time value for the simulated eye function.

 

CALCulate:TDR:EYE:INPut:RTIMe:DATA

Sets the rise time threshold for the simulated eye.

 

CALCulate:TDR:EYE:INPut:RTIMe:THReshold

Sets the voltage level for bit "0" for the simulated eye function.

 

CALCulate:TDR:EYE:INPut:ZLEVel

Returns the mask test result.

 

CALCulate:TDR:EYE:MASK:FAIL?

Turns the mask test function state with simulated eye ON or OFF.

 

CALCulate:TDR:EYE:MASK:STATe

Returns the results of the eye measurement.

 

CALCulate:TDR:EYE:RESults:DATA?

Turns the overlay ON or OFF.

 

CALCulate:TDR:EYE:RESults:DISPlay:STATe

Sets the rise time threshold level for the results of eye measurement.

 

CALCulate:TDR:EYE:RESults:THReshold

Turns the Eye/Mask window ON or OFF.

 

CALCulate:TDR:EYE:STATe

Sets active marker number.

 

CALCulate:TDR:MEASure[1-16]:ACTive:MARKer

Returns the delta time result value.

 

CALCulate:TDR:MEASure[1-16]:DTIMe:DATA?

Sets delta time reference position.

 

CALCulate:TDR:MEASure[1-16]:DTIMe:POSition

Turns the delta time marker in the marker search ON or OFF.

 

CALCulate:TDR:MEASure[1-16]:DTIMe:STATe

Sets the target trace number for the delta time function.

 

CALCulate:TDR:MEASure[1-16]:DTIMe:TARGet

Sets the trace format.

 

CALCulate:TDR:MEASure[1-16]:FORMat

Sets the measurement parameter.

 

CALCulate:TDR:MEASure[1-16]:PARameter

Sets state for the peeling function.

 

CALCulate:TDR:MEASure[1-16]:PEELing:STATe

Sets state for the smoothing function.

 

CALCulate:TDR:MEASure[1-16]:SMOothing:STATe

Sets the impulse width value for the transform function.

 

CALCulate:TDR:MEASure[1-16]:TIME:IMPulse:WIDTh

Sets rise time value for the transform function.

 

CALCulate:TDR:MEASure[1-16]:TIME:STEP:RTIMe

Sets the rise time threshold level for the results of eye measurement.

 

CALCulate:TDR:MEASure[1-16]:TIME:STEP:RTIMe:THReshold

Sets the stimulus type for the transform function.

 

CALCulate:TDR:MEASure[1-16]:TIME:TYPE

Returns the rise time result value for marker search.

 

CALCulate:TDR:MEASure[1-16]:TTIMe:DATA?

Displays the rise time marker.

 

CALCulate:TDR:MEASure[1-16]:TTIMe:STATe

Sets the rise time threshold for the rise time in the marker search function.

 

CALCulate:TDR:MEASure[1-16]:TTIMe:THReshold

Enable/Disable slope flattening function.

 

CALCulate:TDR:MEASure:SFLatten:STATe

Set the start time of slope flattening.

 

CALCulate:TDR:MEASure:SFLatten:STARt

Set the stop time of slope flattening.

 

CALCulate:TDR:MEASure:SFLatten:STOP

Display TDR Commands

 

 

Turns the continuous auto-scale mode for the eye y-axis ON or OFF.

 

DISPlay:TDR:EYE:Y:SCALe:AUTO:STATe

Sets the value of the y-axis scale per division for eye diagram.

 

DISPlay:TDR:EYE:Y:SCALe:PDIVision

Sets the value of the eye diagram y-axis reference line.

 

DISPlay:TDR:EYE:Y:SCALe:RLEVel

Sets the value of the eye diagram y-axis reference position.

 

DISPlay:TDR:EYE:Y:SCALe:RPOSition

Changes the background color of the screen.

 

DISPlay:TDR:IMAGe

Sets the display to off, data type, memory type, or data and memory type.

 

DISPlay:TDR:MEASure[1-16]:DMEMory:TYPE

Executes x-axis auto scaling.

 

DISPlay:TDR:MEASure[1-16]:X:SCALe:AUTO

Sets the value of the x-axis scale per division.

 

DISPlay:TDR:MEASure[1-16]:X:SCALe:PDIVision

Sets the value of the x-axis reference line.

 

DISPlay:TDR:MEASure[1-16]:X:SCALe:RLEVel

Executes y-axis auto scaling.

 

DISPlay:TDR:SCALe:AUTO

Sets the x-axis reference position for the time domain measurement.

 

DISPlay:TDR:SCALe:RPOSition

Selects the view point for waveform analysis either before or after the DUT.

 

DISPlay:TDR:VIEW

Sets or gets the minimize state.

 

DISPlay:TDR:MINimize:STATe

Memory TDR Commands

 

 

Loads the specified user bit pattern file.

 

MMEMory:TDR:LOAD[:EYE]:BPATtern

Loads eye-mask file.

 

MMEMory:TDR:LOAD[:EYE][:MASK]

Stores the user bit pattern file.

 

MMEMory:TDR:STORe[:EYE]:BPATtern

Stores the eye-mask file.

 

MMEMory:TDR:STORe[:EYE][:MASK]

Correction TDR Commands

 

 

Executes load measurement.

 

SENSe:CORRection:TDR:COLLection:DLComp:LOAD

Executes open measurement.

 

SENSe:CORRection:TDR:COLLection:DLComp:OPEN

Saves the result of the Loss Compensation sequence.

 

SENSe:CORRection:TDR:COLLection:DLComp:SAVE

Executes a thru measurement.

 

SENSe:CORRection:TDR:COLLection:DLComp:THRU

Executes fixture compensation after ECAL.

 

SENSe:CORRection:TDR:COLLection:ECAL:FCOMp:IMMediate

Executes full calibration using the ECal module.

 

SENSe:CORRection:TDR:COLLection:ECAL:IMMediate

Sets the dielectric constant value.

 

SENSe:CORRection:TDR:DCONstant

Executes deskew (auto port extension).

 

SENSe:CORRection:TDR:EXTension:AUTO:IMMediate

Sets the standard type for auto port extension.

 

SENSe:CORRection:TDR:EXTension:AUTO:STANdard

Enable Loss Compensation in Fixture Compensation

 

SENSe:CORRection:EXTension:AUTO:LOSS

Set start frequency in Fixture Compensation

 

SENSe:CORRection:EXTension:AUTO:STARt

Set stop frequency in Fixture Compensation

 

SENSe:CORRection:EXTension:AUTO:STOP

 

Sets the reference impedance value.

 

SENSe:CORRection:TDR:RIMPedance

Bandwidth, DUT information, avoid spurious function, and sweep TDR Commands

Sets the IF bandwidth value.

 

SENSe:TDR:BWIDth[:RESolution]

Executes auto DUT length setting.

 

SENSe:TDR:DLENgth:AUTO:IMMediate

Sets the DUT length value.

 

SENSe:TDR:DLENgth:DATA

Executes avoid spurious.

 

SENSe:TDR:SPURious:AVOid:IMMediate

Queries the avoid spurious state.

 

SENSe:TDR:SPURious:AVOid:STATe?

Sets the value of input bit rate for avoid spurious.

 

SENSe:TDR:SPURious:INPut:DRATe

Queries the Hot TDR mode status.

 

SENSe:TDR:SPURious:STATe?

Sets the TDR averaging trigger state on/off.

 

SENSe:TDR:SWEep:AVERage

Sets trigger mode.

 

SENSe:TDR:SWEep:MODE

Executes single trigger.

 

SENSe:TDR:SWEep:SINGle

Enables/disables the Reduce IF BW at Low Frequencies feature in segments with IFBW arbitrary.

 

SENSe:TDR:BWIDth:TRACk:FORCe

Source Power Level TDR Command

Sets the source power level.

 

SOURce:TDR:POWer[:LEVel][:IMMediate][:AMPLitude]

Preset TDR Command

Executes a TDR preset.

 

SYSTem:TDR:PRESet

 

Active (Hot) Parameters

Sets whether or not interpolation is on for display.

SENSe:ACTive:DISP:INTerpolate[:STATe]

DisplayInterpolationState

Set and read a fixed input power level.

SENSe:ACTive:DISPlay:TRACe:IPWer

DisplayInputPower

Set and read the number of phase points.

SENSe:ACTive:SWEep:PHASe:POINt

PhaseSweepPoints

Set and read the start power level for a 3D sweep.

SENSe:ACTive:SWEep:POWer:STARt

StartPowerIn3DSweep

Set and read the number of power steps for a 3D sweep.

SENSe:ACTive:SWEep:POWer:STEP

PowerStepsIn3DSweep

Set and read the stop power level for a 3D sweep.

SENSe:ACTive:SWEep:POWer:STOP

StopPowerIn3DSweep

Set and read the sweep type.

SENSe:ACTive:SWEep:TYPE

SweepType

Set and read the tuning tone mode.

SENSe:ACTive:TTONe:MODE

ExtractionToneMode

Set and read the absolute tone power level.

SENSe:ACTive:TTONe:ABSolute

AbsoluteExtractionToneLevel

Set and read the tone power relative to the input power (dBc).

SENSe:ACTive:TTONe:RELative

RelativeExtractionToneLevel

Set and read the X-axis domain type.

CALC:X:AXIS:DOMain

DisplayDomain

 

Modulation Distortion Commands

Sets and returns the noise bandwidth.

SENSe:SA:BANDwidth:NOISe

Enable or disable setting the noise bandwidth to its maximum possible value.

SENSe:SA:BANDwidth:NOISe:AUTO

Selects between a narrow and wide IF filter anti-aliasing path.

SENSe:DISTortion:ADC:FILTer:TYPE

This command launches the Receiver IF Cal.

SENSe<cnum>:DISTortion:CORRection:COLLect:IF:ACQuire [SYNChronous | ASYNchronous]

Identifies the normalization used for the EVM measurements.

SENSe:DISTortion:EVM:NORMalize

Sets and returns the frequency span window used for modeling the DUT's gain and distortion.

SENSe:DISTortion:MEASure:CORRelation:APERture

Enable or disable automatic calculation of the frequency span window used for modeling the DUT's gain and distortion.

SENSe:DISTortion:MEASure:CORRelation:APERture:AUTO[:STATe]

Sets and returns the integration bandwidth (IBW) of the lower ACP measurement.

SENSe:DISTortion:MEASure:BAND:ACP:LOWer:IBW

Sets and returns the lower ACP measurement offset.

SENSe:DISTortion:MEASure:BAND:ACP:LOWer:OFFSet

Sets and returns the integration bandwidth (IBW) of the upper ACP measurement.

SENSe:DISTortion:MEASure:BAND:ACP:UPPer:IBW

Sets and returns the upper ACP measurement offset.

SENSe:DISTortion:MEASure:BAND:ACP:UPPer:OFFSet

Adds a new distortion measurement band.

SENSe:DISTortion:MEASure:BAND:ADD

Automatically fills in the measurement settings for all bands from the currently active modulation file loaded in the source.

SENSe:DISTortion:MEASure:BAND:AUTofill

Sets and returns the carrier (Signal) integration bandwidth (IBW) for the distortion measurement.

SENSe:DISTortion:MEASure:BAND:CARRier:IBW

Sets and returns the carrier offset (Signal).

SENSe:DISTortion:MEASure:BAND:CARRier:OFFSet

Queries the total number of distortion measurement bands.

SENSe:DISTortion:MEASure:BAND:COUNt?

Deletes the specified distortion measurement band.

SENSe:DISTortion:MEASure:BAND:DELete

Deletes all existing bands and adds a single default band back into the Measurement Band Table.

SENSe:DISTortion:MEASure:BAND:INITialize

Assigns a name to the specified distortion measurement band.

SENSe:DISTortion:MEASure:BAND:NAME

Sets and returns the notch integration bandwidth (IBW) for an NPR Notch modulation measurement.

SENSe:DISTortion:MEASure:BAND:NOTCh:IBW

Sets and returns the notch offset for an NPR Notch modulation measurement.

SENSe:DISTortion:MEASure:BAND:NOTCh:OFFSet

Set and read the modulation distortion type.

SENSe:DISTortion:MEASure:BAND:TYPE

Sets the measurement filter to either None (default) or RRC (root-raised-cosine filter)

SENSe:DISTortion:MEASure:FILTer

Sets and returns the Alpha factor of the measurement filter.

SENSe:DISTortion:MEASure:FILTer:ALPHa

Sets and returns the Symbol Rate of the filter.

SENSe:DISTortion:MEASure:FILTer:SRATe

Enables or disables using the symbol rate from the file.

SENSe:DISTortion:MEASure:FILTer:SRATe:AUTO[:STATe]

Sets and returns the distortion modulation source name.

SENSe:DISTortion:MODulate:SOURce

Sets and returns the VNA port number connected to the DUT input.

SENSe:DISTortion:PATH:DUT:INPut

Sets and returns the nominal DUT gain.

SENSe:DISTortion:PATH:DUT:NOMinal:GAIN

Sets and returns the nominal DUT noise figure.

SENSe:DISTortion:PATH:DUT:NOMinal:NF

Include or exclude the NF nominal value.

SENSe:DISTortion:PATH:DUT:NOMinal:NF:INCLude

None

Sets and returns the VNA port number connected to the DUT output.

SENSe:DISTortion:PATH:DUT:OUTPut

Enables or disables the external modulated source to pass through the attenuator of the specified PNA source

SENSe:DISTortion:PATH:SOURce:ATTenuation:INCLude

Sets and returns the nominal gain of an external source amplifier.

SENSe:DISTortion:PATH:SOURce:NOMinal:AMPLifier

Enables or disables receiver timing auto generation from the source pulse timing.

SENSe:DISTortion:PULSe:RECeiver:AUTO

Sets and returns the carrier center frequency.

SENSe:DISTortion:SWEep:CARRier:FREQuency

Selects between a ramp type power sweep or a list of power values to define a power sweep.

SENSe:DISTortion:SWEep:POWer:CARRier:LEVel:TYPE

Adds a new row to the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:ADD

Deletes the specified row from the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:DELete

Sets and returns the power level used for the specified row in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:LEVel

Specifies the file path to recall a previous power sweep list file.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:LOAD

Sets and returns the noise bandwidth setting used for the specified row in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:NBW

Selects the noise bandwidth mode in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:NBW:MODE

Sets and returns the number of power points to measure for the power sweep list measurement.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:POINts

Sets and returns the receiver attenuation for the specified row in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:RECeiver:ATTenuation

Selects the receiver attenuation mode in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:RECeiver:ATTenuation:MODE

Specifies the file path to save a power sweep list file.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:SAVE

Sets and returns the source attenuation for the specified row in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:SOURce:ATTenuation

Selects the source attenuation mode in the power sweep list table.

SENSe:DISTortion:SWEep:POWer:CARRier:LIST:SOURce:ATTenuation:MODE

Sets and returns the starting power level for the power sweep ramp measurement.

SENSe:DISTortion:SWEep:POWer:CARRier:RAMP:LEVel:STARt

Sets and returns the stop power level for the power sweep ramp measurement.

SENSe:DISTortion:SWEep:POWer:CARRier:RAMP:LEVel:STOP

Enable or disable increasing noise bandwidth at high powers automatically for faster measurements.

SENSe:DISTortion:SWEep:POWer:CARRier:RAMP:NBW:AUTO

Sets and returns the number of power points to measure for the power sweep ramp measurement.

SENSe:DISTortion:SWEep:POWer:CARRier:RAMP:POINts

Enable or disable the re-use of the previous linear S-parameter measurements if available and skip sweep.

SENSe:DISTortion:SWEep:SPARam:REUSe

Enable or disable noise sweep used for the distortion test.

SENSe:DISTortion:SWEep:NOISe

Enables or disables S-parameter sweep.

SENSe:DISTortion:SWEep:SPARam[:STATe]

Sets and returns the power level used to measure the DUT gain when operating in its linear region.

SENSe:DISTortion:SWEep:POWer:SPARam:LEVel

Sets and returns the IF bandwidth for the linear S21 sweep.

SENSe:DISTortion:SWEep:SPARam:BWIDth

Sets and returns the step size for the linear S21 sweep.

SENSe:DISTortion:SWEep:SPARam:STEP

 Selects between a chirp signal from the external signal generator or an internal CW signal in the VNA for measuring S-parameters.

SENSe:DISTortion:SWEep:SPARam:TYPE

Sets and returns the power level used for the distortion test at either the input or output of the DUT.

SENSe:DISTortion:SWEep:POWer:CARRier:LEVel

Set and read where to apply power to the DUT (input or output).

SENSe:DISTortion:SWEep:POWer:CARRier:LEVel:PORT

Keeps RF power ON at the End of Sweep.

SENSe:DISTortion:SWEep:RETRace:POWer

Sets and returns the delay in seconds before the test signal to allow the RF source to settle.

SENSe:DISTortion:SWEep:DWELl

Selects between a fixed or power sweep type of sweep.

SENSe:DISTortion:SWEep:TYPE

Specifies the file path to save a modulation distortion table file.

SENSe:DISTortion:TABLe:DISPlay:SAVE

Sort distortion table by band or power.

SENSe:DISTortion:TABLe:DISPlay:SORT

LO Feedthru Monitor Commands

 

Return the last monitor result of LO feedthru monitor.

SENSe:SA:COHerance:LO:FTHRu:MONitor:LAST:FAILed

Return the last monitor value of LO feedthru monitor.

SENSe:SA:COHerance:LO:FTHRu:MONitor:LAST:VALue

Set and read the target receiver for LO Feedthru monitor.

SENSe:SA:COHerance:LO:FTHRu:MONitor:RECeiver

Set and read the LO feedthru monitoring state.

SENSe:SA:COHerence:LO:FTHRu:MONitor[:STATe]

Set and read the threshold level for warning.

SENSe:SA:COHerence:LO:FTHRu:MONitor:TOLerance

Set and read the monitoring method for LO feedthru monitor.

SENSe:SA:COHerence:LO:FTHRu:MONitor:TYPE

Calibrate Source Modulation Commands

Set and read the ACP modulation calibration state.

SOURce:MODulation:CORRection:COLLection:ACP:ENABle

Sets and reads the maximum number of iterations for the lower ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:LOWer:ITERations

Sets and reads the receiver for the lower ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:LOWer:RECeiver

Sets and reads the calibration span for a lower ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:LOWer:SPAN

Sets and reads the desired ACP calibration tolerance for the lower ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:LOWer:TOLerance

Enables or disables the upper ACP (ACPUp) modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:UPPer:ENABle

Sets and reads the maximum number of iterations for the upper ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:UPPer:ITERations

Sets and reads the receiver for the upper ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:UPPer:RECeiver

Sets and reads the calibration span for an upper ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:UPPer:SPAN

Sets and reads the desired ACP calibration tolerance for the upper ACP modulation calibration.

SOURce:MODulation:CORRection:COLLection:ACP:UPPer:TOLerance

Setsand reads  the ACP lower  frequency delta from the edge of the carrier to the beginning of the Cal Span.

SOURce:MODulation:CORRection:COLLection:ACP:LOWer:GBANd

Sets and reads the ACP upper frequency delta from the edge of the carrier to the beginning of the calibration span.

SOURce:MODulation:CORRection:COLLection:ACP:UPPer:GBANd

Enable or disable the distortion calibration state.

SOURce:MODulation:CORRection:COLLection:DISTortion:ENABle

Sets and reads the maximum number of iterations used by the calibration routine.

SOURce:MODulation:CORRection:COLLection:DISTortion:ITERations

Sets and reads the receiver for distortion calibration.

SOURce:MODulation:CORRection:COLLection:DISTortion:RECeiver

Sets and reads the calibration span for a distortion calibration.

SOURce:MODulation:CORRection:COLLection:DISTortion:SPAN

Sets and reads the desired distortion calibration tolerance.

SOURce:MODulation:CORRection:COLLection:DISTortion:TOLerance

Enable or disable the equalization calibration state.

SOURce:MODulation:CORRection:COLLection:EQUalization:ENABle

Sets and reads the maximum number of iterations used by the calibration routine.

SOURce:MODulation:CORRection:COLLection:EQUalization:ITERations

Sets and reads the receiver for equalization calibration.

SOURce:MODulation:CORRection:COLLection:EQUalization:RECeiver

Sets and reads the calibration span for a equalization calibration.

SOURce:MODulation:CORRection:COLLection:EQUalization:SPAN

Sets and reads the desired equalization calibration tolerance.

SOURce:MODulation:CORRection:COLLection:EQUalization:TOLerance

Returns a list of  the calibrations stored in the .mdx file.

SOURce:MODulation:FILE:CORRection:CATalog?

Deletes any of the calibration files stored in the .mdx file.

SOURce:MODulation:FILE:CORRection:DELete?

Returns the frequency of the specified source modulation calibration file.

SOURce:MODulation:FILE:CORRection:FREQuency?

Returns the power level of the specified source modulation calibration file.

SOURce:MODulation:FILE:CORRection:POWer?

Append source modulation calibration files stored in the .mdx file.

SOURce:MODulation:CORRection:COLLection:APPend

Sets and reads a fixed frequency.

SOURce:MODulation:CORRection:COLLection:FREQuency[:FIXed]

Sets and reads the number of frequency measurement points.

SOURce:MODulation:CORRection:COLLection:FREQuency:POINts

Sets and reads the start frequency to use for a swept frequency source modulation calibration.

SOURce:MODulation:CORRection:COLLection:FREQuency:STARt

Sets and reads the stop frequency to use for a swept frequency calibration.

SOURce:MODulation:CORRection:COLLection:FREQuency:STOP

Sets and reads the calibration frequency type to fixed or swept.

SOURce:MODulation:CORRection:COLLection:FREQuency:TYPE

Enable or disable the LO feedthru calibration state.

SOURce:MODulation:CORRection:COLLection:LO:FTHRu:ENABle

Sets and reads the maximum number of iterations used by the calibration routine.

SOURce:MODulation:CORRection:COLLection:LO:FTHRu:ITERations

Sets and reads the receiver for LO feedthru modulation calibration.

SOURce:MODulation:CORRection:COLLection:LO:FTHRu:RECeiver

Sets and reads the calibration span for a LO feedthru modulation calibration.

SOURce:MODulation:CORRection:COLLection:LO:FTHRu:SPAN

Sets and reads the desired LO feedthru modulation calibration tolerance.

SOURce:MODulation:CORRection:COLLection:LO:FTHRu:TOLerance

Sets and reads a fixed power level.

SOURce:MODulation:CORRection:COLLection:POWer[:FIXed]

Sets and reads the number of power measurement points.

SOURce:MODulation:CORRection:COLLection:POWer:POINts

Sets and reads the start power level to use for a swept calibration.

SOURce:MODulation:CORRection:COLLection:POWer:STARt

Sets and reads the stop power level to use for a swept calibration.

SOURce:MODulation:CORRection:COLLection:POWer:STOP

Sets and reads the calibration power type to fixed or swept.

SOURce:MODulation:CORRection:COLLection:POWer:TYPE

Create/Edit Modulation File

Sets and reads the source sample rate.

SOURce:MODulation:FILE:INITialize

Specifies the file path to recall a previous modulation file.

SOURce:MODulation:FILE:LOAD

Sets and reads the source sample rate.

SOURce:MODulation:FILE:SAVE

Sets and reads the Carrier offset value.

SOURce:MODulation:FILE:SIGNal:CARRier:OFFSet

Sets and reads the number of compact modulation files to create.

SOURce:MODulation:FILE:SIGNal:COMPact:FILE:NUMBer

Sets and reads the compact modulation file selection.

SOURce:MODulation:FILE:SIGNal:COMPact:FILE:NUMBer:SELect

Specifies the file path to recall a previous modulation file from which to create a compact signal.

SOURce:MODulation:FILE:SIGNal:COMPact:OFILe

Returns the peak-to-average value of the original signal.

SOURce:MODulation:FILE:SIGNal:COMPact:PAVG?

Returns the peak-to-average value of the signal created from the original signal.

SOURce:MODulation:FILE:SIGNal:COMPact:PAVG:CALCulated?

Sets and reads the Peak-to-Avg priority for Compact signals.

SOURce:MODulation:FILE:SIGNal:COMPact:PAVG:PRIority

Allows setup of multiple carriers when defining a multicarrier signal.

SOURce:MODulation:FILE:SIGNal:COMPact:SUBCarrier:NUMBer

Sets and reads the offset of the selected subcarrier.

SOURce:MODulation:FILE:SIGNal:COMPact:SUBCarrier:OFFSet

Sets and reads the span of the selected subcarrier.

SOURce:MODulation:FILE:SIGNal:COMPact:SUBCarrier:SPAN

Sets and reads where to start the compact signal within the original signal.

SOURce:MODulation:FILE:SIGNal:COMPact:TIME:STARt

Returns the calculated start time of the signal created from the original signal.

SOURce:MODulation:FILE:SIGNal:COMPact:TIME:STARt:CALCulated?

Sets and reads the start time priority for Compact signals.

SOURce:MODulation:FILE:SIGNal:COMPact:TIME:STARt:PRIority

Sets and reads the DAC scale as a percentage of full scale.

SOURce:MODulation:FILE:SIGNal:DAC:SCALing

Sets the NPR notch location type for the selected NPR Notch modulation type.

SOURce:MODulation:FILE:SIGNal:NPR:NOTCh:LOCation

Sets and reads the number of NPR notches for NPR Notch modulation type.

SOURce:MODulation:FILE:SIGNal:NPR:NOTCh:NUMBer

Sets and reads the NPR notch offset frequency of the selected notch.

SOURce:MODulation:FILE:SIGNal:NPR:NOTCh:OFFSet

Sets and reads the span of the selected notch.

SOURce:MODulation:FILE:SIGNal:NPR:NOTCh:SPAN

Enables or disables signal optimization settings.

SOURce:MODulation:FILE:SIGNal:OPTimize:ENABle

Sets and reads the number of decimal digits limit for calculated frequencies.

SOURce:MODulation:FILE:SIGNal:OPTimize:FREQuency:LIMit:DDIGits

Enables or disables the number of decimal digits limit for calculated frequencies.

SOURce:MODulation:FILE:SIGNal:OPTimize:FREQuency:LIMit:ENABle

Sets and reads the frequency tolerance value (in percent).

SOURce:MODulation:FILE:SIGNal:OPTimize:FREQuency:TOLerance

Sets and reads the number of test signal harmonics you want to be protected against.

SOURce:MODulation:FILE:SIGNal:OPTimize:HREJect

Sets and reads the maximum distance between each tone.

SOURce:MODulation:FILE:SIGNal:OPTimize:MAX:TONE:SPacing

Sets and reads the minimum number of tones.

SOURce:MODulation:FILE:SIGNal:OPTimize:MIN:TONE:NUMBer

Sets and reads theminimum waveform period.

SOURce:MODulation:FILE:SIGNal:OPTimize:MIN:WAVeform:PERiod

Enables or disables the rejection of Nyquist frequencies.

SOURce:MODulation:FILE:SIGNal:OPTimize:NYQReject:ENABle

Sets the optimize signal type.

SOURce:MODulation:FILE:SIGNal:OPTimize:TYPE

Returns the calculated peak-to-average value.

SOURce:MODulation:FILE:SIGNal:PAVG:CALCulated?

Sets and reads the phase when Fixed phase is the Phase Type.

SOURce:MODulation:FILE:SIGNal:PHASe:FIXed

Sets and reads the phase seed when Random phase is the Phase Type.

SOURce:MODulation:FILE:SIGNal:PHASe:RANDom:SEED

Sets the phase type.

SOURce:MODulation:FILE:SIGNal:PHASe:TYPE

Sets and reads the signal span.

SOURce:MODulation:FILE:SIGNal:SPAN

Returns the calculated signal span.

SOURce:MODulation:FILE:SIGNal:SPAN:CALCulated?

Sets and reads the signal span priority.

SOURce:MODulation:FILE:SIGNal:SPAN:PRIority

Sets and reads the source sample rate.

SOURce:MODulation:FILE:SIGNal:SRATe

Returns the calculated sampling rate of the signal created from the original signal.

SOURce:MODulation:FILE:SIGNal:SRATe:CALCulated?

Set and read the auto sample rate.

SOURce:MODulation:FILE:SIGNal:SRATe:AUTO

Sets and reads the number of tones.

SOURce:MODulation:FILE:SIGNal:TONE:NUMBer

Returns the calculated number of tones.

SOURce:MODulation:FILE:SIGNal:TONE:NUMBer:CALCulated?

Sets and reads the tone number priority.

SOURce:MODulation:FILE:SIGNal:TONE:NUMBer:PRIority

Sets and reads the tone spacing.

SOURce:MODulation:FILE:SIGNal:TONE:SPACing

Returns the calculated spacing between the tones.

SOURce:MODulation:FILE:SIGNal:TONE:SPACing:CALCulated?

Sets and reads the tone spacing priority.

SOURce:MODulation:FILE:SIGNal:TONE:SPACing:PRIority

Returns the number of tones.

SOURce:MODulation:FILE:TONE:NUMBer?

Returns the tone frequency in Hz relative to the carrier.

SOURce:MODulation:FILE:TONE:FREQuency?

Sets and reads the power in dBm of the specified tone number.

SOURce:MODulation:FILE:TONE:POWer

Sets and reads the phase in degrees of the specified tone number.

SOURce:MODulation:FILE:TONE:PHASe

Set specified tone state to on or off.

SOURce:MODulation:FILE:TONE[:STATe]

Set all tone states to on or off.

SOURce:MODulation:FILE:TONE:ALL[:STATe]

Saves the specified multitone file.

SOURce:MODulation:FILE:TONE:SAVE

Loads the specified multitone file.

SOURce:MODulation:FILE:TONE:LOAD

Sets the modulation type.

SOURce:MODulation:FILE:TYPE

Distortion Table Commands

Returns the currently displayed Distortion Table parameters.

SENSe:DISTortion:TABLe:DISPlay:CATalog?

Deletes the specified parameter from the Distortion Table.

SENSe:DISTortion:TABLe:DISPlay:DELete

Adds the specified parameter to the Distortion Table.

SENSe:DISTortion:TABLe:DISPlay:FEED

Returns a list of existing band names from the Measurement Band Table.

SENSe:DISTortion:TABLe:CATalog?

Returns a list of data parameter names corresponding to the currently specified Measurement Type.

SENSe:DISTortion:TABLe:DATA:CATalog?

Returns a list of data values from the Distortion Table for the specified band and parameter name.

SENSe:DISTortion:TABLe:DATA:VALue?

 

 

Modulation Distortion Marker Commands

Set and read the SA marker function type.

CALCulate:MEASure:SA:MARKer:BAND:FUNCtion

Sets and reads the integration bandwidth marker.

CALCulate:MEASure:SA:MARKer:BAND:IBW

Sets and reads the ACPR density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:ACPR[:STATe]

CALCulate:SA:MARKer:BDENsity:ACPR[:STATe]

Sets and reads the NPR density marker.

CALCulate:MEASure:SA:MARKer:BDENsity:NPR[:STATe]

CALCulate:SA:MARKer:BDENsity:NPR[:STATe]

Executes the search ACPR density marker.

CALCulate:MEASure:SA:MARKer:SEARch:ACPR

Executes the search NPR density marker.

CALCulate:MEASure:SA:MARKer:SEARch:NPR

 

 

Measurement Data

Retrieves trace data (Y data) from the modulation distortion measurement.

CALCulate:MEASure:DATA:BUFFer:Y?

Retrieves frequency tone data from the modulation distortion measurement.

CALCulate:MEASure:DATA:BUFFer:X?