Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the Maximum Allowed UL TX Power setting. The setting can be set in active cell operating mode only when the call status is Idle, or in other operating modes. If BCCH Update Page is set to Auto and you change the setting while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure ; If BCCH Update Page is set to Inhibit (the default value) and you change the setting while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change (see CALL:BCCHannel:UPDAte:PAGE AUTO). |
|
Setting |
Range: -50 to +33 dBm |
|
Query |
Range: -50 to +33 |
|
*RST Setting |
33 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:TXPower:LEVel:MAXimum 33" |
|
Function |
Sets/queries the UpPCH Power Ramp Step setting. |
|
Setting |
Range: 0|1|2|3 dB |
|
Query |
Range: 0|1|2|3 |
|
*RST Setting |
3 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:UPPChannel:POWer:STEP 3" |
|
Function |
Sets/queries Desired UpPCH RX Power. The setting can be set in active cell operating mode only when the call status is Idle, or in other operating modes. |
|
Setting |
Range: -120 to -58 dBm |
|
Query |
Range: -120 to -58 |
|
*RST Setting |
-100 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:UPPChannel:POWer:LEVel -100" |
|
Function |
Queries the Initial UpPCH TX Power. |
|
Query |
Range: -65 to +30 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:UPPChannel:POWer:INITial?" |
|
Function |
Sets/queries SYNC UL Code Bitmap setting. |
|
Setting |
Range: 0000 0001 to 1111 1111 |
|
Query |
Range: 0000 0001 to 1111 1111 |
|
*RST Setting |
1111 1111 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:UPPChannel:SYNChronize:CBITmap '00000001'" |
|
Function |
Sets/queries the maximum numbers of SYNC_UL transmissions in a synchronisation attempt initiated by the UE. This parameter will be sent in SIB5 on BCCH. |
|
Setting |
Range: TRANsmit1 | TRANsmit2 | TRANsmit4 | TRANsmit8 |
|
Query |
Range: TRAN1|TRAN2|TRAN4|TRAN8 |
|
*RST Setting |
TRANsmit8 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:UPPChannel:SYNChronize:TRANsmission:MAXimum TRANsmit8" |
|
Function |
Sets/queries the maximum number of synchronisation attempts in one random access procedure. This parameter will be sent in SIB5 on BCCH. |
|
Setting |
Range: 1 to 32 |
|
Query |
Range: 1 to 32 |
|
*RST Setting |
32 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:UPPChannel:SYNChronize:ANUMber:MAXimum 32" |
|
Function |
Sets/queries Desired PRACH RX Power. The setting can be set in active cell operating mode only when the call status is Idle, or in other operating modes. |
|
Setting |
Range: -120 to -80 dBm |
|
Query |
Range: -120 to -80 |
|
*RST Setting |
-100 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:PRAChannel:POWer:LEVel -100" |
|
Function |
Queries the Initial PRACH TX Power. |
|
Query |
Range: -65 to +30 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:UPLink:PRAChannel:POWer:INITial:LEVel?" |