Call Setup Screen

Last updated: 2010-03-10

Active Cell Operating Mode Screen

TD-SCDMA Test Operating Mode Screen

CW Operating Mode Screen

Active Cell Connection State

Active Cell Operating Mode Screen

Click on the red circle for more information.

UE Information

GPIB command: CALL:MS:REPorted:IMSI[:SELected]?

GPIB command: CALL:MS:REPorted:IMEI:CALCulated:TATDscdma?

You can also query the UE direct-reported IMEI whose last digit is "0" by CALL:MS:REPorted:IMEI:TATDscdma?

GPIB command: CALL:MS:REPorted:PCLass[:SELected]?

GPIB command: CALL:MS:REPorted:UPPChannel:DETected:SIGnature?

GPIB command: CALL:MS:REPorted:ASTRatum:RINDicator

GPIB command: CALL:HSDPa:MS:REPorted:HSDSchannel:CATegory?

GPIB command: CALL:HSUPa:MS:REPorted:EDCHannel:CATegory?

UE Expected Open Loop Transmit Power

Initial UpPCH Tx Power = (Broadcast Primary CCPCH Tx Power – Cell Power – P-CCPCH Power Level Offset) + Desired UpPCH RX Power.

GPIB command: CALL:UPLink:UPPChannel:POWer:INITial[:LEVel]?

Initial PRACH Tx Power = (Broadcast Primary CCPCH Tx Power – Cell Power – P-CCPCH Power Level Offset) + Desired PRACH RX Power.

GPIB command: CALL:UPLink:PRAChannel:POWer:INITial[:LEVel]?

Call Processing Status

GPIB command: CALL:STATus:RRC:STATe?  

MM Status indicates whether the UE has registered, and what type of registration (Location Updating procedure) was last performed. When the UE registers with the network, its Location Updating Request message includes a Location Updating Type information element that can have a value of "Normal location updating", "Periodic updating" or "IMSI attach" (see 3GPP TS 24.008 s4.4.1, s9.2.15 and s10.5.3.5).

GPIB command: CALL:STATus:MM?  

GMM State indicates the result of the most recent GPRS attach or detach.

GPIB command: CALL:STATus:GMM?  

HSDPA Information

The HSDPA Information window displays counters to help you monitor the HSDPA connection status. The results are continually updated until one of the following occurs:

When one of these events occurs, the counters reset to zero and then resume counting.

The HSDPA Information window provide similar results to the HSDPA BLER measurement (see HSDPA Block Error Ratio (HBLER) Measurement). However, note that because they are being calculated for a different set of blocks (the HSDPA counters are typically calculated over a much greater number of blocks), the results will often vary.

The following results can be queried together by CALL:HSDPa:RTIMe:RESults:ALL?  

3GPP TS 34.121 F.6.3.2 defines the HSDPA block error ratio as: (NACK + statDTX)/(NACK+ statDTX +ACK).

HSUPA Information

The HSUPA Information window displays counters to help you monitor the HSUPA connection status. The results are continually updated. When one of the following events occurs, the counters reset to zero and then resume counting:

The following HSUPA information are displayed (This is front panel display only):

TD-SCDMA Test Operating Mode Screen

Generated Power Level Information

The power levels that are currently being used by the test set (Current Level) and the "desired" levels you've input (Desired Level) are shown on the Generated Power Level Information screen as below.

If you request an invalid combination of power levels, the test set posts a persistent error and the settings you've requested will be shown in the Desired Level column. The set of levels in use by the test set does not change until you request a valid combination of levels, then the values in the Current Level and Desired Level columns will match.

Whether the combination of power levels is valid is determined by the following requirements:

To query the power levels, use the GPIB commands for setting/querying:

Parameter

Current Level

Desired Level

Cell Power

CALL:STATus:CELL:POWer[:AMPLitude][:SELected]?

CALL[:CELL]:POWer:AMPLitude[:SELected]

AWGN Power

CALL:STATus:AWGNoise[:INTernal]:POWer[:AMPLitude][:SELected]?

CALL:AWGNoise[:INTernal]:POWer[:SAMPlitude][:SELected]

Total RF Power

CALL:STATus:TOTal:POWer[:AMPLitude][:SELected]?

CALL:TOTal:POWer[:AMPLitude][:SELected]?

Downlink Code Channel Power Level Information

See Downlink Code Channel Power Level Information

CW Operating Mode Screen

CW Parameters

FM Broadcast Parameters

GPS Parameters

See GPS Parameter Information

Active Cell Connection State

Additional call processing state information is also displayed in the small Active Cell window at the bottom of the Call Setup screen. Note that for single services, the respective Call Connection State or Data Connection State is displayed.

Call Connection State

The call connection state can transition between the following states:

GPIB command: CALL:STATus[:STATe][:VOICe]?

Data Connection State

The data connection state can transition between the following states:

GPIB command: CALL:STATus[:STATe]:DATA?

Related Topics

GPIB Commands: CALL:STATus