Last updated: 2014-11-28
Through the Time Slot to Measure setting, you can select which uplink time slot the test set will measure. This setting has been applied to four measurements: Adjacent Channel Leakage Ratio (ACLR) Measurement, Channel Power Measurement, Spectrum Emission Mask (SEM) Measurement, and Waveform Quality Measurement.
There are four parameters: TS1, TS2, TS3, and TS4.
The default setting is TS1.

The measurement trigger source should be Protocol or Auto to enable this setting.
|
|
The operating mode is set to Active Cell. |
Or else, this setting will be out of scope and won't affect the measurement behavior.
The time slot to measure should be the actual uplink time slot. Or else, initiating measurement will cause the +754 error message prompts. For more details, see +700 through +799 Error Message Descriptions.
When the setting is in scope and takes effect, the trigger delay will act alongside this setting.
GPIB Command: SETup:TCPower:TSLot:MEASure